Post Go back to editing

Yocto Linux build version 5.0.0 on ADSP-SC594 EZKIT - system freezes

Category: Software
Product Number: ADSP-SC594
Software Version: 5.0.0

Hi community,

I was very happy to run the process to build a Yocto Linux version 5.0.0 to be run on the SC594 EZKIT these days. In particular, the description how to build, release and install the system was really very good, thank you for that!

Unfortunately, the system does not really work in a stable way: once booted from SPI, the system freezes after a while. I found that it freezes within the time of a few seconds whenever a GBit cable is connected to the ethernet port. If no cable is connected, I have observed that the system freezes after some minutes, e.g., approximately 30 minutes.  

I also ran the system in nfsboot mode. Unfortunately, then, the system freezes after boot as well.

In the next step I built the older Yocto Linux version 3.1.2. With this version, the nfsboot on the EZKIT seems to work in a stable way. However, when trying to run spiboot, an error occurs whenever reading the kernel from spi memory in uboot with an error message reporting a wrong image format for bootm. I was able to work around this problem by using the stage1-boot.ldr and stage2-boot.ldr files from the version 5.0.0 build instead of the versions from 3.1.2 in combination with the kernel and the jff2 file from version 3.1.2.
Principally the boot process worked fine but later, unfortunately, error messages are shown indicating that the jff2 file system is broken (missing folder /var/run).

I am using a recent ADSP-SC594-EZKIT with SOM Rev C and EZKIT baseboard revision D.

Is there any kind of workaround to have version 5.0.0 running from SPI flash in a stable way?

Thank you and best regards

Hauke

Parents
  • Hi  ,

    Is this stock yocto/linux with nothing else running whatsover?

    Additionally, could you try the following steps with yocto 5.0.0:

    - Load uboot via gdb as usual

    - Once in uboot shell, run "run erase_spi"

    NOTE: This will take some time, do not worry if there is no output. The process should take about 10-15mins.

    - run "env default -a"
    - run "run update_spi"

    Alternatively, you could also attempt using the OSPI: github.com/.../Getting-Started-with-ADSP‐SC594-(Linux-for-ADSP‐SC5xx-Processors-5.0.0)

  • Hi,

    thank you for your response.
    I am using the stock yocto/linux - following in detail what is described on the website for version 5.0.0 Yocto/Linux build on a Ubuntu 24.04 host PC.

    I tried what you proposed:

    run erase_spi
    env default -a
    run update_spi

    Then switch boot switch to option 1 and reset. The system boots as expected and is then up and running. I then left the room and after 30 minutes, the watchdog had restarted the device. Hence, problem is still present even though the hang seems not to start immediately. A few days ago my feeling was that the uptime is shorter the longer the board is on, therefore, I added a cooling capability on the device - without any real impact.

    I also tried to run the OSPI option. However, I am not able to store the overall system on OSPI since the size of the image is too large (seems that OSPI is only 32 MB large).

    By the way, the behavior of the linux is also kind of strange: Typing, e.g., "ip a" does not return unless I push return. Could also be that something is broken in the serial output of the Linux with version 5.0.0.

    Thank you and best regards

    hkhauke

Reply
  • Hi,

    thank you for your response.
    I am using the stock yocto/linux - following in detail what is described on the website for version 5.0.0 Yocto/Linux build on a Ubuntu 24.04 host PC.

    I tried what you proposed:

    run erase_spi
    env default -a
    run update_spi

    Then switch boot switch to option 1 and reset. The system boots as expected and is then up and running. I then left the room and after 30 minutes, the watchdog had restarted the device. Hence, problem is still present even though the hang seems not to start immediately. A few days ago my feeling was that the uptime is shorter the longer the board is on, therefore, I added a cooling capability on the device - without any real impact.

    I also tried to run the OSPI option. However, I am not able to store the overall system on OSPI since the size of the image is too large (seems that OSPI is only 32 MB large).

    By the way, the behavior of the linux is also kind of strange: Typing, e.g., "ip a" does not return unless I push return. Could also be that something is broken in the serial output of the Linux with version 5.0.0.

    Thank you and best regards

    hkhauke

Children


  • I also tried to run the OSPI option. However, I am not able to store the overall system on OSPI since the size of the image is too large (seems that OSPI is only 32 MB large).

    You can store the file system on the qspi, if you have another media present like a USB stick, that should work too. You can then run "run update_ospi_uboot_only" and only flash uboot onto the ospi and boot with bootmode 5 that way. The default command that is executed on autoboot or just "boot" is set at "bootcmd". So if you wanted to mix and match boot modes, you could give that a try as well.

    Hence, problem is still present even though the hang seems not to start immediately.


    As for the system after booting with qspi, we will try to reproduce on our side.


    By the way, the behavior of the linux is also kind of strange: Typing, e.g., "ip a" does not return unless I push return. Could also be that something is broken in the serial output of the Linux with version 5.0.0.

    Hmm, about the serial console, it sounds a bit strange. From what I understand, you type the command out - no delay, working as expected, press return - no response and return again - after which you get a response?

  • Is there any kernel panic or kernel crashes? Any logs to share?

  • I just got the system booting from USB external drive - memory stick. This works for version 5.0.0 BUT - again system freezes after a short moment and is not useable.

    However, I did the same for version 3.1.2 and it works. Hence, for me to work with version 3.1.2 booting from USB memory stick is a good option for now. Hopefully all features for communication between DSPs and ARM core also work with version 3.1.2...

    Searching this for a while, I finally found the option to override the "bootcmd" expression in uboot, but now the systems boots straight through which was the desired goal for the next development issues.


    Regarding the serial console with version 5.0.0: I type "ip a". Then the information is shown but prompt is not back. Then I push return and see prompt twice. It seems hence that the first "return" after "ip a" was stuck.

  • can you try to run "run ramboot" from u-boot and if you experience same issue? I have closer look at this issue

  • I just running Yocto-5 from my current build and I can't reproduce same behaviour, so will need to get clean build and see if I can reproduce 

  • Yes, I started to "run ramboot" a few hours ago. The system was still stable after 6 hours - looks good. It does not show the weird console behavior reported earlier.

  • I could provide you with those six files (uboot, fitImage, root filesystem) which are stored in my /tftpboot folder for version 5.0.0 to give it a quick try.

  • Another update on this issue: I cross combined rootfs and kernels:

    1) Rootfs from version 5.0.0, Kernel from version 3.1.2 -> System runs properly and stable for at least 30 minutes
    2) Rootfs from version 3.1.2, kernel from version 5.0.0 -> System boots and hangs immediately

    No log can be reviewed as the system freezes without any verbose output. I cannot even logon using ssh as the system does not live long enough to view the IP address.

    Also, I have run the same tests on a second board today - same results, unfortunately. 

    From these tests I conclude that the problem is related to the kernel itself and not a hw issue.

    Best regards

  • Hi, I removed the ethernet from device-tree for Yocto-5 and spi boot seems stable. Will need to spend more time on this and see root cause of issue. 

  • We just found that some of the patches for the Linux kernel Yocto recipe (device tree) are applied for SC598 in case of machine type SC594. In this case, the patches will not be applied for SC594 since SC598 is ARM64 and SC594 is ARM(32) - hence the device trees are not modified. Maybe a hint for what goes wrong..

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.