I've downloaded the latest Yocto 3.0.0 version.
The build for CONFIG_MACH_SC584_EZKIT is running smoothly.
However, I now need to set up the configuration for ADSP-SC587.
Upon reviewing the configuration files, I've noticed some specific numerical values in the makefile.boot that seem crucial.
Could you please provide guidance on which numerical values I should input to ensure the proper functioning of ADSP-SC587?
Failing to set these values correctly will result in a compilation halt.
Additionally, are there any other modifications or patches required to make ADSP-SC587 work seamlessly?
I couldn't find any references to ADSP-SC587 in the existing documentation.
My primary objective is to run a minimal kernel on the ARM core while enabling USB-gadget support and establishing inter-process communication with the two DSP cores.
Unfortunately, the build issues I'm encountering are hindering the progress of my development project.
makefile.boot:
# SPDX-License-Identifier: GPL-2.0 ifeq ($(CONFIG_MACH_SC573_EZKIT),y) zreladdr-y += 0x82008000 params_phys-y := 0x82000100 endif ifeq ($(CONFIG_MACH_SC584_EZKIT),y) zreladdr-y += 0x89008000 params_phys-y := 0x89000100 endif ifeq ($(CONFIG_MACH_SC589_EZKIT),y) zreladdr-y += 0xC2008000 params_phys-y := 0xC2000100 endif ifeq ($(CONFIG_MACH_SC589_MINI),y) zreladdr-y += 0xC2008000 params_phys-y := 0xC2000100 endif ifeq ($(CONFIG_MACH_SC594_SOM),y) zreladdr-y += 0x82008000 params_phys-y := 0x82000100 endif