Post Go back to editing

pin configuration

Category: Software
Product Number: ADSP-SC594
Software Version: 2.11.0

The sc594 has a file pinctrl-adi2-sc59x.c  which sets the pin used by each peripheral.

For example this is the configuration for the uart0 peripheral

static const unsigned uart0_pins[] = {
GPIO_PB2, GPIO_PB3,
};

Im porting our linux changes to the sc598, but this file doesn't exist

The pinctrl code looks to be in the directory drivers/pinctrl/adi but I cannot find where the pins are configured for each peripheral.

Can you point me to where the uart0 and ethernet pins are configured ?

Thanks Chris