I have to debug one new project in linux CCES Application just have to print some printing statement
I used the following procedure for debugging the project which is created in CCES.
Now i ain't able to execute the program it throwing some error
Error message from debugger back end:
172.21.3.130:3333: Connection timed out.
172.21.3.130:3333: Connection timed out.
In uboot side i deployed the linux in ADSP-SC573 (IPAddress: 172.21.3.130)
I hope something i am messing up the things which is already provided.
Wait for the reply to correct my mistakes,
Thankyou,
Sushindren