I've been attempting to use MCAPI to converse with the SHARC+ cores on an SC589.
The recipe for libmcapi.so doesn't publish header files so you can't actually compile anything with it.
But after a trivial patch, I still can't get a simple program to link using a yocto recipe. Either my linking with `-lmcapi` isn't right, or there's something else required because I only get "undefined reference to `mcapi_initialize'"
Has anyone ever actually used a yocto built arm mcapi application to talk to a SHARC+ core?
diff --git a/meta-adi-adsp-sc5xx/recipes-icc/libmcapi/libmcapi.bb b/meta-adi-adsp-sc5xx/recipes-icc/libmcapi/libmcapi.bb index db41169..a503400 100644 --- a/meta-adi-adsp-sc5xx/recipes-icc/libmcapi/libmcapi.bb +++ b/meta-adi-adsp-sc5xx/recipes-icc/libmcapi/libmcapi.bb @@ -29,9 +29,14 @@ do_compile_prepend(){ do_install(){ install -d ${D}/usr/bin - install -d ${D}/usr/lib + install -d ${D}/usr/lib + install -d ${D}/usr/include install -m 755 ${S}/tests/.libs/* ${D}/usr/bin/ install -m 755 ${S}/.libs/libmcapi.so.0.0.0 ${D}/usr/lib/ - ln -s libmcapi.so.0.0.0 ${D}/usr/lib/libmcapi.so.0 - ln -s libmcapi.so.0.0.0 ${D}/usr/lib/libmcapi.so -} \ No newline at end of file + ln -s libmcapi.so.0.0.0 ${D}/usr/lib/libmcapi.so.0 + ln -s libmcapi.so.0.0.0 ${D}/usr/lib/libmcapi.so + install ${S}/include/*.h ${D}/usr/include +} + +FILES_${PN} += "/usr/lib/* /usr/bin/*" +FILES_${PN}-dev += "/usr/include"
Edit Notes
spelling[edited by: rireland at 7:03 PM (GMT -5) on 25 Jan 2022]