Dear,
How we can integrate an sigmastudio application on sharc cores together with Linux.
Is there an example?
Dear,
How we can integrate an sigmastudio application on sharc cores together with Linux.
Is there an example?
Hi,
could you provide us with more details regarding what you are looking to achieve with Linux and Sigma Studio?
For example, are you looking to pass audio data to/from the Linux core to the SHARC cores?
Or are you looking to do something more specific with Sigma Studio and Linux.
Regards,
Dave
Hi,
To explain it more easily, let's use the "DemoUC project as example for a SC589 .
At this moment we want nothing to change in the sharc0 and 1 cores.
CORE0 (ARM core) works on Linux.
The code on core0, what we must do with it?
Compiling this source code in a app on linux or something else?
What to do with the memory addressing like (#pragma section("ss_app_code") in this code?
How we can get/set the parameters/registers from the linux core to the sigmastudio schematic project?
Is there an example project where signamstudio schematic works together with linux?
Can someone answer my request.
It's very urgent