Hi, support,
I am starting familiarize myself with the ADSP-SC589 EZ-Board, and so far I have got the linux core working, using the default linux image.
I am following the instructions in "linux_add_in_user_guide_1.3.1", and I have been able to set it up to boot from the SD card.
However, I had no ethernet network running, so I did the "make menuconfig" and enabled "DHCP", and ran "make" to build from source. In this process I also selected the "nano" text editor.
I replaced the content of the SD-card and rebooted the board.
The nano text editor was there, and the /etc/network/interfaces had changed to include DHCP.
But "ifconfig -a" showed no ip.
If I do "/etc/init.d/S40network restart" I get
# ./S40network restart
Stopping network...ifdown: interface lo not configured
ifdown: interface eth0 not configured
Starting network...
/bin/sh: run-parts: not found
ifup: don't seem to have all the variables for eth0/inet
What am I doing wrong?
BN
Thanks to your advice, it is working now.
Thank you very much.
Hi bnilsson,
When you boot from SD card, the ethernet should first setup in u-boot or bring up manually by input "ifconfig eth0 IP_ADDR up" after linux kernel bootup, once the log "stmmaceth 3100c000.ethernet eth0: Link is Up - 100Mbps/Full - flow control rx/tx " occurs it means the eth0 is ready.
In u-boot(one more step than the linux addin user guide - run addip):
set sdargs set bootargs root=/dev/mmcblk0p1 rw rootwait rootfstype=ext3 clkin_hz=(25000000) earlyprintk console=ttySC0,57600 set sdboot 'run sdargs; run addip;ext2load mmc 0:1 ${dtbaddr} sc589-ezkit.dtb;ext2load mmc 0:1 ${loadaddr} vmImage-sc589-ezkit;bootm ${loadaddr} - ${dtbaddr}'
In linux-kernel:
# ifconfig eth0 10.99.24.107 up # stmmaceth 3100c000.ethernet eth0: Link is Up - 100Mbps/Full - flow control rx/tx ifconfig eth0 Link encap:Ethernet HWaddr 02:80:AD:20:31:E4 UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1 RX packets:7 errors:0 dropped:0 overruns:0 frame:0 TX packets:0 errors:0 dropped:0 overruns:0 carrier:0 collisions:0 txqueuelen:1000 RX bytes:420 (420.0 B) TX bytes:0 (0.0 B) Interrupt:103 Base address:0xc000
If you want to use the dhcp command, you could refer to the talks in this thread. https://ez.analog.com/dsp/software-and-development-tools/linux-for-adsp-sc5xx-processors/f/q-a/100106/can-t-get-ifup-eth0-to-work/299290#299290 . It talks about how to enable the dhcp command based on the exsiting linux addin 1.3.1 release.
For more questions please let me know. Thanks a lot.