Enabling New Space Missions: Commercial Space Screening Approach for Agile, High-Reliability Payloads

    As the Space market evolves and accelerates, mission designers need space-capable electronics that balance performance, reliability, and affordability...
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
    • Other Products Library
    • Precision Technology Signal Chains Library
    • Software Modules and SDKs Library
    • Supervisory Circuits Library
    • Wireless Sensor Networks Library

    Latest Webinars

    • Enabling New Space Missions: Commercial Space Screening Approach for Agile, High-Reliability Payloads
    • Understanding and Selecting RF Low Noise Amplifiers for Instrumentation, Phased Array and General Purpose Applications
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
      1. Quote of this month: " When I die, I want to die like my grandfather who died peacefully in his sleep. Not screaming like all the passengers in his...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: Mature, Not Old! The Longevity of 4 – 20 mA New...
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
    Charting Calm Seas: Tips for Robust RS-485 Data Transmission

    by Bryson Barney As our world becomes ever more dependent on flawless digital communication, engineers need to find new ways of charting calm seas when...

     

    Unpacking IEC 61508: Low Complexity versus Type A Made Simple

    IEC 61508 appears to include two very similar concepts. Type A and simple, which is referred to as “low complexity”. Anything that isn’t low complexity...

    Latest Blogs

    • Taming the AI Power Storm: Part 2 of 3
    • TIA Me Up, But Keep It Stable: Part 2 of 3
    • Celebrating Innovation: Top 3 EngineerZone Spotlight Blogs from 2025
    • Transforming Power: Transfer Techniques in SMPS: Part 3 of 4
    • Taming the Chaos: Correlated and Uncorrelated Sources in LTspice .NOISE Simulations: Part 3 of 3
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
Linux Distribution for Blackfin
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Linux Distribution for Blackfin
  • Processors & DSP
  • Software & Development Tools
  • Linux Distribution for Blackfin
  • Cancel
Linux Distribution for Blackfin
Documents How to autorun applications in uClinux
  • Q&A
  • Docs/FAQs
  • Members
  • Tags
  • Cancel
  • +Documents
  • +2013R1 Linux release for Blackfin: FAQ
  • +2013R1: FAQ
  • +AD5700: FAQ
  • +ADI test script: FAQ
  • +bf537 SPI Bus: FAQ
  • +BF609: FAQ
  • +BF70x processor: FAQ
  • +bfin-elf-libstdc++-4.3: FAQ
  • +bfin-elf: FAQ
  • +bfin-uclinux-libstdc++-4.3: FAQ
  • +Blackfin Linux Projects: FAQ
  • +Blackinfin Linux: FAQ
  • +build toolchain: FAQ
  • +CPLB fault or SIGABRT: FAQ
  • +DAS U-BOOT FOR BLACKFIN: FAQ
  • +Default ADI release: FAQ
  • +Flash the uImage into Flash: FAQ
  • +gas test: FAQ
  • +gcc-4.3 ICEs: FAQ
  • +gcc.c-torture/execute/memset-2.c: FAQ
  • +gcc.dg/trampoline-1.c test: FAQ
  • +gcc/g++ test: FAQ
  • +gcc/g++ testcase: FAQ
  • +GDB commands: FAQ
  • +gdb.base/sigall.exp: FAQ
  • +gdb.cp/userdef.exp: FAQ
  • +gdb.gdbtk/c_variable.exp: FAQ
  • +GDB: FAQ
  • +gdb: symbol: FAQ
  • +gdbproxy: FAQ
  • +GNU TOOLCHAIN: FAQ
  • +How to load Linux: FAQ
  • +ldr-utils: FAQ
  • +libstdc++-4.3 21_strings/basic_string/capacity/char/18654.cc test: FAQ
  • +LOOP: FAQ
  • +mcpu: FAQ
  • +Parent Document for U-Boot Bug Archive: FAQ
  • +Parent Document for U-Boot Bug Forum Archive: FAQ
  • +Parent for all content moved from GNU Archive: FAQ
  • +prepare_target_solibs: FAQ
  • +SDP-B: FAQ
  • +signal 11: FAQ
  • +sim binutils: FAQ
  • +SPI eeprom: FAQ
  • +svn head u-boot build: FAQ
  • +test libmudflap: FAQ
  • +toolchain-regtest -r: FAQ
  • +toolchain-regtest: FAQ
  • +trunk head gdbproxy: FAQ
  • +trunk toolchain: FAQ
  • +u-boot with UART: FAQ
  • +u-boot: FAQ
  • +uClinux kernel: FAQ
  • -uClinux: FAQ
    • How to autorun applications in uClinux
    • [DOC] Configuring Qt Creator as SDK for uClinux
  • +Upgrade from 3801 to 3852: FAQ
  • +VDSP: FAQ

How to autorun applications in uClinux

Good day to all,

Hi, in my previous question I asked how one can configure u-boot to automatically load the kernel (uimage) after booting in my BF537 board. Thanks to the help that I received I was able to do so. However, another problem arose. After doing some research and readings from different sources, I still haven't found the answer to how one can configure the uimage to automatically run the application I have done. As an example, say I want to run the simple "Hello World" application written in C, I need to do lrz to transfer it to the board then run ./helloworld (or whatever file name I have set it); now I am wondering what are the methods I need to do in order for my "Hello World" application to run after the uimage has boot without me having to manually input the commands to run it.

As added info, I believe that one can incorporate the application to the image file through 'make', but still the question remains how I can have that application run automatically. Also, I am unsure if etc/rc or etc/inittab is the right way to go, if so are there any documents that can guide me to set this up? Any form of help would be greatly appreciated!

Thank you in advance!

-Angelo

Angelo,

You can use /etc/rc to run your application.  The init application needs to be setup; and usually isn't used or defaults to the command shell for start-up.

Some notes:

a)  If you want a blocking process, or one that takes a long time, to run in the background use the '&' postfix to the command to spawn it in the background.

b)  Path and environment variables usually are not visible in /etc/rc; so, you need to specify the full path for most commands.

c)  You can also include the application as part of the image (uImage) file as well.  Look in the uclinux/Documentation/Adding-User-Apps-HOWTO file.

Look in the uclinux/Documentation/Adding-Platforms-HOWTO and the uclinux/vendors directory... you will see a directory for AnalogDevices there.  in AnalogDevices/common there is the rc file that gets loaded for all the AnalogDevices boards.  But, I'm assuming you are using an AnalogDevices board.

You can't use relative paths to run your application.

The only exception seems to be if it is installed in /bin directory.

So if you have the executable installed to /home/angelo/hello you need:

     /home/angelo/hello

to start the application.

the 2 documents I pointed out are good references to get started on getting the user application and building a vendor point (which may or may not be needed).

The rc script when run in alongside the busybox command shell that environment variables that set the time-zone, search path, and etc are not properly exported to the applications that run from the rc script file.  I haven't been able to find a good solution for this other than it is a known issue with busybox implementation.

Even if you aren't a vendor, it helps to keep your stuff separate from changes upstream.  But, it does mean you may have to make changes as upstream changes.

James

This FAQ was generated from the following discussion: How to autorun applications in uClinux

  • Share
  • History
  • More