Power Integrity for High Performance Measurement Systems

    Increasing data rates driven by AI workloads and the evolution from 5G to emerging 6G standards are placing new demands on electronic test and measurement...
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
      1.Quote of the month: "People Who Say They Sleep Like a Baby usually don't have one" - unknown 2. New quiz AQQ302 about Band Gap Reference Voltage...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card! - Watts Going On? — The AI Power Delivery Quiz

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Reimagining Power for AI: Shaping the Future of AI Acceleration...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Game of DronesPart 1: How IMU Navigation Architectures Make or Break a Drone

    This article explains why industrial-grade UAVs require fundamentally different architectures than consumer drones. It highlights the need for inertial...

EngineerZone
EngineerZone
Linux Distribution for Blackfin
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Linux Distribution for Blackfin
  • Processors & DSP
  • Software & Development Tools
  • Linux Distribution for Blackfin
  • Cancel
Linux Distribution for Blackfin
Documents [#7318] Ensure that -mmulticore -mcore0 is set on Eclipse ADSP-BF561/BF60x project creation
  • Q&A
  • Docs/FAQs
  • Members
  • Tags
  • Cancel
  • +Documents
  • +2013R1 Linux release for Blackfin: FAQ
  • +2013R1: FAQ
  • +AD5700: FAQ
  • +ADI test script: FAQ
  • +bf537 SPI Bus: FAQ
  • +BF609: FAQ
  • +BF70x processor: FAQ
  • +bfin-elf-libstdc++-4.3: FAQ
  • +bfin-elf: FAQ
  • +bfin-uclinux-libstdc++-4.3: FAQ
  • +Blackfin Linux Projects: FAQ
  • +Blackinfin Linux: FAQ
  • +build toolchain: FAQ
  • +CPLB fault or SIGABRT: FAQ
  • +DAS U-BOOT FOR BLACKFIN: FAQ
  • +Default ADI release: FAQ
  • +Flash the uImage into Flash: FAQ
  • +gas test: FAQ
  • +gcc-4.3 ICEs: FAQ
  • +gcc.c-torture/execute/memset-2.c: FAQ
  • +gcc.dg/trampoline-1.c test: FAQ
  • +gcc/g++ test: FAQ
  • +gcc/g++ testcase: FAQ
  • +GDB commands: FAQ
  • +gdb.base/sigall.exp: FAQ
  • +gdb.cp/userdef.exp: FAQ
  • +gdb.gdbtk/c_variable.exp: FAQ
  • +GDB: FAQ
  • +gdb: symbol: FAQ
  • +gdbproxy: FAQ
  • +GNU TOOLCHAIN: FAQ
  • +How to load Linux: FAQ
  • +ldr-utils: FAQ
  • +libstdc++-4.3 21_strings/basic_string/capacity/char/18654.cc test: FAQ
  • +LOOP: FAQ
  • +mcpu: FAQ
  • +Parent Document for U-Boot Bug Archive: FAQ
  • +Parent Document for U-Boot Bug Forum Archive: FAQ
  • -Parent for all content moved from GNU Archive: FAQ
    • [#7290] Blackfin GNU tool chain Eclipse plug-in does not support ADSP-BF60x
    • [#7291] Blackfin GNU tool chain Eclipse plug-in does not specify -mcpu for Assembly source
    • [#7292] Blackfin GNU tool chain Eclipse plug-in reports "WARNING: The "Debug" Configuration may not build"
    • [#7293] Blackfin GNU tool chain Eclipse plug-in reports "This discovery method is deprecated" when used with Juno Release
    • [#7299] Blackfin GNU tool chain Eclipse Memory Mapped Registers View plug-in uses outdated proc files and does not support ADSP-BF60x
    • [#7300] kernel build with busybox 1.20 by trunk head toolchain and uClibc 0.9.33.2 boot up fails
    • [#7305] bfin-jtag.exe and bfin-gdbproxy.exe do not work on Windows
    • [#7313] bfin-gdbproxy crashes when attempting to load an executable on Windows
    • [#7317] GCC should generate code for Core 0 by default
    • [#7318] Ensure that -mmulticore -mcore0 is set on Eclipse ADSP-BF561/BF60x project creation
  • +prepare_target_solibs: FAQ
  • +SDP-B: FAQ
  • +signal 11: FAQ
  • +sim binutils: FAQ
  • +SPI eeprom: FAQ
  • +svn head u-boot build: FAQ
  • +test libmudflap: FAQ
  • +toolchain-regtest -r: FAQ
  • +toolchain-regtest: FAQ
  • +trunk head gdbproxy: FAQ
  • +trunk toolchain: FAQ
  • +u-boot with UART: FAQ
  • +u-boot: FAQ
  • +uClinux kernel: FAQ
  • +uClinux: FAQ
  • +Upgrade from 3801 to 3852: FAQ
  • +VDSP: FAQ

[#7318] Ensure that -mmulticore -mcore0 is set on Eclipse ADSP-BF561/BF60x project creation

[#7318] Ensure that -mmulticore -mcore0 is set on Eclipse ADSP-BF561/BF60x project creation

Submitted By: Andrew McLachlan

Open Date

2012-09-11 05:32:22     Close Date

2012-10-10 03:32:56

Priority:

Medium High     Assignee:

Andrew McLachlan

Board:

N/A     Silicon Revision:

Resolution:

Fixed     Fixed In Release:

N/A

Processor:

ALL     

Host Operating System:

toolchain rev.:

    kernel rev.:

State:

Closed     Found In Release:

2012R1

Is this bug repeatable?:

N/A     

Summary: Ensure that -mmulticore -mcore0 is set on Eclipse ADSP-BF561/BF60x project creation

Details:

#7317 and #7313 outline an issue with running a program on Core 0 that could

have easily been avoided.

Although #7317 (GCC should generate code for Core 0 by default) would mean that

an out-of-the box BF609 single project would run on Core 0, an App-per-core

project set-up would fail, if we were to create two projects.

We therefore require the setting of "-mmulticore -mcore0" during New project

creation in Eclipse too. And, perhaps, the ability to toggle the core nicely

in the Tools Settings.

Follow-ups

--- Andrew McLachlan                                         2012-10-10 04:34:27

Fixed in plug-ins version 1.0.7.

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

File Name     File Type     File Size     Posted By

No Files Were Found

  • Share
  • History
  • More