Open RAN 5G Radio Design: SDR SoCs for Energy-Efficient, Secure Deployments

    Building Secure and Energy‑Efficient 5G Networks with Software Defined Radios. The rapid evolution of 5G networks is driving new requirements for performance...
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
    • Power Integrity for High Performance Measurement Systems
    View All Webinars
  • Community Hub

    Challenge Yourself!

      KCC Quizzes AQQ302 about Bang Gap Reference Generation

      1.Quote of the month: "People Who Say They Sleep Like a Baby usually don't have one" - unknown 2. New quiz AQQ302 about Band Gap Reference Voltage...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card! - Watts Going On? — The AI Power Delivery Quiz

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Reimagining Power for AI: Shaping the Future of AI Acceleration...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Game of DronesPart 1: How IMU Navigation Architectures Make or Break a Drone

    This article explains why industrial-grade UAVs require fundamentally different architectures than consumer drones. It highlights the need for inertial...

EngineerZone
EngineerZone
Linux Distribution for Blackfin
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Linux Distribution for Blackfin
  • Processors & DSP
  • Software & Development Tools
  • Linux Distribution for Blackfin
  • Cancel
Linux Distribution for Blackfin
Documents [#7305] bfin-jtag.exe and bfin-gdbproxy.exe do not work on Windows
  • Q&A
  • Docs/FAQs
  • Members
  • Tags
  • Cancel
  • +Documents
  • +2013R1 Linux release for Blackfin: FAQ
  • +2013R1: FAQ
  • +AD5700: FAQ
  • +ADI test script: FAQ
  • +bf537 SPI Bus: FAQ
  • +BF609: FAQ
  • +BF70x processor: FAQ
  • +bfin-elf-libstdc++-4.3: FAQ
  • +bfin-elf: FAQ
  • +bfin-uclinux-libstdc++-4.3: FAQ
  • +Blackfin Linux Projects: FAQ
  • +Blackinfin Linux: FAQ
  • +build toolchain: FAQ
  • +CPLB fault or SIGABRT: FAQ
  • +DAS U-BOOT FOR BLACKFIN: FAQ
  • +Default ADI release: FAQ
  • +Flash the uImage into Flash: FAQ
  • +gas test: FAQ
  • +gcc-4.3 ICEs: FAQ
  • +gcc.c-torture/execute/memset-2.c: FAQ
  • +gcc.dg/trampoline-1.c test: FAQ
  • +gcc/g++ test: FAQ
  • +gcc/g++ testcase: FAQ
  • +GDB commands: FAQ
  • +gdb.base/sigall.exp: FAQ
  • +gdb.cp/userdef.exp: FAQ
  • +gdb.gdbtk/c_variable.exp: FAQ
  • +GDB: FAQ
  • +gdb: symbol: FAQ
  • +gdbproxy: FAQ
  • +GNU TOOLCHAIN: FAQ
  • +How to load Linux: FAQ
  • +ldr-utils: FAQ
  • +libstdc++-4.3 21_strings/basic_string/capacity/char/18654.cc test: FAQ
  • +LOOP: FAQ
  • +mcpu: FAQ
  • +Parent Document for U-Boot Bug Archive: FAQ
  • +Parent Document for U-Boot Bug Forum Archive: FAQ
  • -Parent for all content moved from GNU Archive: FAQ
    • [#7290] Blackfin GNU tool chain Eclipse plug-in does not support ADSP-BF60x
    • [#7291] Blackfin GNU tool chain Eclipse plug-in does not specify -mcpu for Assembly source
    • [#7292] Blackfin GNU tool chain Eclipse plug-in reports "WARNING: The "Debug" Configuration may not build"
    • [#7293] Blackfin GNU tool chain Eclipse plug-in reports "This discovery method is deprecated" when used with Juno Release
    • [#7299] Blackfin GNU tool chain Eclipse Memory Mapped Registers View plug-in uses outdated proc files and does not support ADSP-BF60x
    • [#7300] kernel build with busybox 1.20 by trunk head toolchain and uClibc 0.9.33.2 boot up fails
    • [#7305] bfin-jtag.exe and bfin-gdbproxy.exe do not work on Windows
    • [#7313] bfin-gdbproxy crashes when attempting to load an executable on Windows
    • [#7317] GCC should generate code for Core 0 by default
    • [#7318] Ensure that -mmulticore -mcore0 is set on Eclipse ADSP-BF561/BF60x project creation
  • +prepare_target_solibs: FAQ
  • +SDP-B: FAQ
  • +signal 11: FAQ
  • +sim binutils: FAQ
  • +SPI eeprom: FAQ
  • +svn head u-boot build: FAQ
  • +test libmudflap: FAQ
  • +toolchain-regtest -r: FAQ
  • +toolchain-regtest: FAQ
  • +trunk head gdbproxy: FAQ
  • +trunk toolchain: FAQ
  • +u-boot with UART: FAQ
  • +u-boot: FAQ
  • +uClinux kernel: FAQ
  • +uClinux: FAQ
  • +Upgrade from 3801 to 3852: FAQ
  • +VDSP: FAQ

[#7305] bfin-jtag.exe and bfin-gdbproxy.exe do not work on Windows

[#7305] bfin-jtag.exe and bfin-gdbproxy.exe do not work on Windows

Submitted By: Andrew McLachlan

Open Date

2012-09-03 03:39:40     Close Date

2012-09-28 12:25:54

Priority:

High     Assignee:

Jie Zhang

Board:

N/A     Silicon Revision:

Resolution:

Rejected     Fixed In Release:

N/A

Processor:

ALL     

Host Operating System:

Windows

toolchain rev.:

    kernel rev.:

State:

Closed     Found In Release:

2012R1

Is this bug repeatable?:

N/A     

Summary: bfin-jtag.exe and bfin-gdbproxy.exe do not work on Windows

Details:

Trying to connect to ADSP-BF609 rev 1.2 with ICE-100B

(firmware version is 2.0.7)

http://docs.blackfin.uclinux.org/doku.php?id=hw:jtag:ice100b says

that the firmware must be >= 1.0.7

-- GNU tools running under Cygwin on Windows 7 64bit --

$ bfin-jtag.exe

cable probe

Found USB cable: ICE-100B

(no more output)

$ bfin-gdbproxy.exe

Remote proxy for GDB, v0.7.2, Copyright (C) 1999 Quality Quorum Inc.

MSP430 adaption Copyright (C) 2002 Chris Liechti and Steve Underwood

Blackfin adaption Copyright (C) 2008 Analog Devices, Inc.

GDBproxy comes with ABSOLUTELY NO WARRANTY; for details

use `--warranty' option. This is Open Source software. You are

welcome to redistribute it under certain conditions. Use the

'--copying' option for details.

Found USB cable: ICE-100B

error:     bfin: cable initialization failed

-- Ubuntu running through Virtualbox --

$ sudo ./bfin-gdbproxy

Remote proxy for GDB, v0.7.2, Copyright (C) 1999 Quality Quorum Inc.

MSP430 adaption Copyright (C) 2002 Chris Liechti and Steve Underwood

Blackfin adaption Copyright (C) 2008 Analog Devices, Inc.

GDBproxy comes with ABSOLUTELY NO WARRANTY; for details

use `--warranty' option. This is Open Source software. You are

welcome to redistribute it under certain conditions. Use the

'--copying' option for details.

Found USB cable: ICE-100B

ICE-100B firmware version is 2.0.7

IR length: 5

Chain length: 1

Device Id: 00000010100000000100000011001011 (0x028040CB)

  Manufacturer: Analog Devices, Inc. (0x0CB)

  Part(0):      SDU (0x2804)

  Stepping:     0

  Filename:     ./../share/urjtag/analog/sdu/sdu

warning:   bfin: no board selected, 3 parts are detected

warning:   bfin:   parts: [BF609 BF609] SDU

notice:    bfin: jc: waiting on TCP port 2001

notice:    bfin: jc:  (you must connect GDB before using jtag console)

notice:    bfin-gdbproxy: waiting on TCP port 2000

$ sudo ./bfin-gdbproxy

Remote proxy for GDB, v0.7.2, Copyright (C) 1999 Quality Quorum Inc.

MSP430 adaption Copyright (C) 2002 Chris Liechti and Steve Underwood

Blackfin adaption Copyright (C) 2008 Analog Devices, Inc.

GDBproxy comes with ABSOLUTELY NO WARRANTY; for details

use `--warranty' option. This is Open Source software. You are

welcome to redistribute it under certain conditions. Use the

'--copying' option for details.

Found USB cable: ICE-100B

ICE-100B firmware version is 2.0.7

IR length: 5

Chain length: 1

Device Id: 00000010100000000100000011001011 (0x028040CB)

  Manufacturer: Analog Devices, Inc. (0x0CB)

  Part(0):      SDU (0x2804)

  Stepping:     0

  Filename:     ./../share/urjtag/analog/sdu/sdu

warning:   bfin: no board selected, 3 parts are detected

warning:   bfin:   parts: [BF609 BF609] SDU

notice:    bfin: jc: waiting on TCP port 2001

notice:    bfin: jc:  (you must connect GDB before using jtag console)

notice:    bfin-gdbproxy: waiting on TCP port 2000

Follow-ups

--- Andrew McLachlan                                         2012-09-03 04:44:28

running under CMD (run As Administrator), I get similar results to Cygwin:

bfin-jtag:

jtag> cable probe

Found USB cable: ICE-100B

error: libusb error: libusb_open() failed: -12

bfin-gdbproxy:

Found USB cable: ICE-100B

error:     bfin: cable initialization failed

--- Mike Frysinger                                           2012-09-05 15:11:37

this is expected behavior documented in the wiki:

http://docs.blackfin.uclinux.org/doku.php?id=hw:jtag:ice100b#use_different_usb_pids_for_visualdsp_and_urjtag_gdbproxy

--- Andrew McLachlan                                         2012-09-06 08:12:22

I now understand the set-up. Sadly, this means that it isn't very straight-

forward to debug a CCES project and then swap to debugging a GNU project

without messing with drivers and jumpers.

--- Jie Zhang                                                2012-09-06 11:04:50

Not a bug.

--- Mike Frysinger                                           2012-09-06 13:26:14

yes, as long as the VDSP windows drivers use their own usb stack (rather than

the usermode usb driver), there's not much the open source side can do.  once

(if?) they convert to the usermode usb driver, then things will "just

work" with urjtag.

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

File Name     File Type     File Size     Posted By

No Files Were Found

  • Share
  • History
  • More