Stop guessing, start certifying. Learn how to use IC safety application notes to streamline your FMEDA and meet IEC 61508 and ISO 13849 standards with...
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
      New KCC Quiz AQQ299 about Opamp Open Loop Gain and LTspice

      A kind proposal from Al Butvidas 1. Quote of the month: " A good friend calls you in jail. A great friend bails you out of jail. Your best friend sits...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card

      Important: Read the blog first . The quiz questions are all based on the content from the blog: The Power Problem Inside Every AI Breakthrough Everyone...
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
    Master FPGA-Based DSP Design: The Complete Building Blocks Guide You Need to Read

    The Engineering Mind Blog on EngineerZone presents an exceptional five-part series titled " DSP Building Blocks " that walks engineers through the essential...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    PSM Integration for Enhanced Module Solutions in 48 V Data Centers

    The integration of the LTC2971 into quarter brick solutions for 48 V data centers enhances monitoring, control, and reliability by providing high precision...

EngineerZone
EngineerZone
Linux Distribution for Blackfin
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Linux Distribution for Blackfin
  • Processors & DSP
  • Software & Development Tools
  • Linux Distribution for Blackfin
  • Cancel
Linux Distribution for Blackfin
Documents [#7292] Blackfin GNU tool chain Eclipse plug-in reports "WARNING: The "Debug" Configuration may not build"
  • Q&A
  • Docs/FAQs
  • Members
  • Tags
  • Cancel
  • +Documents
  • +2013R1 Linux release for Blackfin: FAQ
  • +2013R1: FAQ
  • +AD5700: FAQ
  • +ADI test script: FAQ
  • +bf537 SPI Bus: FAQ
  • +BF609: FAQ
  • +BF70x processor: FAQ
  • +bfin-elf-libstdc++-4.3: FAQ
  • +bfin-elf: FAQ
  • +bfin-uclinux-libstdc++-4.3: FAQ
  • +Blackfin Linux Projects: FAQ
  • +Blackinfin Linux: FAQ
  • +build toolchain: FAQ
  • +CPLB fault or SIGABRT: FAQ
  • +DAS U-BOOT FOR BLACKFIN: FAQ
  • +Default ADI release: FAQ
  • +Flash the uImage into Flash: FAQ
  • +gas test: FAQ
  • +gcc-4.3 ICEs: FAQ
  • +gcc.c-torture/execute/memset-2.c: FAQ
  • +gcc.dg/trampoline-1.c test: FAQ
  • +gcc/g++ test: FAQ
  • +gcc/g++ testcase: FAQ
  • +GDB commands: FAQ
  • +gdb.base/sigall.exp: FAQ
  • +gdb.cp/userdef.exp: FAQ
  • +gdb.gdbtk/c_variable.exp: FAQ
  • +GDB: FAQ
  • +gdb: symbol: FAQ
  • +gdbproxy: FAQ
  • +GNU TOOLCHAIN: FAQ
  • +How to load Linux: FAQ
  • +ldr-utils: FAQ
  • +libstdc++-4.3 21_strings/basic_string/capacity/char/18654.cc test: FAQ
  • +LOOP: FAQ
  • +mcpu: FAQ
  • +Parent Document for U-Boot Bug Archive: FAQ
  • +Parent Document for U-Boot Bug Forum Archive: FAQ
  • -Parent for all content moved from GNU Archive: FAQ
    • [#7290] Blackfin GNU tool chain Eclipse plug-in does not support ADSP-BF60x
    • [#7291] Blackfin GNU tool chain Eclipse plug-in does not specify -mcpu for Assembly source
    • [#7292] Blackfin GNU tool chain Eclipse plug-in reports "WARNING: The "Debug" Configuration may not build"
    • [#7293] Blackfin GNU tool chain Eclipse plug-in reports "This discovery method is deprecated" when used with Juno Release
    • [#7299] Blackfin GNU tool chain Eclipse Memory Mapped Registers View plug-in uses outdated proc files and does not support ADSP-BF60x
    • [#7300] kernel build with busybox 1.20 by trunk head toolchain and uClibc 0.9.33.2 boot up fails
    • [#7305] bfin-jtag.exe and bfin-gdbproxy.exe do not work on Windows
    • [#7313] bfin-gdbproxy crashes when attempting to load an executable on Windows
    • [#7317] GCC should generate code for Core 0 by default
    • [#7318] Ensure that -mmulticore -mcore0 is set on Eclipse ADSP-BF561/BF60x project creation
  • +prepare_target_solibs: FAQ
  • +SDP-B: FAQ
  • +signal 11: FAQ
  • +sim binutils: FAQ
  • +SPI eeprom: FAQ
  • +svn head u-boot build: FAQ
  • +test libmudflap: FAQ
  • +toolchain-regtest -r: FAQ
  • +toolchain-regtest: FAQ
  • +trunk head gdbproxy: FAQ
  • +trunk toolchain: FAQ
  • +u-boot with UART: FAQ
  • +u-boot: FAQ
  • +uClinux kernel: FAQ
  • +uClinux: FAQ
  • +Upgrade from 3801 to 3852: FAQ
  • +VDSP: FAQ

[#7292] Blackfin GNU tool chain Eclipse plug-in reports "WARNING: The "Debug" Configuration may not build"

[#7292] Blackfin GNU tool chain Eclipse plug-in reports "WARNING: The "Debug" Configuration may not build"

Submitted By: Andrew McLachlan

Open Date

2012-08-27 06:59:30     Close Date

2012-08-30 08:55:14

Priority:

Medium     Assignee:

Andrew McLachlan

Board:

N/A     Silicon Revision:

Resolution:

Fixed     Fixed In Release:

N/A

Processor:

ALL     

Host Operating System:

All

toolchain rev.:

    kernel rev.:

State:

Closed     Found In Release:

2012R1

Is this bug repeatable?:

N/A     

Summary: Blackfin GNU tool chain Eclipse plug-in reports "WARNING: The "Debug" Configuration may not build"

Details:

1, Install the Blackfin GNU tool chain Eclipse plug-ins into Juno

2, Create a new "Blackfin Linux FDPIC GNU Toolchain (bfin-linux-uclibc)" project for BF538

3, Build the project

**** Build of configuration Debug for project test ****

****  WARNING: The "Debug" Configuration may not build  ****

****  because it uses the "Blackfin Linux FDPIC GNU Toolchain (bfin-linux-uclibc)"  ****

****  tool-chain that is unsupported on this system.  ****

****  Attempting to build...  ****

make all

'Building file: ../system/adi_initialize.c'

'Invoking: Blackfin FDPIC C Compiler'

bfin-linux-uclibc-gcc -D_DEBUG -I"C:\Users\amclach\Desktop\CCES Workspace\test\system" -O0 -g3 -Wall -c -fmessage-length=0 -mcpu=bf549m-any -MMD -MP -MF"system/adi_initialize.d" -MT"system/adi_initialize.d" -o "system/adi_initialize.o" "../system/adi_initialize.c"

'Finished building: ../system/adi_initialize.c'

' '

'Building file: ../src/test.c'

'Invoking: Blackfin FDPIC C Compiler'

bfin-linux-uclibc-gcc -D_DEBUG -I"C:\Users\amclach\Desktop\CCES Workspace\test\system" -O0 -g3 -Wall -c -fmessage-length=0 -mcpu=bf549m-any -MMD -MP -MF"src/test.d" -MT"src/test.d" -o "src/test.o" "../src/test.c"

'Finished building: ../src/test.c'

' '

'Building target: test'

'Invoking: Blackfin FDPIC C Linker'

bfin-linux-uclibc-gcc -mcpu=bf549m-any -o "test"  ./system/adi_initialize.o  ./src/test.o  

'Finished building target: test'

' '

The issue is that the `bfin-linux-uclibc-ldr` command has not been filled in for the Blackfin Loader Tools Settings.

Workaround: add bfin-linux-uclibc-ldr explicitly to command entry box.

Additional: the Loader settings are not necessarily needed for this type of project set-up.

Ideally, we'd have an "Artifact type: Loader file" and make visible|enable/invisible|disable

the Loader tools settings according to the Artifact selection.

Follow-ups

--- Andrew McLachlan                                         2012-08-30 09:53:26

  Fixed in Blackfin GNU tool chain Eclipse plug-in v1.0.6.

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

File Name     File Type     File Size     Posted By

No Files Were Found