Getting Started with SDP-B using GCC toolchain:
The SDP (System Demonstration Platform) is a collection of controller boards, interposer boards, and daughter boards used for easy, low cost evaluation of ADI components and reference circuits. The controller boards provide a means of communicating to the PC from the system being evaluated or demonstrated. The SDP-B is a Blackfin, ADSP-BF527, based controller board. The SDP-B has on board JTAG, SDRAM, Flash memory and an LED making it an attractive package for those looking at low cost development platforms on Blackfin. This, combined with the open source GNU tool-chain and a low-cost emulator, reduces the cost factor significantly. SDP-B is available at: USD 99 [1] and the Low-cost emulator ICE-100B is available at: USD 150 [2], so one could kick-off 600Mhz Blackfin based development in just USD 250 [1] [2]. User can also opt between Windows or Linux host development platforms.
This article is a quick start guide for those who want to evaluate SDP-B in a GCC environment. A pdf version of the article is available as attachment. SDP-B Rev-B & Windows host is used for testing purpose. Refer to the reference section for various related links.
The SDP-B board features:
• Analog Devices ADSP-BF527 Blackfin processor
• Core performance up to 600 MHz
• 208-ball CSP-BGA package
• 24 MHz CLKIN oscillator
• 5 Mb of internal RAM memory
• 32 Mb flash memory
Numonyx M29W320EB (Rev B) or
Numonyx M25P32 (Rev 1.3)
• SDRAM memory
Micron MT48LC16M16A2P-6A - 16 Mb x 16 bits (256 Mb/32 MB)
• 3 × 120-pin small foot print connectors
Hirose FX8-120P-SV1(91), 120-pin header
• JTAG header footprint
• USB 2.0 device interface to host PC.
• Blackfin processor peripherals exposed
SPI
SPORT
TWI/I2C
GPIO
PPI
Asynchronous parallel
Timers
Development System:
SDP-B is a USB powered board [3], so one needs to have a USB mini-cable to power on the system. Typical development environment consists of a JTAG-based emulator and a GUI-based Debugger. ICE-100B is a low cost emulator from ADI that has direct support for the GCC toolchain. Another USB-cable is required to hook up the emulator to the JTAG connector in SDP-B board. Eclipse is an open source IDDE, which presents a complete debugger front-end to the developer. It can support almost any debugging requirement such as build code, execute, stop-at-breakpoints, single-step through code, view memory, MMRs etc.
GNU Debugger:
GDB (GNU Debugger) is the debugger utility for debugging applications built using GCC toolchain. User should be aware of the basic infrastructure that enables Eclipse to debug applications via gdb. A typical setup is given below.
ez.analog.com/.../5367.fd3855815812c79426e60914ed29fc2b.html
Eclipse needs to use gdbproxy in order to talk to the target device. Gdbproxy, as the name indicates, is a proxy server or a stub which in turn uses urJTAG software for the actual JTAG operations.
Installation of bare metal toolchain and Eclipse:
The latest release of the toolchain and the utilities (blackfin-toolchain-win32-) can be downloaded from the following link:
http://blackfin.uclinux.org/gf/project/toolchain/frs/
Once all files are installed, the emulator driver must be installed through *.inf file modifications. This file can be found in the toolchain installation path: “..\GNU Toolchain\2010R1\gnICE-drivers”. Next, modify the *.inf to include support for ICE-100B, as given below:
| Sample *.inf file |
|---|
|
;[Devices] |
Connecting JTAG first time:
- Connect emulator.
- Connect USB cable from emulator to PC.
- When PC asks for driver software, install the same from the path: “..\GNU Toolchain\2010R1\gnICE-drivers"
4. Restart PC.
5. Check whether the device is listed in the device manager such as below.
ez.analog.com/.../3583.871e44bc14912272a7e023f46baaeee5.html
Running gdbproxy:
Before any actual program can be debugged, the gdbproxy must successfully detect the jtag device. Gdbproxy maybe untouched after the connection is established. Example log is given below, after running this command:
| Running gdbproxy |
|---|
|
C:\Program Files\Analog Devices\GNU Toolchain\2010R1\elf\bin>bfin-gdbproxy.exe Remote proxy for GDB, v0.7.2, Copyright (C) 1999 Quality Quorum Inc. MSP430 adaption Copyright (C) 2002 Chris Liechti and Steve Underwood Blackfin adaption Copyright (C) 2008 Analog Devices, Inc. GDBproxy comes with ABSOLUTELY NO WARRANTY; for details use `--warranty' option. This is Open Source software. You are welcome to redistribute it under certain conditions. Use the '--copying' option for details. Found USB cable: ICE-100B ICE-100B firmware version is 2.0.6 IR length: 5 Chain length: 1 Device Id: 00100010011111100000000011001011 (0x227E00CB) Manufacturer: Analog Devices, Inc. (0x0CB) Part(0): BF527 (0x27E0) Stepping: 2 Filename: c:\program files\analog devices\gnu toolchain\svn-20101128\elf\b in\../share/urjtag/analog/bf527/bf527 warning: bfin: no board selected, BF527 is detected notice: bfin: jc: waiting on TCP port 2001 notice: bfin: jc: (you must connect GDB before using jtag console) notice: bfin-gdbproxy.exe: waiting on TCP port 2000 |
Creating project in Eclipse (only sample screenshots and explanations):
Start with new C project and appropriate toolchain:
Click on next until you arrive at processor definition:
A new project is now created with default file template. Remember that there are no low level drivers for stdio functions; you need to create your own implementation with newlib library for this. So delete the following code for now:
| stdio related code to be removed |
|---|
|
#include <stdio.h> puts("!!!Hello World!!!"); /* prints !!!Hello World!!! */ |
Right click on the project tab and build the code. Eclipse throws out verbose like below:
| build console output |
|---|
|
**** Build of configuration Debug for project SDP_test_project **** make all 'Building file: ../src/SDP_test_project.c' 'Invoking: Blackfin ELF C Compiler' bfin-elf-gcc -O0 -g3 -Wall -c -fmessage-length=0 -mcpu=bf527-any -MMD -MP -MF"src/SDP_test_project.d" -MT"src/SDP_test_project.d" -o"src/SDP_test_project.o" "../src/SDP_test_project.c" 'Finished building: ../src/SDP_test_project.c' ' ' 'Building target: SDP_test_project' 'Invoking: Blackfin ELF C Linker' bfin-elf-gcc -mcpu=bf527-any -o"SDP_test_project" ./src/SDP_test_project.o 'Finished building target: SDP_test_project' ' ' |
If the status is reporting as finished building, we have an executable ready for testing.
Debugging with Eclipse:
Next step is to create a debug configuration for the project. Right click on project and choose Debug Configurations. Create a new configuration under “bare metal application on JTAG device”. Go to Debugger tab and change the port number to 2000. Click on “apply” and “debug”. Sample screenshots are given below.
A screenshot for successful debug will look like below. Terminate with red-button and re-launch with Debug tab right click for every new build.
Explore the toolchain settings for project and the MMR window:
Minimal test of SDP-B hardware with GCC:
The following code blinks LED1 in the SDP:
| LED blink code | LED blink code contd... |
|---|---|
|
#include <cdefBF527.h> void writeToSdpLatch(unsigned char latchData); void flashLed(void); void waitMilliSec(void); void configEBIU(void); void configFlashEnable(void); #define PIN_PG0 0x0001 unsigned char latchValue = 0; int main() { configFlashEnable(); configEBIU(); while(1) { flashLed(); } return 0; } void configFlashEnable() { *pPORTGIO_DIR |= PIN_PG0; *pPORTGIO_SET = PIN_PG0; asm("ssync;"); latchValue = 0; } void configEBIU() { *pEBIU_AMGCTL = 0x00F9; *pEBIU_AMBCTL0 = 0x7BB07BB0; *pEBIU_AMBCTL1 = 0x7BB07BB0; asm("ssync;"); latchValue = 0; } |
void writeToSdpLatch(unsigned char latchData) { // write to latch (bank 2) *((unsigned char*)0x20200000) = latchData; asm("ssync;"); } void flashLed(void) { unsigned char i = 0; for (i=0; i<5; i++) { latchValue = latchValue | 0x08; writeToSdpLatch(latchValue); waitMilliSec(); latchValue = latchValue & 0xF7; writeToSdpLatch(latchValue); waitMilliSec(); } } void waitMilliSec() { int j = 0; for(j=0;j<1000000;j++) asm("NOP;"); } |
Creating LDR file:
Once the project has been debugged via emulator, one needs to create the corresponding LDR (Loader) file in order to use in a standalone system. A standalone system consists of a boot source, typically a non-volatile memory from where the LDR file is read by the on-chip BOOT-ROM in Blackfin. The BOOT-ROM copies the various code and data objects in to various memories available in the system. Once BOOT-ROM has finished this operation, it jumps to the start of application to perform further execution.
In GCC environment, this LDR file is created via ld-utils provided in “\GNU Toolchain\2010R1\elf\bin” folder in the installation directory. Command bfin-elf-ldr.exe along with its parameters needs to be run in order to burn the ldr in the correct way to the flash. For example, the following command operates on the executable named SDP_LED_BLINK and creates an LDR file called LEDblink.ldr for BF527 supporting a 16-bit Flash device.
| creating ldr file |
|---|
|
C:\Program Files\Analog Devices\GNU Toolchain\2010R1\elf\bin>bfin-elf-ldr.exe -T bf527 -v -c --bits 16 LEDblink.ldr SDP_LED_BLINK --bmode para Creating LDR LEDblink.ldr ... Adding DXE 'SDP_LED_BLINK' ... [jump block to 0xFFA00000] [ELF block: 1104 @ 0xFF800000] [ELF block: 1620 @ 0xFFA00000] OK! Done! |
Automating LDR creation with Eclipse
Create a new configuration under Run -> External Configuration, and appropriate parameters.
Add this tool to the Builder list so that Eclipse calls this automatically.
Upon successful build, eclipse throws the output as below:
Loading LDR file via urJTAG software:
Perform the following command sequence with urJTAG command prompt in order to load an ldr file. The tool supports auto-completion pre-load from history. Example sequence used for burning the LED_blink_ ldr:
| urJTAG command sequence |
|---|
|
C:\Program Files\Analog Devices\GNU Toolchain\2010R1\elf\bin>bfin-jtag.exe UrJTAG 0.10 #5733 Copyright (C) 2002, 2003 ETC s.r.o. Copyright (C) 2007, 2008, 2009 Kolja Waschk and the respective authors UrJTAG is free software, covered by the GNU General Public License, and you arewelcome to change it and/or distribute copies of it under certain conditions. There is absolutely no warranty for UrJTAG. warning: UrJTAG may damage your hardware! Type "quit" to exit, "help" for help. jtag> cable ICE-100B ICE-100B firmware version is 2.0.6 jtag> detect IR length: 5 Chain length: 1 Device Id: 00100010011111100000000011001011 (0x227E00CB) Manufacturer: Analog Devices, Inc. (0x0CB) Part(0): BF527 (0x27E0) Stepping: 2 Filename: c:\program files\analog devices\gnu toolchain\svn-20101128\elf\b in\../share/urjtag/analog/bf527/bf527 jtag> initbus bf527_sdp jtag> detectflash 0x20000000 Simultaneous Operation: Not supported block 0 unlocked C:\Program Files\Analog Devices\GNU Toolchain\2010R1\elf\bin> |
Notes:
[1] – Refer to SDP web page in Analog Devices website for up to date information on pricing and availability.
[2] - Refer to ICE 100B web page in Analog Devices website for up to date information on pricing and availability.
https://www.analog.com/en/processors-dsp/blackfin/emulator-100/processors/product.html
[3] - While the SDP can be powered over USB, when there are daughter boards attached the daughter boards should normally power the SDP. This is because of the variability of the USB power (+/-10% and current dependent on what other devices share the bus).
Reference:
SDP: https://www.analog.com/sdp
SDP Wiki: https://wiki.analog.com/resources/eval/sdp
Blackfin Processor: https://www.analog.com/blackfin
Open Source documentation: http://docs.blackfin.uclinux.org/
GCC bare metal documention: http://docs.blackfin.uclinux.org/doku.php?id=toolchain:bare_metal
GCC Files and development: http://blackfin.uclinux.org/gf/project/toolchain
Eclipse: http://www.eclipse.org/
Discussion Forums:
SDP: https://ez.analog.com/community/circuits_from_the_lab/sdp
Blackfin: https://ez.analog.com/community/dsp/blackfin-processors
Open Source development: https://ez.analog.com/community/dsp/open-source