Power Management Fundamentals II Session 5: Deeper Look into Power Protection

    When is the best time to discover your power circuit needs protection? Let's explore the use of some input protection and control options like ideal diodes...
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
      1. Quote of this month: " When I die, I want to die like my grandfather who died peacefully in his sleep. Not screaming like all the passengers in his...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: Too Much Chatter and Not Enough Talk - Learn the Benefits...
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
    Achieving Power Over Data with RS-485 Transceivers

    By Bryson Barney What if a single wire could carry both energy and information seamlessly—without either getting in the way? The future of connectivity...

     

    ​​Functional Safety: A Driver of “Shift Left”​

    By Richard Obrien The key to faster, safer product development is to start smart - not catch up hard. In this blog, we’ll explore how the "Shift Left...

    Latest Blogs

    • The 5 Advantages of Hardware Fault Tolerance
    • The Power Problem Inside Every AI Breakthrough: Part 1 of 3
    • Simplifying Stability with EVAL-KW4503Z: Part 1 of 3
    • Energy Transfer Considerations in Isolated SMPS: Part 2 of 4
    • Automating LTspice .NOISE Measurements with .STEP and .MEAS Directives: Part 2 of 3
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
Linux Distribution for Blackfin
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Linux Distribution for Blackfin
  • Processors & DSP
  • Software & Development Tools
  • Linux Distribution for Blackfin
  • Cancel
Linux Distribution for Blackfin
Documents 2007-04-03 05:21:47     SPI eeprom write read
  • Forums
  • Docs/FAQs
  • Members
  • Tags
  • Cancel
  • +Documents
  • +2013R1 Linux release for Blackfin: FAQ
  • +2013R1: FAQ
  • +AD5700: FAQ
  • +ADI test script: FAQ
  • +bf537 SPI Bus: FAQ
  • +BF609: FAQ
  • +BF70x processor: FAQ
  • +bfin-elf-libstdc++-4.3: FAQ
  • +bfin-elf: FAQ
  • +bfin-uclinux-libstdc++-4.3: FAQ
  • +Blackfin Linux Projects: FAQ
  • +Blackinfin Linux: FAQ
  • +build toolchain: FAQ
  • +CPLB fault or SIGABRT: FAQ
  • +DAS U-BOOT FOR BLACKFIN: FAQ
  • +Default ADI release: FAQ
  • +Flash the uImage into Flash: FAQ
  • +gas test: FAQ
  • +gcc-4.3 ICEs: FAQ
  • +gcc.c-torture/execute/memset-2.c: FAQ
  • +gcc.dg/trampoline-1.c test: FAQ
  • +gcc/g++ test: FAQ
  • +gcc/g++ testcase: FAQ
  • +GDB commands: FAQ
  • +gdb.base/sigall.exp: FAQ
  • +gdb.cp/userdef.exp: FAQ
  • +gdb.gdbtk/c_variable.exp: FAQ
  • +GDB: FAQ
  • +gdb: symbol: FAQ
  • +gdbproxy: FAQ
  • +GNU TOOLCHAIN: FAQ
  • How to get ssh server (dropbear) running on BF609 EZ BOARD using Blackfin ucLinux 2014R1-RC1
  • +How to load Linux: FAQ
  • +ldr-utils: FAQ
  • +libstdc++-4.3 21_strings/basic_string/capacity/char/18654.cc test: FAQ
  • +LOOP: FAQ
  • +mcpu: FAQ
  • +Parent Document for U-Boot Bug Archive: FAQ
  • +Parent Document for U-Boot Bug Forum Archive: FAQ
  • +Parent for all content moved from GNU Archive: FAQ
  • +prepare_target_solibs: FAQ
  • +SDP-B: FAQ
  • +signal 11: FAQ
  • +sim binutils: FAQ
  • -SPI eeprom: FAQ
    • 2007-04-03 05:21:47     SPI eeprom write read
  • +svn head u-boot build: FAQ
  • +test libmudflap: FAQ
  • +toolchain-regtest -r: FAQ
  • +toolchain-regtest: FAQ
  • +trunk head gdbproxy: FAQ
  • +trunk toolchain: FAQ
  • +u-boot with UART: FAQ
  • +u-boot: FAQ
  • +uClinux kernel: FAQ
  • +uClinux: FAQ
  • +Upgrade from 3801 to 3852: FAQ
  • +VDSP: FAQ

2007-04-03 05:21:47     SPI eeprom write read

2007-04-03 05:21:47     SPI eeprom write read

Richard Aldrich (UNITED KINGDOM)

Message: 23979    I'm using the latest SVN versions of uboot, toolchain and uclinux (updated and compiled yesterday).

I followed the document http://docs.blackfin.uclinux.org/doku.php?id=accessing_serial_nor_flash_with_u-boot

to attempt to write to SPI flash (ST M25P64). I call the eeprom write command, and it appears to works, then I read it back to another memory location.

However, when I do the memory compare, it says that 0 bytes are the same (output is something like:

cmp.b 0x1000000 0x2000000 $(filesize)

byte at 0x01000000 (0x40) != byte at 0x02000000 (0x00)

Total of 0 bytes were the same)

where 0x2000000 is the location I have read the eeprom to.

Does anyone have any ideas on what I should investigate next?

QuoteReplyEditDelete

2007-04-04 00:37:59     Re: SPI eeprom write read

Mike Frysinger (UNITED STATES)

Message: 24009    this is a custom board right ?  i would first verify memory is sane by using the u-boot "mtest" command ... then try writing out all like 0x00 and 0xFF to the flash and then read it back out and use md.b to verify the location you read back out matches

QuoteReplyEditDelete

2007-04-04 09:01:50     Re: SPI eeprom write read

Richard Aldrich (UNITED KINGDOM)

Message: 24039    Ok, I am now able to write to and read from the SPI memory (its on a BF 537-stamp board). My problem came down to the wire length / type that had been used to connect the memory to a header.

I am able to load the uImage and read it back, and boot it and this process works well. All the bytes are identical.

However, I now want to investigate booting the u-boot from SPI. What I understand is that I compile u-boot with the

#define BFIN_BOOT_MODE        BF537_SPI_MASTER_BOOT

in the file found at: u-boot/include/configs/bf537-stamp.h

I do this, and then I have written the u-boot.ldr image to the eeprom, at offset 0x0.

I then switch SW16 to 3, and power up. ...nothing happens, I don't get anything back in minicom.

Am I missing a stage along the way? Btw, the board is Rev 0.2

QuoteReplyEditDelete

2007-04-04 14:52:21     Re: SPI eeprom write read

Mike Frysinger (UNITED STATES)

Message: 24062    nope, the steps you've listed are correct ...

in order to take one step out of the equation though, you should try using one of our tested releases:

http://blackfin.uclinux.org/gf/project/u-boot/frs

we have a SPI LDR for u-boot there for the BF537-STAMP ... that should eliminate question of whether it's a software (compiling u-boot) or hardware (using correct settings)

QuoteReplyEditDelete

2008-04-01 10:20:03     Re: SPI eeprom write read

Hadi Boulfelfel (FRANCE)

Message: 53456    I think it's :  #define BFIN_BOOT_MODE        BF537_BOOT_SPI_MASTER     not     BF537_SPI_MASTER_BOOT

TranslateQuoteReplyEditDelete

2008-04-11 10:26:53     Re: SPI eeprom write read

Pafone Lee (CHINA)

Message: 54093    There is also a difference between the docs and the u-boot source code

in http://docs.blackfin.uclinux.org/doku.php?id=bootloaders:u-boot:release-notes:2007r1

<pre class="code">// ADSP-BF533

#define BF533_BYPASS_BOOT 0x0001

#define BF533_PARA_BOOT 0x0002

#define BF533_SPI_BOOT 0x0004 but in u-boot2008-R1-1.1.6  source code /include/configs/bf533-ezkit.h

#define BFIN_BOOT_MODE       BFIN_BOOT_BYPASS

I don't know whether it is a mistake.

TranslateQuoteReplyEditDelete

2008-04-11 11:58:54     Re: SPI eeprom write read

Mike Frysinger (UNITED STATES)

Message: 54096    there is no difference nor error with the documentation

you're comparing old release notes against a newer release.  that'll never work.

QuoteReplyEditDelete

  • Share
  • History
  • More