2008-08-07 06:03:44 data transfer
Pranay Upadhyay (INDIA)
Message: 60094
Hello sir,
I have compiled the u-boot 2008R1, and formed the uboot binary file .After loading the u-boot, I am trying to sending the file but data is not transmitting through the kermit in hyperterminal.The size of formed u-boot is 445 KB.Is it right.I have change only clock frequency 486 MHZ and data rate 115200 in bf-561 config.h file. Can you suggest me something about this?
-REGARDS
Pranay
QuoteReplyEditDelete
2008-08-07 15:23:00 Re: data transfer
Robin Getz (UNITED STATES)
Message: 60122
Pranay:
What is your hardware? Custom board or an EZkit? Default U-Boot images (to at least compare sizes) are avalible in the files section.
-Robin
2008-08-07 23:58:45 Re: data transfer
Message: 60130
My hardware is the Ez-kit BF561.But in my appliaction we need different CCLK and SCLK , so I have change in it.
-Regards
2008-08-08 10:53:57 Re: data transfer
Mike Frysinger (UNITED STATES)
Message: 60174
post the changes you have actually made to your board config file
then post the actual commands you are running and the errors you are seeing