Power Integrity for High Performance Measurement Systems

    Increasing data rates driven by AI workloads and the evolution from 5G to emerging 6G standards are placing new demands on electronic test and measurement...
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
      1.Quote of the month: "People Who Say They Sleep Like a Baby usually don't have one" - unknown 2. New quiz AQQ302 about Band Gap Reference Voltage...

    View All

    What's Brewing

      Read the Blog:  Simplified I/O: One Chip, Flexible Voltage Output, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Simplified I/O: One Chip, Flexible Voltage Outpu...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Game of DronesPart 1: How IMU Navigation Architectures Make or Break a Drone

    This article explains why industrial-grade UAVs require fundamentally different architectures than consumer drones. It highlights the need for inertial...

EngineerZone
EngineerZone
Linux Distribution for Blackfin
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Linux Distribution for Blackfin
  • Processors & DSP
  • Software & Development Tools
  • Linux Distribution for Blackfin
  • Cancel
Linux Distribution for Blackfin
Documents [#6285] MMC/SD can't work on bf537-stamp when either icache or dcache is off
  • Q&A
  • Docs/FAQs
  • Members
  • Tags
  • Cancel
  • +Documents
  • +2013R1 Linux release for Blackfin: FAQ
  • +2013R1: FAQ
  • +AD5700: FAQ
  • +ADI test script: FAQ
  • +bf537 SPI Bus: FAQ
  • +BF609: FAQ
  • +BF70x processor: FAQ
  • +bfin-elf-libstdc++-4.3: FAQ
  • +bfin-elf: FAQ
  • +bfin-uclinux-libstdc++-4.3: FAQ
  • +Blackfin Linux Projects: FAQ
  • +Blackinfin Linux: FAQ
  • +build toolchain: FAQ
  • +CPLB fault or SIGABRT: FAQ
  • +DAS U-BOOT FOR BLACKFIN: FAQ
  • +Default ADI release: FAQ
  • +Flash the uImage into Flash: FAQ
  • +gas test: FAQ
  • +gcc-4.3 ICEs: FAQ
  • +gcc.c-torture/execute/memset-2.c: FAQ
  • +gcc.dg/trampoline-1.c test: FAQ
  • +gcc/g++ test: FAQ
  • +gcc/g++ testcase: FAQ
  • +GDB commands: FAQ
  • +gdb.base/sigall.exp: FAQ
  • +gdb.cp/userdef.exp: FAQ
  • +gdb.gdbtk/c_variable.exp: FAQ
  • +GDB: FAQ
  • +gdb: symbol: FAQ
  • +gdbproxy: FAQ
  • +GNU TOOLCHAIN: FAQ
  • +How to load Linux: FAQ
  • +ldr-utils: FAQ
  • +libstdc++-4.3 21_strings/basic_string/capacity/char/18654.cc test: FAQ
  • +LOOP: FAQ
  • +mcpu: FAQ
  • -Parent Document for U-Boot Bug Archive: FAQ
    • [#5797] usb fails to work in latest u-boot 2009.11
    • [#6262] Default SPI flash device NO. is wrong in u-boot trunk for bf518-ezbrd
    • [#6285] MMC/SD can't work on bf537-stamp when either icache or dcache is off
    • [#6286] characters is not shown correctly in u-boot jtag console test
    • [#6302] reduse U-boot time
    • [#6303] reduse U-boot time
    • [#6804] 561 u-boot fails to run save after update now
    • [#6693] u-boot tools build fail
    • [#6809] build uboot tools fails when running toolchain buildscript now
    • [#7733] fatls show two lines of the same file
  • +Parent Document for U-Boot Bug Forum Archive: FAQ
  • +Parent for all content moved from GNU Archive: FAQ
  • +prepare_target_solibs: FAQ
  • +SDP-B: FAQ
  • +signal 11: FAQ
  • +sim binutils: FAQ
  • +SPI eeprom: FAQ
  • +svn head u-boot build: FAQ
  • +test libmudflap: FAQ
  • +toolchain-regtest -r: FAQ
  • +toolchain-regtest: FAQ
  • +trunk head gdbproxy: FAQ
  • +trunk toolchain: FAQ
  • +u-boot with UART: FAQ
  • +u-boot: FAQ
  • +uClinux kernel: FAQ
  • +uClinux: FAQ
  • +Upgrade from 3801 to 3852: FAQ
  • +VDSP: FAQ

[#6285] MMC/SD can't work on bf537-stamp when either icache or dcache is off

[#6285] MMC/SD can't work on bf537-stamp when either icache or dcache is off

Submitted By: Vivi Li

Open Date

2010-10-09 06:24:06    

Priority:

Low     Assignee:

Nobody

Category:

N/A     Fixed In Release:

N/A

Found In Release:

2010R1     Status:

Open

Board:

N/A     Processor:

BF537

Silicon Revision:

    Resolution:

Assigned (Not Start)

Is the bug repeatable?:

N/A     

Summary: MMC/SD can't work on bf537-stamp when either icache or dcache is off

Details:

MMC/SD can't work on bf537-stamp when either icache or dcache is off. This happens on both branch 2010r1 and trunk.

Last passed version is 2405; first failed version is 2411.

Bellow is the log:

--

U-Boot 2010.06-svn2467 (ADI-2010R1) (Oct 09 2010 - 14:29:38)

CPU:   ADSP bf537-0.2 (Detected Rev: 0.2) (bypass boot)

Board: ADI BF537 stamp board

       Support: http://blackfin.uclinux.org/

Clock: VCO: 400 MHz, Core: 200 MHz, System: 100 MHz

RAM:   64 MiB

Flash: 4 MiB

In:    serial

Out:   serial

Err:   serial

KGDB:  [on serial] ready

Net:   bfin_mac

Hit any key to stop autoboot:  0

bfin> icache on

Instruction Cache is ON

bfin> dcache off

Data (writethrough) Cache is OFF

bfin> set mmc_cs 4; set mmc_hz 20000000

bfin> printenv mmc_cs mmc_hz

mmc_cs=4

mmc_hz=20000000

bfin> mmc init

using spi0.4 at 20000000 hz with mode 3

mmc1 is available

bfin> fatls mmc 0

** Unable to use mmc 0:1 for fatls **

bfin>

--

Follow-ups

--- Sonic Zhang                                              2010-10-12 06:10:55

Hi Mike,

This bug was introduced by your latest change to the SPI DMA code before code

freeze. Could you take a look?

--- Mike Frysinger                                           2010-10-12 21:10:14

i'm not worried about cache off behavior.  does the issue only crop up when

caches are off ?

--- Vivi Li                                                  2010-10-13 23:52:32

Yes, it happens only when either one of the caches is off.

--- Sonic Zhang                                              2010-10-18 22:32:47

Hi Mike,

I guess the conclusion is that we should not worry about spi device with cache

off? If so, Vivi may disable SPI cases with cache off.

--- Mike Frysinger                                           2011-05-07 18:09:57

i dont think any customer will ever run with caches turned off since the speed

loss is so high.  it is useful to test with caches off as the increased latency

sometimes can detect race conditions in the code.

does this still fail with the newer mmc/spi driver ?  i think this test was run

against the old one which no longer exists ...

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

File Name     File Type     File Size     Posted By

No Files Were Found

  • Share
  • History
  • More