Stop guessing, start certifying. Learn how to use IC safety application notes to streamline your FMEDA and meet IEC 61508 and ISO 13849 standards with...
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
      New KCC Quiz AQQ299 about Opamp open looop gain and LTspice (a kind proposal from Al Butvidas)

      1. Quote of the month: " A good friend calls you in jail. A great friend bails you out of jail. Your best friend sits next to you and says 'wasn't that...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: Understanding Voltage Domain Isolation in Field-Bus...
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
    Master FPGA-Based DSP Design: The Complete Building Blocks Guide You Need to Read

    The Engineering Mind Blog on EngineerZone presents an exceptional five-part series titled " DSP Building Blocks " that walks engineers through the essential...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    PSM Integration for Enhanced Module Solutions in 48 V Data Centers

    The integration of the LTC2971 into quarter brick solutions for 48 V data centers enhances monitoring, control, and reliability by providing high precision...

EngineerZone
EngineerZone
Linux Distribution for Blackfin
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Linux Distribution for Blackfin
  • Processors & DSP
  • Software & Development Tools
  • Linux Distribution for Blackfin
  • Cancel
Linux Distribution for Blackfin
Documents How to make u-boot to do somthing automatically after booting
  • Q&A
  • Docs/FAQs
  • Members
  • Tags
  • Cancel
  • +Documents
  • +2013R1 Linux release for Blackfin: FAQ
  • +2013R1: FAQ
  • +AD5700: FAQ
  • +ADI test script: FAQ
  • +bf537 SPI Bus: FAQ
  • +BF609: FAQ
  • +BF70x processor: FAQ
  • +bfin-elf-libstdc++-4.3: FAQ
  • +bfin-elf: FAQ
  • +bfin-uclinux-libstdc++-4.3: FAQ
  • +Blackfin Linux Projects: FAQ
  • +Blackinfin Linux: FAQ
  • +build toolchain: FAQ
  • +CPLB fault or SIGABRT: FAQ
  • +DAS U-BOOT FOR BLACKFIN: FAQ
  • +Default ADI release: FAQ
  • +Flash the uImage into Flash: FAQ
  • +gas test: FAQ
  • +gcc-4.3 ICEs: FAQ
  • +gcc.c-torture/execute/memset-2.c: FAQ
  • +gcc.dg/trampoline-1.c test: FAQ
  • +gcc/g++ test: FAQ
  • +gcc/g++ testcase: FAQ
  • +GDB commands: FAQ
  • +gdb.base/sigall.exp: FAQ
  • +gdb.cp/userdef.exp: FAQ
  • +gdb.gdbtk/c_variable.exp: FAQ
  • +GDB: FAQ
  • +gdb: symbol: FAQ
  • +gdbproxy: FAQ
  • +GNU TOOLCHAIN: FAQ
  • +How to load Linux: FAQ
  • +ldr-utils: FAQ
  • +libstdc++-4.3 21_strings/basic_string/capacity/char/18654.cc test: FAQ
  • +LOOP: FAQ
  • +mcpu: FAQ
  • +Parent Document for U-Boot Bug Archive: FAQ
  • +Parent Document for U-Boot Bug Forum Archive: FAQ
  • +Parent for all content moved from GNU Archive: FAQ
  • +prepare_target_solibs: FAQ
  • +SDP-B: FAQ
  • +signal 11: FAQ
  • +sim binutils: FAQ
  • +SPI eeprom: FAQ
  • +svn head u-boot build: FAQ
  • +test libmudflap: FAQ
  • +toolchain-regtest -r: FAQ
  • +toolchain-regtest: FAQ
  • +trunk head gdbproxy: FAQ
  • +trunk toolchain: FAQ
  • +u-boot with UART: FAQ
  • -u-boot: FAQ
    • How to make u-boot to do somthing automatically after booting
  • +uClinux kernel: FAQ
  • +uClinux: FAQ
  • +Upgrade from 3801 to 3852: FAQ
  • +VDSP: FAQ

How to make u-boot to do somthing automatically after booting

Q:I want to make u-boot to do something automatically after power up, thinking about I am booting from a serial Flash of limited size, and want to read my kernel stored in the SD card in to RAM and boot it, how?

A: You can achieve this by customize the u-boot environment. type print to show all the envs.

take the current default setting for example, the sequence is like this:

bfin> print bootcmd

bootcmd=run ramboot

bfin> print run ramboot

## Error: "run" not defined

ramboot=tftp $(loadaddr) $(ramfile);run ramargs;run addip;bootm

the bootcmd get automatically runs after boots, fetch the uImage from tftp server, set kernel boot args, and run bootm.

so you can customize the bootcmd, do jobs including reading your flash contents to a RAM location, and bootm this RAM location.

  • Share
  • History
  • More
  • Cancel
 
Related Content
  • RE: Setting up Blackfin to be independent from the computer
    ADIApproved
    You can achieve this by customize the u-boot environment. type print to show all the envs. take the current default setting for example, the sequence is like this: bfin> print bootcmd bootcmd=run...
  • RE: Halt when starting kernel
    ADIApproved
    1, use the ADI default configuraion 2, from your description, PF0, PF1is used, then your setting of "console=ttyBF0" is correct. You are going to check it somewhere else, I would like to recommend you...
  • RE: unable to mount jffs2 file system in bf548
    ADIApproved
    Now let's try to boot from the uImage first, to boot from uImage, you need to clean up your u-boot environment first, take my u-boot env paste below for example, bootcmd is the command that get executed...
 
Related Content
  • RE: Setting up Blackfin to be independent from the computer
    ADIApproved
    You can achieve this by customize the u-boot environment. type print to show all the envs. take the current default setting for example, the sequence is like this: bfin> print bootcmd bootcmd=run...
  • RE: Halt when starting kernel
    ADIApproved
    1, use the ADI default configuraion 2, from your description, PF0, PF1is used, then your setting of "console=ttyBF0" is correct. You are going to check it somewhere else, I would like to recommend you...
  • RE: unable to mount jffs2 file system in bf548
    ADIApproved
    Now let's try to boot from the uImage first, to boot from uImage, you need to clean up your u-boot environment first, take my u-boot env paste below for example, bootcmd is the command that get executed...