Power Management Fundamentals II Session 4: Isolated Converters Explained

    What does isolation mean for power topologies? Let's review what galvanic isolation means and go through the terminology and standards. We'll explore isolation...
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
    • Maximize Your Power Regulator: Key Considerations for Thermal Performance
    View All Webinars
  • Community Hub

    Challenge Yourself!

      KCC's Quizzes AQQ296 about repairing an equation in a digital display

      1. Quote of this month: " When I die, I want to die like my grandfather who died peacefully in his sleep. Not screaming like all the passengers in his...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: Too Much Chatter and Not Enough Talk - Learn the Benefits...
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
    ​​Functional Safety: A Driver of “Shift Left”​

    By Richard Obrien The key to faster, safer product development is to start smart - not catch up hard. In this blog, we’ll explore how the "Shift Left...

     

    The 5 Advantages of Hardware Fault Tolerance

    In IEC 61508, HFT stands for “ H ardware F ault T olerance”. HFT of one or higher means that there is no single fault that will cause a safety function...

    Latest Blogs

    • The Power Problem Inside Every AI Breakthrough: Part 1 of 3
    • Simplifying Stability with EVAL-KW4503Z: Part 1 of 3
    • Energy Transfer Considerations in Isolated SMPS: Part 2 of 4
    • Automating LTspice .NOISE Measurements with .STEP and .MEAS Directives: Part 2 of 3
    • ​​Channel Specification: The Key to GMSL Compliance​
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
Linux Distribution for Blackfin
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Linux Distribution for Blackfin
  • Processors & DSP
  • Software & Development Tools
  • Linux Distribution for Blackfin
  • Cancel
Linux Distribution for Blackfin
Documents How can I flash the uImage into Flash and boot from it?
  • Forums
  • Docs/FAQs
  • Members
  • Tags
  • Cancel
  • +Documents
  • +2013R1 Linux release for Blackfin: FAQ
  • +2013R1: FAQ
  • +AD5700: FAQ
  • +ADI test script: FAQ
  • +bf537 SPI Bus: FAQ
  • +BF609: FAQ
  • +BF70x processor: FAQ
  • +bfin-elf-libstdc++-4.3: FAQ
  • +bfin-elf: FAQ
  • +bfin-uclinux-libstdc++-4.3: FAQ
  • +Blackfin Linux Projects: FAQ
  • +Blackinfin Linux: FAQ
  • +build toolchain: FAQ
  • +CPLB fault or SIGABRT: FAQ
  • +DAS U-BOOT FOR BLACKFIN: FAQ
  • +Default ADI release: FAQ
  • -Flash the uImage into Flash: FAQ
    • How can I flash the uImage into Flash and boot from it?
  • +gas test: FAQ
  • +gcc-4.3 ICEs: FAQ
  • +gcc.c-torture/execute/memset-2.c: FAQ
  • +gcc.dg/trampoline-1.c test: FAQ
  • +gcc/g++ test: FAQ
  • +gcc/g++ testcase: FAQ
  • +GDB commands: FAQ
  • +gdb.base/sigall.exp: FAQ
  • +gdb.cp/userdef.exp: FAQ
  • +gdb.gdbtk/c_variable.exp: FAQ
  • +GDB: FAQ
  • +gdb: symbol: FAQ
  • +gdbproxy: FAQ
  • +GNU TOOLCHAIN: FAQ
  • How to get ssh server (dropbear) running on BF609 EZ BOARD using Blackfin ucLinux 2014R1-RC1
  • +How to load Linux: FAQ
  • +ldr-utils: FAQ
  • +libstdc++-4.3 21_strings/basic_string/capacity/char/18654.cc test: FAQ
  • +LOOP: FAQ
  • +mcpu: FAQ
  • +Parent Document for U-Boot Bug Archive: FAQ
  • +Parent Document for U-Boot Bug Forum Archive: FAQ
  • +Parent for all content moved from GNU Archive: FAQ
  • +prepare_target_solibs: FAQ
  • +SDP-B: FAQ
  • +signal 11: FAQ
  • +sim binutils: FAQ
  • +SPI eeprom: FAQ
  • +svn head u-boot build: FAQ
  • +test libmudflap: FAQ
  • +toolchain-regtest -r: FAQ
  • +toolchain-regtest: FAQ
  • +trunk head gdbproxy: FAQ
  • +trunk toolchain: FAQ
  • +u-boot with UART: FAQ
  • +u-boot: FAQ
  • +uClinux kernel: FAQ
  • +uClinux: FAQ
  • +Upgrade from 3801 to 3852: FAQ
  • +VDSP: FAQ

How can I flash the uImage into Flash and boot from it?

Q: I understand for production I usually need to fill things into Flash file system like UBIFS or jffs2, but now, I just want a quick stand alone boot up to show my customer my demo, how should I do this?

A: You may flash the u-boot into Parallel Flash, and store the uImage into SD card. Here I will give an example based on BF609 EZ-BOARD and 2012R2 release.

The basic idea is, Flash the u-boot into Parallel Flash, customize the u-boot environment variable, to make the u-boot read the uImage into a RAM location from SD card, and then jump to the RAM location to boot the uImage.

Step 1: Flash the u-boot.

          i) download the tarball from https://blackfin.uclinux.org/gf/download/frsrelease/568/10222/u-boot-bf609-ezkit-2012R2-RC3.tar.bz2, extract it, file u-boot-bf609-ezkit-para-2012R2-RC3.ldr is what we want.

          ii) Flash the downloaded u-boot-bf609-ezkit-para-2012R2-RC3.ldr into parallel following https://docs.blackfin.uclinux.org/doku.php?id=toolchain:ldr-utils

          iii) after the Flashing is done, reset the board, you should see the u-boot UART console with minicom or windows hyperterminal etc with 57600-8-N-1 (make sure the boot mode of the board is set to Parallel Flash boot, position 1)

Step 2: Store the uImage into SD card

          i) download the uImage from https://blackfin.uclinux.org/gf/download/frsrelease/593/10293/uImage-bf609-ezkit-2012R2-RC5 and rename it to uImage for simplicity.

          ii)format a SD card into FAT (you may do this with a windows PC)

          iii)copy the above file uImage into the SD card FAT partition (still on a windows)

Step 3: Customize the u-boot environment

          In the u-boot console, run the following command    

         i) set mmcboot 'fatload mmc 0:1 0x1000000 /uimage; bootm'

         ii)set bootm 'run mmcboot'

         iii)save

Step4: Reset the board

          Reset the board, in a few seconds you should see it's booting into Linux.

  • Share
  • History
  • More