2008-02-20 03:00:16 Problems Building Konqueror
xabi romero (UNITED STATES)
Message: 51313 I am trying to build the konqueror web browser using the latest svn toolchain and uclinux-distr.
when i do "make" i obtaine the following error (see the attached file).
I have the qt library working and i and trying to build FDPIC konqueror with shared QT library
-Xabi
konqueror_make_error
QuoteReplyEditDelete
2008-02-20 11:17:38 Re: Problems Building Konqueror
Robin Getz (UNITED STATES)
Message: 51363 Xabi:
I think you might have better luck with the 2008R1 branches than using trunk.
-Robin
QuoteReplyEditDelete
2008-02-21 02:53:24 Re: Problems Building Konqueror
xabi romero (UNITED STATES)
Message: 51405
Thanks Robin
When you tell me that i might to use the 2008R1 branches, is for the Toolchain or for kernel + toolchain+distro.
thanks
-Xabi
QuoteReplyEditDelete
2008-02-21 03:03:17 Re: Problems Building Konqueror
Mike Frysinger (UNITED STATES)
Message: 51406 please review the FAQ about different versions:
http://docs.blackfin.uclinux.org/doku.php?id=faq
QuoteReplyEditDelete
2008-02-27 06:33:32 Re: Problems Building Konqueror
xabi romero (UNITED STATES)
Message: 51730
I am a new developper in uClinux, and i need more help.
Do anybody have problems building the konqueror explorer?
if somebody have build it, with wich toolchain, distribution and kernel?
thanks again.
QuoteReplyEditDelete
2008-02-27 11:08:13 Re: Problems Building Konqueror
Robin Getz (UNITED STATES)
Message: 51745 Xabi:
Have a look at:
http://docs.blackfin.uclinux.org/doku.php?id=uclinux-dist:browsers&s=konq#konqueror3_embedded
It should work with the 2008R1 toolchain and dist. If it doesn't, it is a bug (either in the docs, or in the source) - let us know, and we can fix either.
-Robin
QuoteReplyEditDelete
2008-02-28 02:45:57 Re: Problems Building Konqueror
xabi romero (UNITED STATES)
Message: 51760
Ok. i a going to try with the 2008R1 version.
The problem that i had, was maken with the latest svn dist. and toolchain, and i follow the documentation.
Thanks
-Xabi
QuoteReplyEditDelete
2008-03-04 11:37:29 Re: Problems Building Konqueror
xabi romero (UNITED STATES)
Message: 52036
Finally i download the2008R1 branches from kernel, uclinux and toolcahin, and when i try to make , i have obtained the same error (as you can see in the first message)
Do anybody try to compile the konqueror web browser?
thanks
-Xabi
QuoteReplyEditDelete
2008-03-13 10:02:26 Re: Problems Building Konqueror
Robin Getz (UNITED STATES)
Message: 52454 Xabi:
Sonic has done it, but I don't think updated things in awhile.
I think Mike was looking at integrating both Qt and Konqueror into trunk.
-Robin