2009-07-07 00:41:36 custom u-boot development query
Harbhajan Singh (INDIA)
Message: 76838
Hi ,
I am working with the BF527 Custom board. I am working on developing the custom u-boot. Boot mode Is the default mode (0001)
When I flashed the customized u-boot.ldr file into the flash it is not booting and I can not connect the jtag and see what is happening,
it says some error in opening the session. I need to spend some time in erasing the flash.
Is there any way to develop/get the the basic u-boot file for any custom board with blackfin processor specific like for BF533 and later I can verify the developed u-boot file using u-boot.bin fle and go command. And later I can flash the final u-boot into the custom board.
Are there any procedure and what things need to be taken care for smooth working with u-boot.
The flash chip on my custom hardware and the flash chip on the BF527 Ezkit are different.
Please advise
QuoteReplyEditDelete
2009-07-07 03:19:46 Re: custom u-boot development query
Yi Li (CHINA)
Message: 76841
This question need to be asked on the u-boot help forum. This is for Linux kernel and uclinux-dist.
For your question, please refer to:
docs.blackfin.uclinux.org/doku.php?id=bootloaders:u-boot:porting
-Yi