2008-01-02 14:07:42      JACK on Blackfin?

Steve Strobel (UNITED STATES)

Message: 49187    I have had several people recommend that I use JACK to handle the audio for my 4-input, 8-output AD1938 project (see <http://blackfin.uclinux.org/gf/project/uclinux-dist/forum/?action=ForumBrowse&forum_id=39&_forum_action=ForumMessageBrowse&thread_id=24943> for more info).  Has anyone tried JACK on Blackfin?  Any suggestions for simple wave/mp3 play/record utilities that work with it?

Thanks,

Steve

QuoteReplyEditDelete

2008-01-07 05:27:42     Re: JACK on Blackfin?

Yi Li (CHINA)

Message: 49314    According to the info: http://jackaudio.org/ - "JACK is a low-latency audio server, written for POSIX conformant operating systems such as GNU/Linux and Apple's OS X", it looks it should be able to be ported to blackfin uclinux.

QuoteReplyEditDelete

2008-01-30 12:22:44     Re: JACK on Blackfin?

Rob Clifford (UNITED STATES)

Message: 50386    Hi all,

I was wondering if anyone has successfully built JACK for the Blackfin?

I am about to attempt it but don't want to re-invent the wheel! Its also been quite a while since I did anything with uCLinux so gonna be a bit rusty.

I've read the 'Porting Apps to uClinux' in the docs section. Any pointers as to porting a daemon to uCLinux would be appreciated.

Thanks,

Rob

QuoteReplyEditDelete

2008-01-30 21:45:15     Re: JACK on Blackfin?

Yi Li (CHINA)

Message: 50410    We did not poring JACK before - but if you met any questions while porting, just post here.

Parents Reply Children
No Data