2011-10-11 03:52:36     cm-bf527 and mmc with spi

2011-10-11 03:52:36     cm-bf527 and mmc with spi

Mingeuk Kim (KOREA, REPUBLIC OF)

Message: 103784   

Hello,

I'm using CM-BF527 with EVAL-BF5xx board of Bluetechnix.

I wanted to use my sd card so that I followed this wep page

  docs.blackfin.uclinux.org/doku.php?id=linux-kernel:drivers:spi_mmc

After finishing kernel config, I modified linux-2.6.x/arch/blackfin/mach-bf527/boards/cm_bf527.c file like wep page.

#if defined(CONFIG_MMC_SPI) || defined(CONFIG_MMC_SPI_MODULE)

#define MMC_SPI_CARD_DETECT_INT IRQ_PF5

static int bfin_mmc_spi_init(struct device *dev,

        irqreturn_t (*detect_int)(int, void *), void *data)

{

        return request_irq(MMC_SPI_CARD_DETECT_INT, detect_int,

                IRQF_TRIGGER_FALLING, "mmc-spi-detect", data);

}

static void bfin_mmc_spi_exit(struct device *dev, void *data)

{

        free_irq(MMC_SPI_CARD_DETECT_INT, data);

}

static struct mmc_spi_platform_data bfin_mmc_spi_pdata = {

        .init = bfin_mmc_spi_init,

        .exit = bfin_mmc_spi_exit,

        .detect_delay = 100, // msecs

};

static struct bfin5xx_spi_chip  mmc_spi_chip_info = {

    .enable_dma = 0,

    .bits_per_word = 8,

};

#endif

#if defined(CONFIG_MMC_SPI) || defined(CONFIG_MMC_SPI_MODULE)

    {

        .modalias = "mmc_spi",

        .max_speed_hz = 20000000,     /* max spi clock (SCK) speed in HZ */

        .bus_num = 0,

        .chip_select = 4,

        .platform_data = &bfin_mmc_spi_pdata,    //

        .controller_data = &mmc_spi_chip_info,

        .mode = SPI_MODE_3,

    },

#endif

And I add #include <linux/spi/mmc_spi.h> because error was occurred without this file.

then my booting log is like this

--------------------------------------------------------------------------------------------------------

## Booting kernel from Legacy Image at 01000000 ...                           

   Image Name:   bf527-2.6.34.7-ADI-2010R1                                    

   Created:      2011-10-11   7:41:07 UTC                                     

   Image Type:   Blackfin Linux Kernel Image (gzip compressed)                

   Data Size:    2731973 Bytes = 2.6 MiB                                      

   Load Address: 00001000                                                     

   Entry Point:  0020e378                                                     

   Verifying Checksum ... OK                                                  

   Uncompressing Kernel Image ... OK                                          

Starting Kernel at = 0020e378                                                 

Linux version 2.6.34.7-ADI-2010R1 (rainbow@Rainbow) (gcc version 4.3.5 (ADI-2011

register early platform devices                                               

bootconsole [early_shadow0] enabled                                           

bootconsole [early_BFuart0] enabled                                           

early printk enabled on early_BFuart0                                         

Board Memory: 32MB                                                            

Kernel Managed Memory: 32MB                                                   

Memory map:                                                                   

  fixedcode = 0x00000400-0x00000490                                           

  text      = 0x00001000-0x0016c5c0                                           

  rodata    = 0x0016c5c0-0x001d2d88                                           

  bss       = 0x001d3000-0x001f6c04                                           

  data      = 0x001f6c04-0x0020a000                                           

    stack   = 0x00208000-0x0020a000                                           

  init      = 0x0020a000-0x004d1000                                           

  available = 0x004d1000-0x01f00000                                           

  DMA Zone  = 0x01f00000-0x02000000                                           

Hardware Trace Active and Enabled                                             

Boot Mode: 1                                                                  

Blackfin support (C) 2004-2010 Analog Devices, Inc.                           

Compiled for ADSP-BF527 Rev 0.1                                               

Warning: Compiled for Rev 1, but running on Rev 2                             

Blackfin Linux support by   blackfin.uclinux.org/                        

Processor Speed: 600 MHz core clock and 120 MHz System Clock                  

NOMPU: setting up cplb tables                                                 

Instruction Cache Enabled for CPU0                                            

  External memory: cacheable in instruction cache                             

Data Cache Enabled for CPU0                                                   

  External memory: cacheable (write-back) in data cache                       

Built 1 zonelists in Zone order, mobility grouping off.  Total pages: 7874    

Kernel command line: root=/dev/mtdblock0 rw clkin_hz=50000000 earlyprintk=seria0

PID hash table entries: 128 (order: -3, 512 bytes)                            

Dentry cache hash table entries: 4096 (order: 2, 16384 bytes)                 

Inode-cache hash table entries: 2048 (order: 1, 8192 bytes)                   

Memory available: 26524k/32768k RAM, (2844k init code, 1453k kernel code, 631k )

Hierarchical RCU implementation.                                              

NR_IRQS:159                                                                   

Configuring Blackfin Priority Driven Interrupts                               

I-pipe 1.14-02: pipeline enabled.                                             

console [ttyBF0] enabled, bootconsole disabled                                

console [ttyBF0] enabled, bootconsole disabled                                

Calibrating delay loop... 1191.93 BogoMIPS (lpj=2383872)                      

Security Framework initialized                                                

Mount-cache hash table entries: 512                                           

Blackfin Scratchpad data SRAM: 4 KB                                           

Blackfin L1 Data A SRAM: 16 KB (16 KB free)                                   

Blackfin L1 Data B SRAM: 16 KB (16 KB free)                                   

Blackfin L1 Instruction SRAM: 48 KB (41 KB free)                              

NET: Registered protocol family 16                                            

Blackfin DMA Controller                                                       

cm_init(): registering device resources                                       

bio: create slab <bio-0> at 0                                                 

SCSI subsystem initialized                                                    

bfin-spi bfin-spi.0: Blackfin on-chip SPI Controller Driver, Version 1.0, regs_7

NET: Registered protocol family 2                                             

IP route cache hash table entries: 1024 (order: 0, 4096 bytes)                

TCP established hash table entries: 1024 (order: 1, 8192 bytes)               

TCP bind hash table entries: 1024 (order: 0, 4096 bytes)                      

TCP: Hash tables configured (established 1024 bind 1024)                      

TCP reno registered                                                           

UDP hash table entries: 256 (order: 0, 4096 bytes)                            

UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)                       

NET: Registered protocol family 1                                             

I-pipe: Domain Xenomai registered.                                            

Xenomai: hal/blackfin started.                                                

Xenomai: scheduling class idle registered.                                    

Xenomai: scheduling class rt registered.                                      

Xenomai: real-time nucleus v2.5.3 (Hordes Of Locusts) loaded.                 

Xenomai: starting default API services.                                        

Xenomai: starting POSIX services.                                             

Xenomai: starting RTDM services.                                              

msgmni has been set to 51                                                     

io scheduler noop registered                                                  

io scheduler cfq registered (default)                                         

bfin-otp: initialized                                                         

Initializing RAINBOW gpio driver...                                           

bfin-uart: Blackfin serial driver                                             

bfin-uart.0: ttyBF0 at MMIO 0xffc00400 (irq = 29) is a BFIN-UART              

bfin-uart.1: ttyBF1 at MMIO 0xffc02000 (irq = 31) is a BFIN-UART              

brd: module loaded                                                            

Hardware Trace:                                                               

   0 Target : <0x0016a93c> { _dump_stack + 0x0 }                              

     Source : <0x00005ba6> { _peripheral_request + 0x252 } JUMP.L             

   1 Target : <0x00005b98> { _peripheral_request + 0x244 }                    

     Source : <0x00005a86> { _peripheral_request + 0x132 } IF !CC JUMP pcrel  

   2 Target : <0x00005a84> { _peripheral_request + 0x130 }                    

     Source : <0xffa01620> { _strcmp + 0x14 } RTS                             

   3 Target : <0xffa0161e> { _strcmp + 0x12 }                                 

     Source : <0xffa01616> { _strcmp + 0xa } IF !CC JUMP pcrel                

   4 Target : <0xffa0160c> { _strcmp + 0x0 }                                  

     Source : <0x0000579a> { _cmp_label + 0x1e } CALL pcrel                   

   5 Target : <0x0000577c> { _cmp_label + 0x0 }                               

     Source : <0x00005a80> { _peripheral_request + 0x12c } JUMP.L             

   6 Target : <0x00005a78> { _peripheral_request + 0x124 }                    

     Source : <0x000059c6> { _peripheral_request + 0x72 } IF !CC JUMP pcrel   

   7 Target : <0x0000597a> { _peripheral_request + 0x26 }                     

     Source : <0x00005974> { _peripheral_request + 0x20 } IF CC JUMP pcrel    

   8 Target : <0x00005970> { _peripheral_request + 0x1c }                     

     Source : <0x00005962> { _peripheral_request + 0xe } IF CC JUMP pcrel     

   9 Target : <0x00005954> { _peripheral_request + 0x0 }                      

     Source : <0x00005c10> { _peripheral_request_list + 0x24 } JUMP.L         

  10 Target : <0x00005c00> { _peripheral_request_list + 0x14 }                

     Source : <0x00005c18> { _peripheral_request_list + 0x2c } IF !CC JUMP pcre)

  11 Target : <0x00005c14> { _peripheral_request_list + 0x28 }                

     Source : <0x0000596e> { _peripheral_request + 0x1a } RTS                 

  12 Target : <0x00005966> { _peripheral_request + 0x12 }                     

     Source : <0x00005b38> { _peripheral_request + 0x1e4 } JUMP.S             

  13 Target : <0x00005b30> { _peripheral_request + 0x1dc }                    

     Source : <0xffa0169c> { _strncpy + 0x40 } RTS                            

  14 Target : <0xffa01696> { _strncpy + 0x3a }                                

     Source : <0xffa0167e> { _strncpy + 0x22 } IF CC JUMP pcrel               

  15 Target : <0xffa01674> { _strncpy + 0x18 }                                

     Source : <0xffa01670> { _strncpy + 0x14 } IF CC JUMP pcrel               

Stack info:                                                                   

SP: [0x0101be10] <0x0101be10> /* kernel dynamic memory */                    

FP: (0x0101bf84)                                                             

Memory from 0x0101be10 to 0101c000                                           

0101be10:[012b642c] 00005baa  00000028  00008228  0137b260  000abce2  012b642c

0101be30: 00000519  0000ffff  013f8500  00005c14  0016cf2c  001f8844  001f84a0

0101be50: 00000000  001a2964  0016cf2c  000abc02  00000008  01012928  0016a360

0101be70: 001f84dc  0101befc  00202e80  001f84b0  00000517  013f8500  000ac5c6

0101be90:<000f2074> 001f84a8  001f4828  00202e80  001f84dc  0101befc  00202e80

0101beb0: 00000001  010121c4  00025ea8  000ac63a  000f21b4  001f84a8  00202e80

0101bed0: 001f84dc  00000000  0101bedc  013f8500 <000f19f4> 000f2150  00202408

0101bef0: 00000000  ff0a0210  000d565e  010055d8  01035150  000f1f4e  0021f130

0101bf10: 00000000  00000001  000f13f2  0101bf3c  000f142c  000f2150  000f144a

0101bf30: 00000001  00012b74  0019f0b4  001a2954  0021695c  000f23e8  0021f130

0101bf50: 00202e80  00000000  00000000  00000007  00000001  001b28c8 <0021696c>

0101bf70: 001d300c  001d0000  00000000  00000000  001d300c (00000000)<00001028>>

0101bf90: 00004000  00004000  000332c4  001fa764  00000001  00000000  0020a134

0101bfb0: 0021f184  00000000  00000000  00000000  00000000  0021ef58  0021ef58

0101bfd0: 0020a1c0  0021ef58  0021ef58  00000000  00000000  00000000 <000014be>

0101bff0: 00000000  00000000  ffffffff  00000006                              

Return addresses in stack:                                                    

    address : <0x000f2074> { _really_probe + 0x60 }                           

    address : <0x000f19f4> { _bus_for_each_dev + 0x44 }                       

    address : <0x0021696c> { _bfin_mac_init + 0x10 }                          

   frame  1 : <0x00001028> { _do_one_initcall + 0x28 }                        

    address : <0x00001028> { _do_one_initcall + 0x28 }                        

    address : <0x000014be> { _kernel_thread_helper + 0x6 }                    

peripheral_request: Peripheral 40 function 1 is already reserved by mmc_spi ! 

bfin_mii_bus bfin_mii_bus.0: Requesting peripherals failed!                   

bfin_mii_bus: probe of bfin_mii_bus.0 failed with error -16                   

bfin_mac bfin_mac.0: Cannot get mii_bus!                                      

rtc-bfin rtc-bfin: rtc core: registered rtc-bfin as rtc0                      

bfin-wdt: initialized: timeout=20 sec (nowayout=0)                            

mmc_spi spi0.4: ASSUMING SPI bus stays unshared!                              

mmc_spi spi0.4: ASSUMING 3.2-3.4 V slot power                                 

mmc_spi spi0.4: SD/MMC host mmc0, no DMA, no WP, no poweroff                  

TCP cubic registered                                                          

NET: Registered protocol family 17                                            

rtc-bfin rtc-bfin: setting system clock to 1970-01-02 08:56:13 UTC (118573)   

dma_alloc_init: dma_page @ 0x0139a000 - 256 pages at 0x01f00000               

mmc_spi spi0.4: can't change chip-select polarity                             

Freeing unused kernel memory: 2844k freed                                     

                           _____________________________________              

        a8888b.           / Welcome to the uClinux distribution \             

       d888888b.         /       _     _                         \            

       8P"YP"Y88        /       | |   |_|            __  __ (TM)  |           

       8|o||o|88  _____/        | |    _ ____  _   _ \ \/ /       |           

       8'    .88       \        | |   | |  _ \| | | | \  /        |           

       8`._.' Y8.       \       | |__ | | | | | |_| | /  \        |           

      d/      `8b.       \      \____||_|_| |_|\____|/_/\_\       |           

     dP   .    Y8b.       \   For embedded processors including   |           

    d8:'  "  `::88b        \    the Analog Devices Blackfin      /            

   d8"         'Y88b        \___________________________________/             

  :8P    '      :888                                                          

   8a.   :     _a88P         For further information, check out:              

._/"Yaa_:   .| 88P|            -   blackfin.uclinux.org/                

\    YP"    `| 8P  `.          -   docs.blackfin.uclinux.org/           

/     \.___.d|    .'           -   www.uclinux.org/                     

`--..__)8888P`._.'  jgs/a:f    -   www.analog.com/blackfin              

                                                                              

Have a lot of fun...                                                          

                                                                              

                                                                              

                            powered by                                        

         ____  _            _            _           _                        

        | __ )| |_   _  ___| |_ ___  ___| |__  _ __ (_)_  __                  

        |  _ \| | | | |/ _ \ __/ _ \/ __| '_ \| '_ \| \ \/ /                  

        | |_) | | |_| |  __/ ||  __/ (__| | | | | | | |>  <                   

        |____/|_|\__,_|\___|\__\___|\___|_| |_|_| |_|_/_/\_\                  

                                                                              

                        www.bluetechnix.com                                        

                                                                              

                                                                              

BusyBox v1.16.2 (2011-10-10 15:12:21 KST) hush - the humble shell             

Enter 'help' for a list of built-in commands.                                 

--------------------------------------------------------------------------------------------------------

The error message can be removed by changing .chipselect = 4 to other numbers.

However I can't use sd card either and there was no mmcblk0 in /dev

1. What's the .chipselect = 4 and the error message means?

2. How could I use my sd card?

Any advise will be helpful to me.

Thanks in advance.

QuoteReplyEditDelete

2011-10-11 06:53:06     Re: cm-bf527 and mmc with spi

Sonic Zhang (CHINA)

Message: 103791   

1. chipselect is the SPI channel you select on your SPI MMC daughter board. If you change it to other number, make sure you also change the hardware on your SPI MMC board.

2. Insert your sd card into the sd slock on your SPI MMC board. mount the partition on your sd card as described in the wiki document.

QuoteReplyEditDelete

2011-10-20 04:52:08     Re: cm-bf527 and mmc with spi

Mingeuk Kim (KOREA, REPUBLIC OF)

Message: 104041   

Thank you for your advise.

In EVAL-BF5xx board, PH9/SPISEL5/ETxD2/HOST_D9/TACLK3 pin(55 of CM-BF527) can be used as chipselect of sd card.

So I changed chipselect to 5.

Then the booting log was like this.

------------------------------------------------------------------------------------------------------------------------------------------------

## Booting kernel from Legacy Image at 01000000 ...                           

   Image Name:   bf527-2.6.34.7-ADI-2010R1                                    

   Created:      2011-10-19  13:18:04 UTC                                     

   Image Type:   Blackfin Linux Kernel Image (gzip compressed)                

   Data Size:    3148216 Bytes = 3 MiB                                        

   Load Address: 00001000                                                     

   Entry Point:  0022034c                                                     

   Verifying Checksum ... OK                                                  

   Uncompressing Kernel Image ... OK                                          

Starting Kernel at = 0022034c                                                 

Linux version 2.6.34.7-ADI-2010R1 (rainbow@Rainbow) (gcc version 4.3.5 (ADI-2011

register early platform devices                                               

bootconsole [early_shadow0] enabled                                           

bootconsole [early_BFuart0] enabled                                           

early printk enabled on early_BFuart0                                         

Board Memory: 32MB                                                            

Kernel Managed Memory: 32MB                                                   

Memory map:                                                                   

  fixedcode = 0x00000400-0x00000490                                           

  text      = 0x00001000-0x00179848                                           

  rodata    = 0x00179848-0x001e4014                                           

  bss       = 0x001e5000-0x00208d30                                           

  data      = 0x00208d30-0x0021c000                                           

    stack   = 0x0021a000-0x0021c000                                           

  init      = 0x0021c000-0x0057d000                                           

  available = 0x0057d000-0x01f00000                                           

  DMA Zone  = 0x01f00000-0x02000000                                           

Hardware Trace Active and Enabled                                             

Boot Mode: 1                                                                  

Blackfin support (C) 2004-2010 Analog Devices, Inc.                           

Compiled for ADSP-BF527 Rev 0.1                                               

Warning: Compiled for Rev 1, but running on Rev 2                             

Blackfin Linux support by   blackfin.uclinux.org/                        

Processor Speed: 600 MHz core clock and 120 MHz System Clock                  

NOMPU: setting up cplb tables                                                 

Instruction Cache Enabled for CPU0                                            

  External memory: cacheable in instruction cache                             

Data Cache Enabled for CPU0                                                   

  External memory: cacheable (write-back) in data cache                       

Built 1 zonelists in Zone order, mobility grouping off.  Total pages: 7874    

Kernel command line: root=/dev/mtdblock0 rw clkin_hz=50000000 earlyprintk=seria0

PID hash table entries: 128 (order: -3, 512 bytes)                            

Dentry cache hash table entries: 4096 (order: 2, 16384 bytes)                 

Inode-cache hash table entries: 2048 (order: 1, 8192 bytes)                   

Memory available: 25836k/32768k RAM, (3460k init code, 1506k kernel code, 650k )

Hierarchical RCU implementation.                                              

NR_IRQS:159                                                                   

Configuring Blackfin Priority Driven Interrupts                               

I-pipe 1.14-02: pipeline enabled.                                             

console [ttyBF0] enabled, bootconsole disabled                                

console [ttyBF0] enabled, bootconsole disabled                                

Calibrating delay loop... 1191.93 BogoMIPS (lpj=2383872)                      

Security Framework initialized                                                

Mount-cache hash table entries: 512                                           

Blackfin Scratchpad data SRAM: 4 KB                                           

Blackfin L1 Data A SRAM: 16 KB (16 KB free)                                   

Blackfin L1 Data B SRAM: 16 KB (16 KB free)                                   

Blackfin L1 Instruction SRAM: 48 KB (41 KB free)                              

NET: Registered protocol family 16                                            

Blackfin DMA Controller                                                       

cm_init(): registering device resources                                       

bio: create slab <bio-0> at 0                                                 

SCSI subsystem initialized                                                    

bfin-spi bfin-spi.0: Blackfin on-chip SPI Controller Driver, Version 1.0, regs_7

NET: Registered protocol family 2                                             

IP route cache hash table entries: 1024 (order: 0, 4096 bytes)                

TCP established hash table entries: 1024 (order: 1, 8192 bytes)               

TCP bind hash table entries: 1024 (order: 0, 4096 bytes)                      

TCP: Hash tables configured (established 1024 bind 1024)                      

TCP reno registered                                                           

UDP hash table entries: 256 (order: 0, 4096 bytes)                            

UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)                       

NET: Registered protocol family 1                                             

I-pipe: Domain Xenomai registered.                                            

Xenomai: hal/blackfin started.                                                

Xenomai: scheduling class idle registered.                                    

Xenomai: scheduling class rt registered.                                      

Xenomai: real-time nucleus v2.5.3 (Hordes Of Locusts) loaded.                 

Xenomai: starting default API services.                                        

Xenomai: starting POSIX services.                                             

Xenomai: starting RTDM services.                                              

msgmni has been set to 50                                                     

io scheduler noop registered                                                  

io scheduler cfq registered (default)                                         

bfin-otp: initialized                                                         

Initializing RAINBOW gpio driver....                                          

bfin-uart: Blackfin serial driver                                             

bfin-uart.0: ttyBF0 at MMIO 0xffc00400 (irq = 29) is a BFIN-UART              

bfin-uart.1: ttyBF1 at MMIO 0xffc02000 (irq = 31) is a BFIN-UART              

brd: module loaded                                                            

bfin_mii_bus: probed                                                          

bfin_mac: attached PHY driver [Generic PHY] (mii_bus:phy_addr=0:00, irq=-1, mdc)

bfin_mac bfin_mac.0: Blackfin on-chip Ethernet MAC driver, Version 1.1        

bfin-wdt: initialized: timeout=20 sec (nowayout=0)                            

sdhci: Secure Digital Host Controller Interface driver                        

sdhci: Copyright(c) Pierre Ossman                                             

mmc_spi spi0.5: ASSUMING 3.2-3.4 V slot power                                 

mmc_spi spi0.5: SD/MMC host mmc0, no DMA, no WP, no poweroff                  

TCP cubic registered                                                          

NET: Registered protocol family 17                                            

dma_alloc_init: dma_page @ 0x01530000 - 256 pages at 0x01f00000               

mmc_spi spi0.5: can't change chip-select polarity                             

Freeing unused kernel memory: 3460k freed                                     

                           _____________________________________              

        a8888b.           / Welcome to the uClinux distribution \             

       d888888b.         /       _     _                         \            

       8P"YP"Y88        /       | |   |_|            __  __ (TM)  |           

       8|o||o|88  _____/        | |    _ ____  _   _ \ \/ /       |           

       8'    .88       \        | |   | |  _ \| | | | \  /        |           

       8`._.' Y8.       \       | |__ | | | | | |_| | /  \        |           

      d/      `8b.       \      \____||_|_| |_|\____|/_/\_\       |           

     dP   .    Y8b.       \   For embedded processors including   |           

    d8:'  "  `::88b        \    the Analog Devices Blackfin      /            

   d8"         'Y88b        \___________________________________/             

  :8P    '      :888                                                          

   8a.   :     _a88P         For further information, check out:              

._/"Yaa_:   .| 88P|            -   blackfin.uclinux.org/                

\    YP"    `| 8P  `.          -   docs.blackfin.uclinux.org/           

/     \.___.d|    .'           -   www.uclinux.org/                     

`--..__)8888P`._.'  jgs/a:f    -   www.analog.com/blackfin              

                                                                              

Have a lot of fun...                                                          

                                                                              

                                                                              

                            powered by                                        

         ____  _            _            _           _                        

        | __ )| |_   _  ___| |_ ___  ___| |__  _ __ (_)_  __                  

        |  _ \| | | | |/ _ \ __/ _ \/ __| '_ \| '_ \| \ \/ /                  

        | |_) | | |_| |  __/ ||  __/ (__| | | | | | | |>  <                   

        |____/|_|\__,_|\___|\__\___|\___|_| |_|_| |_|_/_/\_\                  

                                                                              

                        www.bluetechnix.com                                         

                                                                              

                                                                              

BusyBox v1.16.2 (2011-10-10 15:12:21 KST) hush - the humble shell             

Enter 'help' for a list of built-in commands.                                 

                                                                              

root:/> cat /proc/gpio                                                        

GPIO_5:         gpio-irq76              GPIO INPUT                            

GPIO_18:        bfin-spi                Peripheral                            

GPIO_19:        bfin-spi                Peripheral                            

GPIO_20:        bfin-spi                Peripheral                            

GPIO_23:        bfin-uart               Peripheral                            

GPIO_24:        bfin-uart               Peripheral                            

GPIO_28:        bfin-uart               Peripheral                            

GPIO_29:        bfin-uart               Peripheral                            

GPIO_30:        bfin_mac                Peripheral                            

GPIO_31:        bfin_mac                Peripheral                            

GPIO_32:        bfin_mac                Peripheral                            

GPIO_33:        bfin_mac                Peripheral                            

GPIO_34:        bfin_mac                Peripheral                            

GPIO_35:        bfin_mac                Peripheral                            

GPIO_36:        bfin_mac                Peripheral                            

GPIO_37:        bfin_mac                Peripheral                            

GPIO_38:        bfin_mac                Peripheral                            

GPIO_39:        bfin_mac                Peripheral                            

GPIO_40:        bfin_mac                Peripheral                            

GPIO_41:        mmc_spi                 Peripheral  

------------------------------------------------------------------------------------------------------------------------------------------------

I had inserted my sd card before booting was started.

When I used tcm-bf537 board, this sd card was working well.

  • Created
Was this helpful?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.