2011-06-15 04:04:49     mmc_spi and two chips on the spi bus.

2011-06-15 04:04:49     mmc_spi and two chips on the spi bus.

Dimitar Penev (BULGARIA)

Message: 101278   

Hi Guys,

I've noticed that the mmc_spi driver in 2010R1-RC5 doesn't suport two chips on the SPI bus.

I've saw that there is a pacth for this in the GIT called "move to mainline SPI locking API"

However applying it on 2010R1-RC5 seems to make our board unstable.

It seems it influence our nand flash as well somehow.

I have not investigated further, fortunately the second chip on the SPI bus is not inportant for us right now but still.

Is theer somone using mmc_spi with few chips on the same SPI bus based on 2010R1-RC5 distribution?

Thanks

Dimitar

QuoteReplyEditDelete

2011-06-15 04:50:56     Re: mmc_spi and two chips on the spi bus.

Sonic Zhang (CHINA)

Message: 101281   

That patch has nothing to do with your 2010R1-RC5 release. It is against kernel mainline tree.

Don't forget to select option "SPI Bus lock" under "SPI controller driver for ADI Blackfin" in your case.

QuoteReplyEditDelete

2011-06-15 07:51:22     Re: mmc_spi and two chips on the spi bus.

Dimitar Penev (BULGARIA)

Message: 101284   

Hi Sonic,

Having two SPI chips on the same bus confgured I got in the system log

mmc_spi spi0: can't share SPI bus

Based on this and what I have seen already discussed in the forum I concluded that the mmc_spi driver in the 2010R1-RC5

doesn't support SD card and another SPI chip sharing the SPI bus.

Does it mean I got confused and I will be OK if enable "SPI Bus lock".

And I don't need to patch anything?

Thanks

Dimitar

QuoteReplyEditDelete

2011-06-15 22:43:20     Re: mmc_spi and two chips on the spi bus.

Aaron Wu (CHINA)

Message: 101292   

Yes, no patch needed, please enable the "SPI Bus lock" as Sonic said and share us the feedback.

QuoteReplyEditDelete

2011-06-17 06:09:03     Re: mmc_spi and two chips on the spi bus.

Dimitar Penev (BULGARIA)

Message: 101380   

Hi Guys,

Thank you for the help!

Meanwhile I have noticed that I was using wrong SPI_MODE so I was reading garbage from the SD-card which the driver accepted happily.

I am curious why Linux driver doesn't confirm the CRC for the CSD data which standard defines.

Thanks

Dimitar

QuoteReplyEditDelete

2011-06-17 12:32:34     Re: mmc_spi and two chips on the spi bus.

Mike Frysinger (UNITED STATES)

Message: 101390   

that'd probably be a question to post to the linux-mmc@vger.kernel.org mailing list

  • Created
Was this helpful?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.