2011-06-14 08:14:33     Error in g_zero? (Gadget usb)

2011-06-14 08:14:33     Error in g_zero? (Gadget usb)

Morten Kvistgaard (DENMARK)

Message: 101253   

Hello there,

We're trying to implement some device side usb on BF526 ezbrd. We can make the g_serial work. But the MS Windows driver for that one has some serious faults. So we're trying to use libusb/winusb for the job instead.

We can make the g_zero (sink) work with winusb. (In a very boring unresponsive way.) But the loopback config in g_zero seems to be broken?

Here's the output:

============================================================

root:/> modprobe g_zero loopdefault=1

zero gadget: Gadget Zero, version: Cinco de Mayo 2008

zero gadget: zero ready

root:/> zero gadget: high speed config #2: loopback

zero gadget: can't loop ep6out to ep5in: -22

============================================================

I doubt it's supposed to say "can't loop ... " ? (And it's not sending back any output.)

We're using the 2010R2 uclinux, uboot etc.

Is there a trick or something to make the loopback work?

Does anyone have some good advice in regard to libusb/winusb and uclinux? Despite the whole ease-of-use and near defacto status in micro.c dev. it seems to frighteningly difficult to make it work with uclinux.

QuoteReplyEditDelete

2011-06-14 08:19:40     Re: Error in g_zero? (Gadget usb)

Morten Kvistgaard (DENMARK)

Message: 101254   

Edit: It's the 2010R1-RC5 uclinux ofc.

QuoteReplyEditDelete

2011-06-15 10:45:56     Re: Error in g_zero? (Gadget usb)

Morten Kvistgaard (DENMARK)

Message: 101288   

Meh, never mind. I've found something better than the g_zero loopback.

The g_serial has a "generic" mode which will remove all the fancy stuff. (Pure transfers back and forth)

You can load it with the following command:

modprobe g_serial use_acm=no

Unlike the ACM mode, the generic mode is very easy to communicate with through libs such as winusb.

QuoteReplyEditDelete

2011-06-17 02:14:09     Re: Error in g_zero? (Gadget usb)

Mike Frysinger (UNITED STATES)

Message: 101335   

ive opened a tracker item for the loopback mode:

  blackfin.uclinux.org/gf/tracker/6655

QuoteReplyEditDelete

  • Created
Was this helpful?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.