2011-05-25 19:46:19     bf5xx-i2s, bf5xx-i2s-pcm, bf5xx-sport and OSS: Point me in the right direction, please

2011-05-25 19:46:19     bf5xx-i2s, bf5xx-i2s-pcm, bf5xx-sport and OSS: Point me in the right direction, please

Reggy Perrin (UNITED STATES)

Message: 100841   

Hi folks,

I'd appreciate a pointer in the right direction, because I'm stumped as to where to look next.

Here's the situation:

    BF524 based system using a Wolfson WM8990 codec connected via a SPORT (using i2s driver)

    We're using a 3rd party library for an audio function we need, and that library is OSS based

    In preparation, we compiled in vrec/vplay (both OSS applications), and use them to validate the hardware/drivers to our system

    If I record something with:  vrec -w -t 4 -s 48000 -b 32 /tmp/test.wav, it sounds fine when played back with vplay

    However, when I use this audio library we acquired, it can't record/play the audio correctly (and we don't have the source code or support to diagnose)

I've tracked down one issue with this library related to the i2s communication.  In bf5xx-i2s.c, I had to change:

#define BF5XX_I2S_RATES (SNDRV_PCM_RATE_8000 | SNDRV_PCM_RATE_11025 |\

SNDRV_PCM_RATE_16000 | SNDRV_PCM_RATE_22050 | \

SNDRV_PCM_RATE_44100 | SNDRV_PCM_RATE_48000 | \

SNDRV_PCM_RATE_96000)

to:

#define BF5XX_I2S_RATES (SNDRV_PCM_RATE_48000)

Once I did this, the library started playing audio correctly.  However, recording is still very choppy.

Thinking that it was still a rate mismatch somehow, I chose to fix even more of the variables.  Currently, I have:

sound/soc/codec/wm8990.c:

    #define WM8990_RATES (SNDRV_PCM_RATE_48000)

    #define WM8990_FORMATS (SNDRV_PCM_FMTBIT_S32_LE)

sound/soc/blackfin/bf5xx-i2s.c:

    #define BF5XX_I2S_RATES (SNDRV_PCM_RATE_48000)

    #define BF5XX_I2S_FORMATS (SNDRV_PCM_FMTBIT_S32_LE)

sound/soc/blackfin/bf5xx-i2s-pcm.c:

    .formats = SNDRV_PCM_FMTBIT_S32_LE, 

Now when I record, I can actually confirm that it appears to be at the right frequency rate.

When I drop the rate down to 8KHz, I start to get SPORT TUVF errors, and the valid playback stopped.

To summarize:

    vrec/vplay work fine with the driver

    Custom OSS library can't record properly

What can I do to understand how the custom library is different, and how it is setting up the system differently?  Any pointers as to where to start?

TIA

RP

QuoteReplyEditDelete

2011-06-10 04:46:07     Re: bf5xx-i2s, bf5xx-i2s-pcm, bf5xx-sport and OSS: Point me in the right direction, please

Scott Jiang (CHINA)

Message: 101177   

Hi Reggy,

Your oss library is't compatible with ALSA. vrec/vplay can work fine with OSS emulation layer of ALSA.

Scott

  • Created
Was this helpful?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.