2011-05-12 09:32:39     ATAPI driver

2011-05-12 09:32:39     ATAPI driver

Philippe VERDIER (FRANCE)

Message: 100615   

Dear Sir,

We have developed a multi DSPs application used to analyze and record analog

signals on hard disk. Up to now the record process used a ADSP21065L that we

want to replace by a BF548.

The input data are read from a global shared SRAM memory connected to the BF548

via the external asynchronous memory interface. The hard disk is connected to

the BF548 via the ATAPI bus with the GPIO (not the asynchronous bus). For the

new design we are using uCLinux (release 2010R1) to develop our software

application. To access the global 32 bits SRAM memory we have developed a

simple char driver using DMA (the memory DMA stream 2 with the DMAC1 DMA

controller). To access the hard disk we are using the ATAPI driver of uCLinux

by opening directly the device (/dev/sda) because we have our own file system.

We have developed a test program in order to measure the throughput from the

global memory to the hard disk. The result are the following :

- read from external global SRAM to internal L1 buffer (DMA of 2048 longs) :

~13.96 MByte/s

- write to disk from L1 buffer (by block of 2048

longs) : 13 MByte/s

- read from SRAM to L1 buffer and write to disk (by blocks of 2048 longs) :

~7.36 MByte/s

NOTE : the last result is better than expected (arithmetic average of the 2

firsts throughputs) because the ATAPI driver must used some kinds of non

blocking DMA.

In order to optimize the record process we have modified our global shared

memory driver by adding a non-blocking read mode. In this mode the read

function returns as soon as the DMA from the global SRAM memory to a local

buffer is started.

At the beginning of the function we have also added a call to "wait_for_completion_interruptible"  in order to

wait the completion of the previous non blocking DMA transfer.

The operation is as follows:

- 2 buffers of 2048 longs are allocated into the internal L1 SRAM (one in L1A

bank and the other in L1B)

- a first blocking read into the global memory is started to fill the first

buffer

- we move the driver in non blocking mode

In a loop for a specified record size (1 GByte)

- non blocking read in the global memory to the free buffer

- write the full buffer on the hard disk

End of loop

- Wait for the end of the last global memory read

- write the last buffer on the hard disk

We expected to get a rate of around 13 MByte / s (the time of writing a block

of 2048 longs on the hard disk is comparable to the time of reading a block of

the same size in global memory).

The measured throughput is 8.77 MByte / s.

I send these informations to the Analog Device "processor support" team to ask if it is not an hardware conflict between the global memory DMA and the ATAPI DMA. Their response is no (see the attached file mailanalogpbdma).

I tried several uclinux kernel configuration but failed to improve the write speed to disk (preemption model changed, changed the kernel timer frequency, enabled "DMA priority over core activity"...).

We are using the DASP signal of the IDE bus to drive a LED wich indicates disk activity. When the data writen to the disk are read directly from external DDR or from internal L1 memory the LED is "on" during all the recording time. But if the data are first read from the global shared SRAM memory (with or without non blocking DMA) the activity LED  flash every few Hz (as if something is blocking the system while all this goes well if the two operations, read from shared memory to L1 and write from L1 to disk, are performed separately).

Is it possible that the ATAPI driver block the DMAC1 controller during disk access ?

Or are you another explanation and/or workarround ?

Regards,

Philippe VERDIER

ConfiguClinuxBF548.txt

mailanalogpbdma.txt

bootlinuxbf548.txt

QuoteReplyEditDelete

2011-06-01 04:30:49     Re: ATAPI driver

Sonic Zhang (CHINA)

Message: 100969   

All read/write operations to ATA registers are blocked in DMA mode, which may cost CPU overhead. But, data transfer between DRAM and ATA device is not blocked.

QuoteReplyEditDelete

2011-06-01 05:01:42     Re: ATAPI driver

Sonic Zhang (CHINA)

Message: 100970   

Could you try to run following 2 of your test cases concurrently against 2 different buffers in L1? The result can tell you if it is a L1 access conflict.

- read from external global SRAM to internal L1 buffer (DMA of 2048 longs) :

~13.96 MByte/s

- write to disk from L1 buffer (by block of 2048

longs) : 13 MByte/s

  • Created
Was this helpful?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.