2011-05-06 14:15:44     [GIT] Kernel Configuration Issue

2011-05-06 14:15:44     [GIT] Kernel Configuration Issue

James Kosin (UNITED STATES)

Message: 100491   

Anyone know where the kernel configurations went for the latest GIT tree.

All the vendor directories are missing the kernel configurations and 'make menuconfig' is complaining about the missing configuration stating that it is very difficult to get a good running kernel unless you know what you are doing.

*********************** NOTICE ****************************

There is no preset config for linux-2.6.x on platform AnalogDevices/BF518F-EZBRD.

If you choose to continue you will have to setup a linux

config from scratch which is a very complex task.

You will find it easier if you can copy a config.linux-2.6.x

from another platform that is similar.

If you know what you are doing press <ENTER> otherwise

Type ^C to abort.

Sorry, I don't know what I'm doing here....  But, I'm willing to learn.

Thanks in advance if I missed something.

QuoteReplyEditDelete

2011-05-06 17:34:06     Re: [GIT] Kernel Configuration Issue

Robert Cochran (UNITED STATES)

Message: 100492   

James,

By coincidence, I did a git clone today of uclinux-dist & linux.  All seems OK.   I'm assuming you cloned both the distribution and the kernel?

I saw the same problem you have once before because a checkout from svn had failed, and it didn't pull down the arch/blackfin tree under linux.  Do you have arch/blackfin under linux?  Do you find the defconfigs under arch/blackfin/configs?

Bob

QuoteReplyEditDelete

2011-05-11 09:42:39     Re: [GIT] Kernel Configuration Issue

James Kosin (UNITED STATES)

Message: 100579   

Thanks, I figured that out; but, git is complaining that I can't checkout the sources into another repository....

I'll have to try again later from scratch.  I'll post back later.

QuoteReplyEditDelete

2011-09-20 14:46:08     Re: [GIT] Kernel Configuration Issue

Armando Lopez (MEXICO)

Message: 103466   

i have the some problem:

*********************** NOTICE ****************************

There is no preset config for linux-2.6.x on platform Bluetechnix/TCM-BF518.

If you choose to continue you will have to setup a linux

config from scratch which is a very complex task.

You will find it easier if you can copy a config.linux-2.6.x

from another platform that is similar.

If you know what you are doing press <ENTER> otherwise

Type ^C to abort.

You could fix the problem?

thanks

QuoteReplyEditDelete

2011-09-20 23:02:28     Re: [GIT] Kernel Configuration Issue

Aaron Wu (CHINA)

Message: 103468   

Have you tried the comments from Rob?

QuoteReplyEditDelete

2011-09-21 15:34:33     Re: [GIT] Kernel Configuration Issue

Armando Lopez (MEXICO)

Message: 103482   

helIo!

I'm find the defconfigs under arch/blackfin/configs

but, I think it is problem to GIT tree or symbolic link

but  I can not find any example to help me

any suggestions?

regards

Armando

QuoteReplyEditDelete

2011-09-21 18:51:38     Re: [GIT] Kernel Configuration Issue

Armando Lopez (MEXICO)

Message: 103484   

Problem Solve!!

this problem is cause because uclinux-dist.git no bring the kernel!

to fix this i download "git clone git://git.bluetechnix.at/git/linux-kernel.git linux-kernel.git"

and rename to linux-2.6.x en move this file to uclinux-dist.git direction.

thanks

  • Created
Was this helpful?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.