2011-01-18 23:05:17     linephone compile failed

2011-01-18 23:05:17     linephone compile failed

david wang (CHINA)

Message: 97525   

Hi, all

First of all, My kernel version is 2009R1.1-RC4, toolchain is 2009R1.1-2。

When I  tried to compile the linephone project, I met  below errors

make[6]: Entering directory `/home/wangyixin/working/uclinux/trunk/uClinux-dist-2009R1.1-RC4/lib/readline/build-readline-6.0/shlib'

/bin/sh ../../readline-6.0/support/mkdirs /home/wangyixin/working/uclinux/trunk/uClinux-dist-2009R1.1-RC4/staging/usr/lib

/bin/sh ../../readline-6.0/support/shlib-install -O linux-uclibc -d /home/wangyixin/working/uclinux/trunk/uClinux-dist-2009R1.1-RC4/staging/usr/lib -b /home/wangyixin/working/uclinux/trunk/uClinux-dist-2009R1.1-RC4/staging/usr/bin -i "/usr/bin/install -c -m 644" libhistory.so.6.0

/bin/sh ../../readline-6.0/support/shlib-install -O linux-uclibc -d /home/wangyixin/working/uclinux/trunk/uClinux-dist-2009R1.1-RC4/staging/usr/lib -b /home/wangyixin/working/uclinux/trunk/uClinux-dist-2009R1.1-RC4/staging/usr/bin -i "/usr/bin/install -c -m 644" libreadline.so.6.0

../../libeXosip2-3.2.0/src/jevents.c: In function ‘eXosip_event_wait’:

../../libeXosip2-3.2.0/src/jevents.c:499: warning: unused variable ‘c’

../../libeXosip2-3.2.0/src/jevents.c:529: warning: unused variable ‘c’

../../libeXosip2-3.2.0/src/jevents.c:496: error: impossible constraint in ‘asm’

../../libeXosip2-3.2.0/src/jevents.c:526: error: impossible constraint in ‘asm’

install: you may need to run ldconfig

make[6]: Leaving directory `/home/wangyixin/working/uclinux/trunk/uClinux-dist-2009R1.1-RC4/lib/readline/build-readline-6.0/shlib'

make[5]: Leaving directory `/home/wangyixin/working/uclinux/trunk/uClinux-dist-2009R1.1-RC4/lib/readline/build-readline-6.0'

rm -f /home/wangyixin/working/uclinux/trunk/uClinux-dist-2009R1.1-RC4/staging/usr/lib/*.old

make[4]: Leaving directory `/home/wangyixin/working/uclinux/trunk/uClinux-dist-2009R1.1-RC4/lib/readline'

/home/wangyixin/working/uclinux/trunk/uClinux-dist-2009R1.1-RC4/tools/cross-fix-root

{standard input}: Assembler messages:

{standard input}:1846: Error: syntax error. Input text was cld.

{standard input}:1846: Error:

{standard input}:1846: Error: syntax error. Input text was rep.

{standard input}:1846: Error:

{standard input}:1846: Error: syntax error. Input text was stosl.

{standard input}:1846: Error:

{standard input}:1876: Error: syntax error. Input text was btsl.

{standard input}:1876: Error:

{standard input}:1978: Error: syntax error. Input text was cld.

{standard input}:1978: Error:

{standard input}:1978: Error: syntax error. Input text was rep.

{standard input}:1978: Error:

{standard input}:1978: Error: syntax error. Input text was stosl.

{standard input}:1978: Error:

{standard input}:2008: Error: syntax error. Input text was btsl.

{standard input}:2008: Error:

make[5]: *** [jevents.lo] Error 1

make[5]: *** Waiting for unfinished jobs....

../../libeXosip2-3.2.0/src/jauth.c:440: warning: ‘base64_encode_string’ defined but not used

../../libeXosip2-3.2.0/src/udp.c: In function ‘eXosip_read_message’:

../../libeXosip2-3.2.0/src/udp.c:1720: error: impossible constraint in ‘asm’

bfin-linux-uclibc-gcc -DHAVE_CONFIG_H -I. -I../../libeXosip2-3.2.0/src -I.. -I../../libeXosip2-3.2.0 -I../../libeXosip2-3.2.0/include -I/usr/include -I/usr/include -DEMBED -D__uClinux__ -I/home/wangyixin/working/uclinux/trunk/uClinux-dist-2009R1.1-RC4 -mcpu=bf527-0.1 -Wall -Wcast-align -Wchar-subscripts -Wformat -Winline -Wmissing-declarations -Wmissing-prototypes -Wnested-externs -Wpointer-arith -DOSIP_MT -DENABLE_DEBUG -g -DENABLE_TRACE -pipe -Wall -g -mcpu=bf527-0.1 -pthread -pipe -Wall -g -mcpu=bf527-0.1 -c ../../libeXosip2-3.2.0/src/jauth.c -o jauth.o >/dev/null 2>&1

{standard input}: Assembler messages:

{standard input}:6087: Error: syntax error. Input text was cld.

{standard input}:6087: Error:

{standard input}:6087: Error: syntax error. Input text was rep.

{standard input}:6087: Error:

{standard input}:6087: Error: syntax error. Input text was stosl.

{standard input}:6087: Error:

{standard input}:6134: Error: syntax error. Input text was btsl.

{standard input}:6134: Error:

make[5]: *** [udp.lo] Error 1

make[3]: Leaving directory `/home/wangyixin/working/uclinux/trunk/uClinux-dist-2009R1.1-RC4/lib/readline'

make[5]: Leaving directory `/home/wangyixin/working/uclinux/trunk/uClinux-dist-2009R1.1-RC4/lib/libeXosip/build-libeXosip2-3.2.0/src'

make[4]: *** [install-recursive] Error 1

make[4]: Leaving directory `/home/wangyixin/working/uclinux/trunk/uClinux-dist-2009R1.1-RC4/lib/libeXosip/build-libeXosip2-3.2.0'

make[3]: *** [all] Error 2

make[3]: Leaving directory `/home/wangyixin/working/uclinux/trunk/uClinux-dist-2009R1.1-RC4/lib/libeXosip'

make[2]: *** [libeXosip] Error 2

make[2]: Leaving directory `/home/wangyixin/working/uclinux/trunk/uClinux-dist-2009R1.1-RC4/lib'

make[1]: *** [all] Error 2

make[1]: Leaving directory `/home/wangyixin/working/uclinux/trunk/uClinux-dist-2009R1.1-RC4/lib'

make: *** [subdirs] Error 1

Does anyone else met the error? How to fix it , thanks!

QuoteReplyEditDelete

2011-01-19 00:01:56     Re: linephone compile failed

Aaron Wu (CHINA)

Message: 97527   

First better update to the latest release, second inphone need to be built as FDPIC format

QuoteReplyEditDelete

2011-01-19 00:18:36     Re: linephone compile failed

david wang (CHINA)

Message: 97528   

Hi, Aaron

  Thanks for your reply. I just enable the linephone project in uClinux-dist/config in make menuconfig, whithout any change to its default setting. Does it need any extra config?

QuoteReplyEditDelete

2011-01-19 00:30:54     Re: linephone compile failed

Aaron Wu (CHINA)

Message: 97529   

Yes, you need to compile it as FDPIC ,   customize application/lib option -->blackfin build options-->binary format

QuoteReplyEditDelete

2011-01-19 01:09:14     Re: linephone compile failed

david wang (CHINA)

Message: 97531   

Hi, Aaron

  I just checked the blackfin build option, it has been set as FDPIC already.

qqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqk x

  x x                             Binary format (FDPIC)  --->                                                                 x x

  x x                         --- Install ELF shared libraries                                                                x x

  x x                         [ ]   Cull unused ELF shared libraries                                                          x x

  x x                         [*] Install FLAT shared libraries                                                               x x

  x x                         (-g -O2) User/Lib CFLAGS                                                                        x x

  x x                         [ ] build with stack overflow checking                                                          x x

  x x                         [ ] build with mudflap pointer checking                                                         x x

  x x                         [ ] install uClinux-dist .config into /root                                                     x x

  x x                                                                       

QuoteReplyEditDelete

2011-01-19 01:16:35     Re: linephone compile failed

Aaron Wu (CHINA)

Message: 97532   

have you make clean before making again after change the binary format?

QuoteReplyEditDelete

2011-01-19 01:22:27     Re: linephone compile failed

david wang (CHINA)

Message: 97533   

Hi, Aaron,

I think it's not the issue of make clean,because I've set the app/lib as FDPIC from the beginning. For confirm, I make clean and make it again. the error is the same.

QuoteReplyEditDelete

2011-01-19 03:00:01     Re: linephone compile failed

Aaron Wu (CHINA)

Message: 97539   

I used to try the linphone on 2010 R1 and toolchain release days ago, did not meet compile problem.

QuoteReplyEditDelete

2011-01-21 03:21:31     Re: linephone compile failed

david wang (CHINA)

Message: 97598   

Hi, Aaron,

   I downloaded the 2010R1 and toolchain, but still failed when compie the linephone. the make output was save in the attached file. pls check it for us, thanks!

d400.log

QuoteReplyEditDelete

2011-01-21 03:23:41     Re: linephone compile failed

david wang (CHINA)

Message: 97599   

sorry, the attached file is update here, pls look at this one!

d400.log

QuoteReplyEditDelete

2011-01-21 09:47:55     Re: linephone compile failed

Mike Frysinger (UNITED STATES)

Message: 97603   

/home/luotong/working/workspace/blackfin/opt/uClinux/bfin-linux-uclibc/bin/../lib/gcc/bfin-linux-uclibc/4.3.5/../../../../bfin-linux-uclibc/bin/ld: cannot find /lib//libc.so.0

collect2: ld returned 1 exit status

make[5]: *** [libusbpp.la] Error 1

this error indicates your toolchain is not installed correctly.  are you sure you're PATH is pointing to the right place and your toolchain is installed properly ?

  • Created
Was this helpful?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.