2010-12-14 05:37:46     Problem with SDL and tslib

2010-12-14 05:37:46     Problem with SDL and tslib

Adrian Trüb (SWITZERLAND)

Message: 96705   

Hi

I have a problem with the tslib and sdl. The SDL_MOUSE.. event gives starnge coordinates. When I press on the screen the mouse cursor jumps to random positions.

I tested the Touchscreen with ts_test and it works fine. So the problem is just with the SDL.

=================================================

Toolchain: 2010RC4

uclinux-dist: 2010RC4

Board: BF548-EZKIT

----------------------------------------------------

env:

#SDL

export SDL_NOMOUSE=1

export SDL_MOUSEDEV=/dev/event1

export SDL_MOUSEDRV=TSLIB

#Touchscreen

export TSLIB_TSEVENTTYPE=INPUT

export TSLIB_FBDEVICE=/dev/fb0

export TSLIB_CONSOLEDEVICE=none

export TSLIB_CONFFILE=/etc/ts.conf

export TSLIB_CALIBFILE=/mnt/pointercal

export TSLIB_TSDEVICE=/dev/event1

export TSLIB_PLUGINDIR=/usr/lib/ts

----------------------------------------------------

ts.conf:

module_raw input

module pthres pmin=1

module variance delta=30

module dejitter delta=100

module linear

----------------------------------------------------

pointercal:

-7938 -121 32178844 279 -4718 18233074 65536

----------------------------------------------------

fb.modes: (fbset > fb.modes)

mode "480x272-0"

        geometry 480 272 480 272 24

        timings 0 0 0 0 0 0 0

        accel false

        rgba 8/16,8/8,8/0,0/0

endmode

=================================================

QuoteReplyEditDelete

2010-12-17 05:00:11     Re: Problem with SDL and tslib

Adrian Trüb (SWITZERLAND)

Message: 96842   

Ok, I got it.

I changed the Makefile from the SDL (uclinux-dist/lib/libsdl/Makefile):

CONF_OPTS = \

      --disable-arts \

      --disable-esd \

      --disable-pth \

      --disable-video-directfb \

      --disable-video-x11 \

      --enable-input-tslib

Now it works fine.

  • Created
Was this helpful?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.