2010-11-04 06:38:20     2010R1-RC2 serial / console problems

2010-11-04 06:38:20     2010R1-RC2 serial / console problems

Andreas Schallenberg (GERMANY)

Message: 95553   

I am using 2010R1-RC2 for the DNP/5370 board. For this, I re-used the board support file from a 2009-R1.1-RC4 installation without changes.

The first problem is that there is no console. I don't see the kernel booting. With a soft reset and post-mortem kernel debugging using u-boot I see the kernel boot messages:

U-Boot 2010.09 (ADI-2011R1-pre) (Nov 03 2010 - 18:11:38)

CPU:   ADSP bf537-0.3 (Detected Rev: 0.3) (bypass boot)

Board: DilNet DNP5370 BF537 board

Clock: VCO: 600 MHz, Core: 600 MHz, System: 120 MHz

RAM:   32 MiB

Flash: 4 MiB

In:    serial

Out:   serial

Err:   serial

Net:   MAC address is set.

bfin_mac

bfin> strings 0018289c 32768

<5>Linux version 2.6.34.7-ADI-2010R1ASc (aschallenberg@GWS026Linux) (gcc version 4.3.5 (ADI-2010R1-RC4) ) #23 Thu Nov 4 11:34:06 CET 2010

<6>bootconsole [early_shadow0] enabled

<6>Found mtd parition at 0x001bb000, (len=0x23d000), moving to 0x01cc3000

<6>Board Memory: 32MB

<6>Kernel Managed Memory: 32MB

<6>Memory map:

<6>  fixedcode = 0x00000400-0x00000490

<6>  text      = 0x00001000-0x0012a6a8

<6>  rodata    = 0x0012a6a8-0x0017c09c

<6>  bss       = 0x0017d000-0x0018ed24

<6>  data      = 0x0018ed24-0x001a4000

<6>    stack   = 0x001a2000-0x001a4000

<6>  init      = 0x001a4000-0x001bb000

<6>  available = 0x001bb000-0x01cc3000

<6>  rootfs    = 0x01cc3000-0x01f00000

<6>  DMA Zone  = 0x01f00000-0x02000000

<6>Hardware Trace Active and Enabled

<6>Boot Mode: 0

<6>Blackfin support (C) 2004-2010 Analog Devices, Inc.

<6>Compiled for ADSP-BF537 Rev 0.3

<6>Blackfin Linux support by   blackfin.uclinux.org/

<6>Processor Speed: 600 MHz core clock and 120 MHz System Clock

<7> boot memmap: 00000000001bb000 - 0000000001cc3000 (usable)

<7>On node 0 totalpages: 7363

<7>free_area_init_node: node 0, pgdat 0019fe84, node_mem_map 001bd000

<7>  DMA zone: 58 pages used for memmap

<7>  DMA zone: 0 pages reserved

<7>  DMA zone: 7305 pages, LIFO batch:0

<6>NOMPU: setting up cplb tables

<6>Instruction Cache Enabled for CPU0

<6>  External memory: cacheable in instruction cache

<6>Data Cache Enabled for CPU0

<6>  External memory: cacheable (write-back) in data cache

<4>Built 1 zonelists in Zone order, mobility grouping off.  Total pages: 7305

<5>Kernel command line: console=ttyBF0,115200 root=/dev/mtdblock3 rootfstype=romfs ro

<6>PID hash table entries: 128 (order: -3, 512 bytes)

<6>Dentry cache hash table entries: 4096 (order: 2, 16384 bytes)

<6>Inode-cache hash table entries: 2048 (order: 1, 8192 bytes)

<7>Kernel managed physical pages: 7363

<6>Memory available: 27392k/32768k RAM, (92k init code, 1189k kernel code, 487k data, 1024k dma, 292k reserved)

<6>Hierarchical RCU implementation.

<6>NR_IRQS:138

<6>Configuring Blackfin Priority Driven Interrupts

<6>Calibrating delay loop... 1196.03 BogoMIPS (lpj=2392064)

<4>Mount-cache hash table entries: 512

<6>Blackfin Scratchpad data SRAM: 4 KB

<6>Blackfin L1 Data A SRAM: 16 KB (16 KB free)

<6>Blackfin L1 Data B SRAM: 16 KB (16 KB free)

<6>Blackfin L1 Instruction SRAM: 48 KB (36 KB free)

<6>NET: Registered protocol family 16

<6>Blackfin DMA Controller

<6>DNP/5370: registering device resources

<6>DNP/5370: registering 2 SPI slave devices

<6>DNP/5370: MAC 02:80:ad:21:36:31

<4>bio: create slab <bio-0> at 0

<3>bfin-spi bfin-spi.0: No DMA channel specified

<4>bfin-spi: probe of bfin-spi.0 failed with error -2

<6>i2c-bfin-twi i2c-bfin-twi.0: Blackfin BF5xx on-chip I2C TWI Contoller, regs_base@ffc01400

<6>NET: Registered protocol family 2

<6>IP route cache hash table entries: 1024 (order: 0, 4096 bytes)

<6>TCP established hash table entries: 1024 (order: 1, 8192 bytes)

<6>TCP bind hash table entries: 1024 (order: 0, 4096 bytes)

<6>TCP: Hash tables configured (established 1024 bind 1024)

<6>TCP reno registered

<6>UDP hash table entries: 256 (order: 0, 4096 bytes)

<6>UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)

<6>NET: Registered protocol family 1

<6>JFFS2 version 2.2. (NAND) Copyright 2001-2006 Red Hat, Inc.

<6>ROMFS MTD (C) 2007 Red Hat, Inc.

<6>msgmni has been set to 53

<6>io scheduler noop registered

<6>io scheduler deadline registered (default)

<6>bfin-dma: initialized

<6>bfin-uart: Blackfin serial driver

<5>NULL pointer access

<0>Kernel OOPS in progress

<5>Deferred Exception context

<5>CURRENT PROCESS:

<5>

bfin>

The kernel bootargs are the same as used with the 2009R1.1-RC4 kernel. The 2009 kernel boots with a working console and I can log into that system.

TranslateQuoteReplyEditDelete

2010-11-04 06:43:40     Re: 2010R1-RC2 serial / console problems

Sonic Zhang (CHINA)

Message: 95554   

You should use 2010R1-RC2 uboot release as well other than

U-Boot 2010.09 (ADI-2011R1-pre) (Nov 03 2010 - 18:11:38)

QuoteReplyEditDelete

2010-11-04 06:44:21     Re: 2010R1-RC2 serial / console problems

Sonic Zhang (CHINA)

Message: 95555   

So does the 2010R1-RC4 toolchain.

QuoteReplyEditDelete

2010-11-04 10:41:09     Re: 2010R1-RC2 serial / console problems

Andreas Schallenberg (GERMANY)

Message: 95562   

Ok, the toolchain was 2010R1-RC4, but I am now using the u-Boot version you requested.

I found that the board config changed for the STAMP board from 2009R1.1 to 2010R1 release and I copied the serial settings from there. Now I am back with a system where I can log in.

Now I'm at the same state with the new kernel as I was with the 2009 one. No ethernet, but the PHY is detected correctly without my modification of bfin_mac.c. I'll now dig into that issue again and open a new thread if I'm unsuccessful.

Thanks again for your responses.

  • Created
Was this helpful?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.