2010-10-19 09:59:22     oops with rmmod of simple-gpio module

2010-10-19 09:59:22     oops with rmmod of simple-gpio module

Prasanth Rajagopal (INDIA)

Message: 94735   

I have just created a module project in eclipse & copied the contents of /drivers/char/simple-gpio.c to it. After inserting the module in the target running Linux, I try to remove it, but end up in Kernel OOps message as below. The code is a direct copy of the original driver. I am using uClinux-dist-2009R1.1-RC4. Any hints? I would also be happy to know how the OOps message was diagnosed (whoever replies).

- Prasanth.

>>>>>>>>.

root:/> cd root

root:~> ls

root:~> ls

simple_gpio_modified_driver.ko

root:~> insmod ./simple_gpio_modified_driver.ko

simple-gpio: now handling 160 GPIOs: 0 - 159

root:~> rmmod ./simple_gpio_modified_driver.ko

Instruction fetch misaligned address violation

- Attempted misaligned instruction cache fetch.

Kernel OOPS in progress

Deferred Exception context

CURRENT PROCESS:

COMM=rmmod PID=547

CPU = 0

TEXT = 0x03180000-0x031cd564        DATA = 0x003ac564-0x003afdcc

BSS = 0x003afdcc-0x00340000  USER-STACK = 0x0035fe90

return address: [0x000ca558]; contents of:

0x000ca530:  098b  e52a  002e  0c42  181e  ad52  0c42  181b

0x000ca540:  3045  300f  0062  e52a  0045  0c42  1807  ad52

0x000ca550:  0c42  1804  3045  300f [0062] e52a  0029  0c42

0x000ca560:  1821  ac92  0c42  181e  6c66  3045  300f  0127

ADSP-BF548-0.2 525(MHz CCLK) 131(MHz SCLK) (mpu off)

Linux version 2.6.28.10-ADI-2009R1.1

Built with gcc version 4.1.2 (ADI svn)

SEQUENCER STATUS:               Not tainted

SEQSTAT: 0000002a  IPEND: 8030  SYSCFG: 0006

  EXCAUSE   : 0x2a

  interrupts disabled

  physical IVG5 asserted : <0xffa00c20> { _evt_ivhw + 0x0 }

  physical IVG15 asserted : <0xffa00eb0> { _evt_system_call + 0x0 }

  logical irq   6 mapped  : <0xffa00350> { _timer_interrupt + 0x0 }

  logical irq  14 mapped  : <0x001193cc> { _bfin_rtc_interrupt + 0x0 }

  logical irq  48 mapped  : <0x000c99e8> { _bfin_serial_rx_int + 0x0 }

  logical irq  49 mapped  : <0x000c9974> { _bfin_serial_tx_int + 0x0 }

  logical irq  52 mapped  : <0x0011c3d0> { _bfin_twi_interrupt_entry + 0x0 }

  logical irq  53 mapped  : <0x0011c3d0> { _bfin_twi_interrupt_entry + 0x0 }

  logical irq  68 mapped  : <0x000ee674> { _bfin_ata_interrupt + 0x0 }

  logical irq  74 mapped  : <0x000fce08> { _bf5xx_nand_dma_irq + 0x0 }

  logical irq  76 mapped  : <0x0011798c> { _bfin_kpad_isr + 0x0 }

  logical irq  82 mapped  : <0x00112510> { _blackfin_interrupt + 0x0 }

  logical irq  85 mapped  : <0x0011510c> { _dma_controller_irq + 0x0 }

  logical irq 175 mapped  : <0x000d1ac0> { _smsc911x_irqhandler + 0x0 }

RETE: <0x00000000> /* Maybe null pointer? */

RETN: <0x00361d68> /* kernel dynamic memory */

RETX: <0x00000480> /* Maybe fixed code section */

RETS: <0x000ca5a0> { _dev_uevent + 0xc4 }

PC  : <0x000ca558> { _dev_uevent + 0x7c }

DCPLB_FAULT_ADDR: <0x03111374> /* kernel dynamic memory */

ICPLB_FAULT_ADDR: <0x000ca558> { _dev_uevent + 0x7c }

PROCESSOR STATE:

R0 : 002d4e00    R1 : 0031e000    R2 : 00000007    R3 : fffffffc

R4 : 0311e498    R5 : 001dd98c    R6 : 00000000    R7 : 0031e000

P0 : 0031e0f1    P1 : 0031e010    P2 : 656c706d    P3 : 00231ce4

P4 : 002d4e68    P5 : 002d4e00    FP : 00000001    SP : 00361c8c

LB0: 000af988    LT0: 000af988    LC0: 00000000

LB1: 000aeeae    LT1: 000aeea2    LC1: 00000000

B0 : 00000000    L0 : 00000000    M0 : 00000000    I0 : 00000001

B1 : 00000000    L1 : 00000000    M1 : 00000000    I1 : 0021c164

B2 : 00000000    L2 : 00000000    M2 : 00000000    I2 : ffffffff

B3 : 00000000    L3 : 00000000    M3 : 00000000    I3 : ffffffff

A0.w: 00000002   A0.x: 00000000   A1.w: 00000002   A1.x: 00000000

USP : 0035fc30  ASTAT: 00002000

Hardware Trace:

   0 Target : <0x00004d54> { _trap_c + 0x0 }

     Source : <0xffa0067e> { _exception_to_level5 + 0xba }

   1 Target : <0xffa005c4> { _exception_to_level5 + 0x0 }

     Source : <0xffa00474> { _bfin_return_from_exception + 0x18 }

   2 Target : <0xffa0045c> { _bfin_return_from_exception + 0x0 }

     Source : <0xffa00510> { _ex_trap_c + 0x6c }

   3 Target : <0xffa004a4> { _ex_trap_c + 0x0 }

     Source : <0xffa0074a> { _trap + 0x5a }

   4 Target : <0xffa006f0> { _trap + 0x0 }

     Source : <0x000ca556> { _dev_uevent + 0x7a } 0x300f

   5 Target : <0x000ca546> { _dev_uevent + 0x6a }

     Source : <0x000ca576> { _dev_uevent + 0x9a } JUMP.S

   6 Target : <0x000ca574> { _dev_uevent + 0x98 }

     Source : <0x000ca538> { _dev_uevent + 0x5c } IF !CC JUMP

   7 Target : <0x000ca532> { _dev_uevent + 0x56 }

     Source : <0x000ca520> { _dev_uevent + 0x44 } IF !CC JUMP

   8 Target : <0x000ca51a> { _dev_uevent + 0x3e }

     Source : <0x000ca504> { _dev_uevent + 0x28 } IF !CC JUMP

   9 Target : <0x000ca4fe> { _dev_uevent + 0x22 }

     Source : <0x000ca5a0> { _dev_uevent + 0xc4 } JUMP.S

  10 Target : <0x000ca5a0> { _dev_uevent + 0xc4 }

     Source : <0x000ab8ae> { _add_uevent_var + 0x6a } RTS

  11 Target : <0x000ab880> { _add_uevent_var + 0x3c }

     Source : <0x000af09c> { _vsnprintf + 0x7c } RTS

  12 Target : <0x000af08e> { _vsnprintf + 0x6e }

     Source : <0x000af2ae> { _vsnprintf + 0x28e } JUMP.S

  13 Target : <0x000af2aa> { _vsnprintf + 0x28a }

     Source : <0x000af20a> { _vsnprintf + 0x1ea } IF CC JUMP

  14 Target : <0x000af208> { _vsnprintf + 0x1e8 }

     Source : <0x000af08c> { _vsnprintf + 0x6c } IF CC JUMP

  15 Target : <0x000af06c> { _vsnprintf + 0x4c }

     Source : <0x000af2a8> { _vsnprintf + 0x288 } JUMP.S

Kernel Stack

Stack info:

SP: [0x00361d0c] <0x00361d0c> /* kernel dynamic memory */

FP: (0x00361d70)

Memory from 0x00361d00 to 00362000

00361d00: 00000000  00000000  00000000 [ffffffff] ffffffff  0021c164  00000001  0035

fc30

00361d20: 00000001  002d4e00  002d4e68  00231ce4  656c706d  0031e010  0031e0f1  0031

e000

00361d40: 00000000  001dd98c  0311e498  fffffffc  00000007  0031e000  002d4e00  002d

4e00

00361d60: 0031e0f1  00000006  00361d88  00361d88 (00000000)<000aba24> 03df7da0  0000

0000

00361d80: 0311f0a8 <0006d1d4> 0311e498  00361d8c  00361d8c  03111360  0031e000  03da

1d00

00361da0: 002d4e00  000cabc8  0311f0a8 <000cab82> 03da1d00  002d4e00  000cabc8  002d

4e68

00361dc0: 0022534c  0000009f  0000004c  00000000  03d874b0 <0006e4c4><000cabbc> 0022

58e0

00361de0: 032af400  002d4e00  00000000 <000cabe4> 002258e0 <000cabee><000cabf4> 002d

4e00

00361e00: 0022534c  0311eee0  00231f4c  000ca108 <0311e27e> 00000000 <00022a7c> 0fb0

0000

00361e20: 002253f8  0035fc3c <000cc5d8> 0022534c  0311eee0  00231f4c  002253f8  0000

00ac

00361e40: 00000002  00000068  00000001  001df0a4 <000cc676> 0022534c  0311eee0 <000c

bb34>

00361e60: 0311ef7c  0311eee0 <000cbb3a> 0311ef7c  0311eee0  00000000  ffffe000 <0311

e470>

00361e80: 0311ef7c  00000000 <00027b2e> 0311ef7c  00000081  003f9940  00000000  0000

0073

00361ea0: 00000000  706d6973  675f656c  5f6f6970  69646f6d  64656966  6972645f  0072

6576

00361ec0: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  0000

0000

00361ee0: 0311ef7c  00000880  00361eec  00000000  ffa00880  000279d0  00000081  0000

0000

00361f00: ffffe000  00000002  0000004c  0031c188  003f9cb8  0000fffe  00000002  0000

004c

00361f20: 00000002  0320c5d4  00008000  00000000  00000000  00362000  0320c5d4  0320

c5d4

00361f40:<0318a93c> ffa00f14  02003025  0313d7cf  0313e361  0313d7ce  0313e354  0000

0000

00361f60: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  0000

0000

00361f80: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  0000

0000

00361fa0: 00000000  00000000  00000000  003f9940  0035ffe6  0035fc30  0035fc3c  003a

d9d8

00361fc0: 0035fc54  003f9940  0031c408  0320c5c8  00000081  00000880  000001ad  0000

0002

00361fe0: 0000004c  00000002  0035fc6f  00000880  0035fc54  0035fc54  00000081  0000

0006

Return addresses in stack:

   frame  1 : <0x000aba24> { _kobject_uevent_env + 0x13c }

    address : <0x0006d1d4> { _sysfs_hash_and_remove + 0x34 }

    address : <0x000cab82> { _device_del + 0xf6 }

    address : <0x0006e4c4> { _sysfs_addrm_finish + 0x38 }

    address : <0x000cabbc> { _device_unregister + 0xc }

    address : <0x000cabe4> { _device_destroy + 0x1c }

    address : <0x000cabee> { _device_destroy + 0x26 }

    address : <0x000cabf4> { _device_destroy + 0x2c }

    address : <0x0311e27e> { :simple_gpio_modified_driver:_simple_gpio_remove + 0x3a

}

    address : <0x00022a7c> { _blocking_notifier_call_chain + 0x10 }

    address : <0x000cc5d8> { ___device_release_driver + 0x54 }

    address : <0x000cc676> { _driver_detach + 0x72 }

    address : <0x000cbb34> { _bus_remove_driver + 0x64 }

    address : <0x000cbb3a> { _bus_remove_driver + 0x6a }

    address : <0x0311e470> { :simple_gpio_modified_driver:_simple_gpio_exit + 0x18 }

    address : <0x00027b2e> { _sys_delete_module + 0x15e }

    address : <0x0318a93c> [ /bin/busybox + 0xa93c ]

Modules linked in: simple_gpio_modified_driver(-) hid_zpff hid_tmff ff_memless

Kernel panic - not syncing: Kernel exception

QuoteReplyEditDelete

2010-10-19 14:24:15     Re: oops with rmmod of simple-gpio module

Mike Frysinger (UNITED STATES)

Message: 94737   

simple_gpio is dead.  use the gpio-sysfs code as documented in the wiki.

  docs.blackfin.uclinux.org/doku.php?id=linux-kernel:drivers:gpio-sysfs

QuoteReplyEditDelete

2010-10-21 12:39:08     Re: oops with rmmod of simple-gpio module

Prasanth Rajagopal (INDIA)

Message: 94813   

Thanks.

Another question:

If I were to have a GPIO interrupt enabled for BF548 Push Button PB2 (on Kit), I should basically just call the request_irq with the flags, and this will do the initialization of gpio input, edge, triggered interrupt, along with the mapping of isr. But the below code doesnt give me falling/rising interrupt when I look in /proc/interrupts, after the insmod.

ret = request_irq( IRQ_PB2 , my_irq_handler, IRQF_TRIGGER_RISING | IRQF_TRIGGER_FALLING, GPIO_DEV, NULL);

   if (ret) {

                  printk(KERN_WARNING "IRQ %d is not free.\n", IRQ_PB2);

                  return ret;

              }

I dont get the above warning for PB2 usage, and I can see my IRQ listed in /proc/interrupts.

I know the PB2 interrupt works, because it works with VDSP & I have written a modified simple-gpio program that detects the level of PB2 upon a press.

Tried a search and saw these (tried some code changes as in 2nd thread, though I could not find a technical difference)

  blackfin.uclinux.org/gf/project/uclinux-dist/forum/?action=ForumBrowse&forum_id=39&thread_id=38097&_forum_action=ForumMessageBrowse

  blackfin.uclinux.org/gf/project/uclinux-dist/forum/?action=ForumBrowse&forum_id=39&thread_id=26430&_forum_action=ForumMessageBrowse

The BF54x has these PINT configuration, unlike the older ones like BF533. I am not sure about that here.

Is there anything else I can look at, for the error? Any thoughts?

- Prasanth.

QuoteReplyEditDelete

2010-10-21 17:44:39     Re: oops with rmmod of simple-gpio module

Mike Frysinger (UNITED STATES)

Message: 94825   

the default PINT assignments in the kernel should allow full access to port A and B gpios

look at the gpio-keys driver for handling things like push buttons:

  docs.blackfin.uclinux.org/doku.php?id=linux-kernel:drivers:gpio-keys

QuoteReplyEditDelete

2010-10-22 12:30:10     Re: oops with rmmod of simple-gpio module

Prasanth Rajagopal (INDIA)

Message: 94883   

Thanks, the gpio-keys was a good reference. PB2 interrupt assertion works if I have the gpio-key module running. But I couldnt find any mistake in my approach, after looking at that code also, unless there is something serious I am missing.

Here is the code (I dont think I need gpio_direction_input or gpio_to_irq, and  irq_request should be sufficient, but having or not having those function calls didnt make a difference):

#include <linux/module.h>

#include <asm/gpio.h>

#include <linux/interrupt.h>

#include <linux/irq.h>

MODULE_LICENSE("GPL");

MODULE_DESCRIPTION("GPIO Module");

MODULE_AUTHOR("Prasanth");

int irq;

#define GPIO_DEV "PB2 EVENT CHECK"

static irqreturn_t gpio_irq_handler(int irq, void *dev_id);

static __init int sample_module_init(void)

{

    int ret;

    printk("\nInside PB2 EVENT CHECK Module Init\n");

    ret = gpio_request(GPIO_PB2, GPIO_DEV);

    if (ret) {

    printk("\nPB2 EVENT CHECK: unable to request GPIO_PB2\n");

    return ret;

    }

    printk("\nGPIO granted\n");

    ret = gpio_direction_input(GPIO_PB2);

    if (ret) {

        printk("\nPB2 EVENT CHECK: unable to to set GPIO_PB2 as input\n");

        return ret;

        }

    printk("\nGPIO Direction set as input\n");

    irq = gpio_to_irq(GPIO_PB2);

    ret = request_irq( irq , gpio_irq_handler, IRQF_TRIGGER_RISING | IRQF_TRIGGER_FALLING,

                            GPIO_DEV, NULL);

              if (ret) {

                  printk(KERN_WARNING "\nPB2 EVENT CHECK: IRQ %s is not free.\n", GPIO_DEV);

                  return ret;

              }

    printk("\nEdge triggered IRQ registered\n");

    return 0;

}

static irqreturn_t gpio_irq_handler(int irq, void *dev_id)

{

    printk("\ngpio_irq_handler\n");

    return IRQ_HANDLED;

}

static __exit void sample_module_exit(void)

{

    printk("\nInside Module PB2 EVENT CHECK Exit\n");

    free_irq(irq,NULL);

    gpio_free(GPIO_PB2);

}

module_init(sample_module_init);

module_exit(sample_module_exit);

/////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////

And the output::::

root:~> insmod simple_gpio_modified_driver.ko

Inside PB2 EVENT CHECK Module Init

GPIO granted

GPIO Direction set as input

bfin-gpio: GPIO 18 is already reserved by PB2 EVENT CHECK! (Documentation/blackfi

n/bfin-gpio-notes.txt)

Edge triggered IRQ registered

root:~> cat /proc/interrupts

  6:      24790      CORE  Blackfin CoreTimer

14:          1      INTN  rtc-bfin

48:         95      INTN  BFIN_UART_RX

49:       1768      INTN  BFIN_UART_TX

root:~> insmod simple_gpio_modified_driver.ko

Inside PB2 EVENT CHECK Module Init

GPIO granted

GPIO Direction set as input

bfin-gpio: GPIO 18 is already reserved by PB2 EVENT CHECK! (Documentation/blackfi

n/bfin-gpio-notes.txt)

Edge triggered IRQ registered

root:~> cat /proc/interrupts

  6:      34535      CORE  Blackfin CoreTimer

14:          1      INTN  rtc-bfin

48:        143      INTN  BFIN_UART_RX

49:       3395      INTN  BFIN_UART_TX

52:          0      INTN  i2c-bfin-twi

53:          0      INTN  i2c-bfin-twi

68:          3      INTN  pata-bf54x

74:          0      INTN  BF5XX NFC driver

76:          0      INTN  bf54x-keys

82:          1      INTN  musb_hdrc.0

85:          0      INTN  musb_hdrc.0

121:          0      GPIO  PB2 EVENT CHECK

175:        104      GPIO  smsc911x

NMI:          0      CORE  Non Maskable Interrupt

Err:          0

root:~> cat /proc/gpio

GPIO_16:        i2c-bfin-twi            Peripheral

GPIO_17:        i2c-bfin-twi            Peripheral

GPIO_18:        gpio-irq121 *           GPIO INPUT

Any thoughts?

QuoteReplyEditDelete

2010-10-22 12:41:28     Re: oops with rmmod of simple-gpio module

Prasanth Rajagopal (INDIA)

Message: 94885   

Copied something two times. The output is actually (cat /proc/interrupts is after pressing the button):

>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>

root:~> insmod simple_gpio_modified_driver.ko

Inside PB2 EVENT CHECK Module Init

GPIO granted

GPIO Direction set as input

bfin-gpio: GPIO 18 is already reserved by PB2 EVENT CHECK! (Documentation/blackfi

n/bfin-gpio-notes.txt)

Edge triggered IRQ registered

root:~> cat /proc/interrupts

  6:      34535      CORE  Blackfin CoreTimer

14:          1      INTN  rtc-bfin

48:        143      INTN  BFIN_UART_RX

49:       3395      INTN  BFIN_UART_TX

52:          0      INTN  i2c-bfin-twi

53:          0      INTN  i2c-bfin-twi

68:          3      INTN  pata-bf54x

74:          0      INTN  BF5XX NFC driver

76:          0      INTN  bf54x-keys

82:          1      INTN  musb_hdrc.0

85:          0      INTN  musb_hdrc.0

121:          0      GPIO  PB2 EVENT CHECK

175:        104      GPIO  smsc911x

NMI:          0      CORE  Non Maskable Interrupt

Err:          0

root:~> cat /proc/gpio

GPIO_16:        i2c-bfin-twi            Peripheral

GPIO_17:        i2c-bfin-twi            Peripheral

GPIO_18:        gpio-irq121 *           GPIO INPUT

QuoteReplyEditDelete

2010-10-24 03:13:43     Re: oops with rmmod of simple-gpio module

Prasanth Rajagopal (INDIA)

Message: 94908   

Mike,

Is there anything you would like me to debug? I thought my module was the simplest for the purpose.

Thanks

Prasanth,

QuoteReplyEditDelete

2010-10-24 11:36:17     Re: oops with rmmod of simple-gpio module

Mike Frysinger (UNITED STATES)

Message: 94973   

you have a known working module which you can trim down to find out why yours doesnt work

  • Created
Was this helpful?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.