2010-10-12 02:54:03     Problem when I open a device (supervisor resource)

2010-10-12 02:54:03     Problem when I open a device (supervisor resource)

Usama Shakeel (PAKISTAN)

Message: 94419   

Hello,

I get the message shown at last when I open a device with the following code.

serialDev = open(deviceName, O_RDWR | O_NOCTTY | O_NONBLOCK);

    if (serialDev <= 0 )

    {

        printf("ERROR : Device Not Attached \n");

        exit(-1);

    }      

    fcntl(serialDev, F_SETFL, 0);

    printf("\nAfter Device Open:%d",(int)serialDev);

    xget1(serialDev, &tio, &tiosfd);

    cfsetspeed(&tio, speed);

    if (xset1(serialDev, &tio, deviceName))

        goto done;

Kindly let me know what I am doing wrong..??

Regards

Usama Bin Shakeel

After Device Open:Illegal use of supervisor resource

- Attempted to use a Supervisor register or instruction from User mode.

   Supervisor resources are registers and instructions that are reserved

   for Supervisor use: Supervisor only registers, all MMRs, and Supervisor

   only instructions.

Deferred Exception context

CURRENT PROCESS:

COMM=rec PID=328

CPU = 0

TEXT = 0x03560040-0x03563c00        DATA = 0x03563c20-0x03565308

BSS = 0x03565308-0x03565590  USER-STACK = 0x03566f8c

return address: [0x035641be]; contents of:

0x03564190:  5656  5656  5656  5656  5656  5656  5656  5656

0x035641a0:  5656  5656  5656  5656  5656  5656  5656  5656

0x035641b0:  5656  5656  5656  5656  5656  5656  5656 [0033]

0x035641c0:  40f8  0356  4204  0356  07b8  0356  5248  0356

ADSP-BF532-0.6 400(MHz CCLK) 100(MHz SCLK) (mpu off)

Linux version 2.6.28.10-ADI-2009R1.1

Built with gcc version 4.1.2 (ADI svn)

SEQUENCER STATUS:               Not tainted

SEQSTAT: 0006002e  IPEND: 0030  SYSCFG: 0006

  EXCAUSE   : 0x2e

  interrupts disabled

  physical IVG5 asserted : <0xffa08c20> { _evt_ivhw + 0x0 }

RETE: <0x00000000> /* Maybe null pointer? */

RETN: <0x03570000> /* kernel dynamic memory */

RETX: <0x00000480> /* Maybe fixed code section */

RETS: <0x0356200c> [ rec + 0x1fcc ]

PC  : <0x035641be> [ rec + 0x41be ]

DCPLB_FAULT_ADDR: <0x0356404c> [ rec + 0x404c ]

ICPLB_FAULT_ADDR: <0x035641be> [ rec + 0x41be ]

PROCESSOR STATE:

R0 : ffffffff    R1 : ffffffff    R2 : ffffffff    R3 : ffffffff

R4 : ffffffff    R5 : 00000000    R6 : 00000000    R7 : ffffffff

P0 : 00000020    P1 : 035640a8    P2 : 035640f8    P3 : 00000000

P4 : 00000000    P5 : 03562d7f    FP : 03564068    SP : 0356ff24

LB0: 03562d69    LT0: 03562d5c    LC0: 00000000

LB1: 0356280d    LT1: 035627c6    LC1: 00000001

B0 : 00000000    L0 : 00000000    M0 : 00000000    I0 : 03563c78

B1 : 00000000    L1 : 00000000    M1 : 00000000    I1 : 03540004

B2 : 00000000    L2 : 00000000    M2 : 00000000    I2 : 00000000

B3 : 00000000    L3 : 00000000    M3 : 00000000    I3 : 00000000

A0.w: 00000000   A0.x: 00000000   A1.w: 00000000   A1.x: 00000000

USP : 03564050  ASTAT: 02002022

Hardware Trace:

   0 Target : <0x00004c28> { _trap_c + 0x0 }

     Source : <0xffa0867e> { _exception_to_level5 + 0xae }

   1 Target : <0xffa085d0> { _exception_to_level5 + 0x0 }

     Source : <0xffa0848c> { _bfin_return_from_exception + 0x18 }

   2 Target : <0xffa08474> { _bfin_return_from_exception + 0x0 }

     Source : <0xffa08528> { _ex_trap_c + 0x6c }

   3 Target : <0xffa084bc> { _ex_trap_c + 0x0 }

     Source : <0xffa0874a> { _trap + 0x5a }

   4 Target : <0xffa086f0> { _trap + 0x0 }

     Source : <0x035641bc> [ rec + 0x41bc ] 0x5656

   5 Target : <0x03564064> [ rec + 0x4064 ]

     Source : <0x0356404c> [ rec + 0x404c ] JUMP.S

   6 Target : <0x03562d7a> [ rec + 0x2d3a ]

     Source : <0x03562d70> [ rec + 0x2d30 ] RTS

   7 Target : <0x03562d54> [ rec + 0x2d14 ]

     Source : <0x03562d76> [ rec + 0x2d36 ] CALL pcrel

   8 Target : <0x03562d74> [ rec + 0x2d34 ]

     Source : <0x03562008> [ rec + 0x1fc8 ] CALL pcrel

   9 Target : <0x03562000> [ rec + 0x1fc0 ]

     Source : <0x0356202a> [ rec + 0x1fea ] IF CC JUMP

  10 Target : <0x03562016> [ rec + 0x1fd6 ]

     Source : <0x03562d70> [ rec + 0x2d30 ] RTS

  11 Target : <0x03562d54> [ rec + 0x2d14 ]

     Source : <0x03562012> [ rec + 0x1fd2 ] CALL pcrel

  12 Target : <0x0356200c> [ rec + 0x1fcc ]

     Source : <0x03562d7e> [ rec + 0x2d3e ] 0x5510

  13 Target : <0x03562d7a> [ rec + 0x2d3a ]

     Source : <0x03562d70> [ rec + 0x2d30 ] RTS

  14 Target : <0x03562d54> [ rec + 0x2d14 ]

     Source : <0x03562d76> [ rec + 0x2d36 ] CALL pcrel

  15 Target : <0x03562d74> [ rec + 0x2d34 ]

     Source : <0x03562008> [ rec + 0x1fc8 ] CALL pcrel

Userspace Stack

Stack info:

SP: [0x03564050] <0x03564050> [ rec + 0x4050 ]

Memory from 0x03564050 to 03565000

03564050:[55555555] 55555555  55555555  55555555  55555555  55555555  55555555  55555555

03564070: 55555555  55555555  55555555  55555555  55555555  55555555  55555555  55555555

03564090: 55555555  55555555  55555555  56565656  56565656  56565656  56565656  56565656

035640b0: 56565656  56565656  56565656  56565656  56565656  56565656  56565656  56565656

035640d0: 56565656  56565656  56565656  56565656  56565656  56565656  56565656  56565656

035640f0: 56565656  56565656  56565656  56565656  56565656  56565656  56565656  56565656

03564110: 56565656  56565656  56565656  56565656  56565656  56565656  56565656  56565656

03564130: 56565656  56565656  56565656  56565656  56565656  56565656  56565656  56565656

03564150: 56565656  56565656  56565656  56565656  56565656  56565656  56565656  56565656

03564170: 56565656  56565656  56565656  56565656  56565656  56565656  56565656  56565656

03564190: 56565656  56565656  56565656  56565656  56565656  56565656  56565656  56565656

035641b0: 56565656  56565656  56565656  00335656  035640f8  03564204 <035607b8> 03565248

035641d0: 03565304  03566f90  00000000  00000002  03563c68  0356423c  03565248  00000096

035641f0: 00000005  000000c8  00000006  0000012c  00000007  03564230 <0356066e> 03563c20

03564210: 00000000  03565568  03563be0  00000001  0000000a  00000960  03564244  0356423c

03564230: 03566f38 <0356027e> 0000000d  00000003  00000000  7665642f  7974742f  30425355

03564250: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

03564270: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

03564290: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

035642b0: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

035642d0: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

035642f0: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

03564310: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

03564330: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

03564350: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

03564370: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

03564390: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

035643b0: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

035643d0: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

035643f0: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

03564410: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

03564430: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

03564450: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

03564470: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

03564490: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

035644b0: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

035644d0: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

035644f0: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

03564510: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

03564530: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

03564550: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

03564570: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

03564590: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

035645b0: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

035645d0: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

035645f0: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

03564610: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

03564630: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

03564650: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

03564670: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

03564690: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

035646b0: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

035646d0: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

035646f0: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

03564710: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

03564730: 00000000  00000000  00000000  20657461  6f6d656d  50007972  696d7265  6f697373

03564750: 6564206e  6465696e  64614200  64646120  73736572  6f6c4200  64206b63  63697665

03564770: 65722065  72697571  44006465  63697665  726f2065  73657220  6372756f  75622065

03564790: 46007973  20656c69  73697865  49007374  6c61766e  63206469  73736f72  7665642d

035647b0: 20656369  6b6e696c  206f4e00  68637573  76656420  00656369  20746f4e  69642061

035647d0: 74636572  0079726f  61207349  72696420  6f746365  49007972  6c61766e  61206469

035647f0: 6d756772  00746e65  206f6f54  796e616d  65706f20  6966206e  2073656c  73206e69

03564810: 65747379  6f54006d  616d206f  6f20796e  206e6570  656c6966  6e490073  72707061

03564830: 6972706f  20657461  74636f69  6f66206c  65642072  65636976  78655400  69662074

03564850: 6220656c  00797375  656c6946  6f6f7420  72616c20  4e006567  7073206f  20656361

03564870: 7466656c  206e6f20  69766564  49006563  67656c6c  73206c61  006b6565  64616552

03564890: 6c6e6f2d  69662079  7320656c  65747379  6f54006d  616d206f  6c20796e  736b6e69

035648b0: 6f724200  206e656b  65706970  6d754e00  63697265  61206c61  6d756772  20746e65

035648d0: 2074756f  6420666f  69616d6f  754e006e  6972656d  206c6163  75736572  6f20746c

035648f0: 6f207475  61722066  0065676e  6f736552  65637275  61656420  636f6c64  7661206b

03564910: 6564696f  69460064  6e20656c  20656d61  206f6f74  676e6f6c  206f4e00  6b636f6c

03564930: 76612073  616c6961  00656c62  636e7546  6e6f6974  746f6e20  706d6920  656d656c

03564950: 6465746e  72694400  6f746365  6e207972  6520746f  7974706d  6f6f5400  6e616d20

03564970: 656c2079  736c6576  20666f20  626d7973  63696c6f  6e696c20  0000736b  6d206f4e

03564990: 61737365  6f206567  65642066  65726973  79742064  49006570  746e6564  65696669

035649b0: 65722072  65766f6d  68430064  656e6e61  756e206c  7265626d  74756f20  20666f20

035649d0: 676e6172  654c0065  206c6576  6f6e2032  79732074  7268636e  7a696e6f  4c006465

035649f0: 6c657665  68203320  65746c61  654c0064  206c6576  65722033  00746573  6b6e694c

03564a10: 6d756e20  20726562  2074756f  7220666f  65676e61  6f725000  6f636f74  7264206c

03564a30: 72657669  746f6e20  74746120  65686361  6f4e0064  49534320  72747320  75746375

03564a50: 61206572  6c696176  656c6261  76654c00  32206c65  6c616820  00646574  61766e49

03564a70: 2064696c  68637865  65676e61  766e4900  64696c61  71657220  74736575  73656420

03564a90: 70697263  00726f74  68637845  65676e61  6c756620  6f4e006c  6f6e6120  49006564

03564ab0: 6c61766e  72206469  65757165  63207473  0065646f  61766e49  2064696c  746f6c73

03564ad0: 61420000  6f662064  6620746e  20656c69  6d726f66  44007461  63697665  6f6e2065

03564af0: 20612074  65727473  4e006d61  6164206f  61206174  6c696176  656c6261  6d695400

03564b10: 65207265  72697078  4f006465  6f207475  74732066  6d616572  65722073  72756f73

03564b30: 00736563  6863614d  20656e69  6e207369  6f20746f  6874206e  656e2065  726f7774

03564b50: 6150006b  67616b63  6f6e2065  6e692074  6c617473  0064656c  656a624f  69207463

03564b70: 65722073  65746f6d  6e694c00  6168206b  65622073  73206e65  72657665  41006465

03564b90: 72657664  65736974  72726520  5300726f  756f6d72  6520746e  726f7272  6d6f4300

03564bb0: 696e756d  69746163  65206e6f  726f7272  206e6f20  646e6573  6f725000  6f636f74

03564bd0: 7265206c <00726f72> 746c754d  706f6869  74746120  74706d65  52006465  73205346

03564bf0: 69636570  20636966  6f727265  61420072  656d2064  67617373  61560065  2065756c

03564c10: 206f6f74  6772616c  6f662065  65642072  656e6966  61642064  74206174  00657079

03564c30: 656d614e  746f6e20  696e7520  20657571  6e206e6f  6f777465  46006b72  20656c69

03564c50: 63736564  74706972  6920726f  6162206e  74732064  00657461  6f6d6552  61206574

03564c70: 65726464  63207373  676e6168  43006465  6e206e61  6120746f  73656363  20612073

03564c90: 6465656e  73206465  65726168  696c2064  72617262  63410079  73736563  20676e69

03564cb0: 6f632061  70757272  20646574  72616873  6c206465  61726269  2e007972  2062696c

03564cd0: 74636573  206e6f69  61206e69  74756f2e  726f6320  74707572  41006465  6d657474

03564cf0: 6e697470  6f742067  6e696c20  6e69206b  6f6f7420  6e616d20  68732079  64657261

03564d10: 62696c20  69726172  43007365  6f6e6e61  78652074  61206365  61687320  20646572

03564d30: 7262696c  20797261  65726964  796c7463  766e4900  64696c61  20726f20  6f636e69

03564d50: 656c706d  6d206574  69746c75  65747962  20726f20  65646977  61686320  74636172

03564d70: 49007265  7265746e  74707572  73206465  65747379  6163206d  73206c6c  6c756f68

03564d90: 65622064  73657220  74726174  53006465  61657274  7020736d  20657069  6f727265

03564db0: 6f540072  616d206f  7520796e  73726573  636f5300  2074656b  7265706f  6f697461

03564dd0: 6e6f206e  6e6f6e20  636f732d  0074656b  74736544  74616e69  206e6f69  72646461

03564df0: 20737365  75716572  64657269  73654d00  65676173  6f6f7420  6e6f6c20  72500067

03564e10: 636f746f  77206c6f  676e6f72  70797420  6f662065  6f732072  74656b63  6f725000

03564e30: 6f636f74  6f6e206c  76612074  616c6961  00656c62  746f7250  6c6f636f  746f6e20

03564e50: 70757320  74726f70  53006465  656b636f  79742074  6e206570  7320746f  6f707075

03564e70: 64657472  65704f00  69746172  6e206e6f  7320746f  6f707075  64657472  6f725000

03564e90: 6f636f74  6166206c  796c696d  746f6e20  70757320  74726f70  41006465  65726464

03564eb0: 66207373  6c696d61  6f6e2079  75732074  726f7070  20646574  70207962  6f746f72

03564ed0: 006c6f63  72646441  20737365  65726c61  20796461  75206e69  43006573  6f6e6e61

03564ef0: 73612074  6e676973  71657220  74736575  61206465  65726464  4e007373  6f777465

03564f10: 69206b72  6f642073  4e006e77  6f777465  69206b72  6e752073  63616572  6c626168

03564f30: 654e0065  726f7774  7264206b  6570706f  6f632064  63656e6e  6e6f6974  206e6f20

03564f50: 65736572  6f530074  61777466  63206572  65737561  6f632064  63656e6e  6e6f6974

03564f70: 6f626120  43007472  656e6e6f  6f697463  6572206e  20746573  70207962  00726565

03564f90: 62206f4e  65666675  70732072  20656361  69617661  6c62616c  72540065  70736e61

03564fb0: 2074726f  70646e65  746e696f  20736920  65726c61  20796461  6e6e6f63  65746365

03564fd0: 72540064  70736e61  2074726f  70646e65  746e696f  20736920  20746f6e  6e6e6f63

03564ff0: 65746365  61430064  746f6e6e  6e657320

Return addresses in stack:

    address : <0x035607b8> [ rec + 0x778 ]

    address : <0x0356066e> [ rec + 0x62e ]

    address : <0x0356027e> [ rec + 0x23e ]

    address : <0x00726f72> /* kernel dynamic memory */

QuoteReplyEditDelete

2010-10-12 09:50:59     Re: Problem when I open a device (supervisor resource)

Mike Frysinger (UNITED STATES)

Message: 94433   

verify you arent blowing your stack:

  docs.blackfin.uclinux.org/doku.php?id=uclinux-dist:debugging_applications#stack_checking

QuoteReplyEditDelete

2010-10-14 06:29:13     Re: Problem when I open a device (supervisor resource)

Usama Shakeel (PAKISTAN)

Message: 94511   

Thanx Mike it seems it resolved the problem..

  • Created
Was this helpful?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.