2010-10-09 12:03:57     Trailing message in Terminal when output script to file

2010-10-09 12:03:57     Trailing message in Terminal when output script to file

T. Jump (UNITED STATES)

Message: 94366   

I'm not sure about the following behavior so thought I would put it out to see if there is an error I need to resolve, or simply a process that I need explained.

I ran my "make build" in two differnt ways; one with just "make build" and one with "make build > output".

With just "make build" the process finished and returned to the command prompt.

With "make build > output", after the process had finished (script in output document identical to what was in the terminal with "make build") a new set of data was displayed in the terminal (see attached). This seems to be error messages but I'm wondering if they are, how to repair them; or is it just a behavior related to outputing using the ">" process.

I would appreciate any feedback here.

T. Jump

jobserver warning

QuoteReplyEditDelete

2010-10-09 17:10:57     Re: Trailing message in Terminal when output script to file

Mike Frysinger (UNITED STATES)

Message: 94368   

i dont see any problems with the output

QuoteReplyEditDelete

2010-10-09 17:39:04     Re: Trailing message in Terminal when output script to file

T. Jump (UNITED STATES)

Message: 94371   

So, do I need to do anything to correct the jobserver warning, or did the build/linux handle this someway?

QuoteReplyEditDelete

2010-10-09 18:02:15     Re: Trailing message in Terminal when output script to file

Mike Frysinger (UNITED STATES)

Message: 94372   

you ignore it

QuoteReplyEditDelete

2010-10-09 18:11:25     Re: Trailing message in Terminal when output script to file

T. Jump (UNITED STATES)

Message: 94373   

Okay. Thanks.

Attachments:
  • Created
Was this helpful?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.