2010-09-30 12:33:23     GnuPG

2010-09-30 12:33:23     GnuPG

Matt Gilg (UNITED STATES)

Message: 94079   

I'm looking to do PGP style encryption/decryption on the blackfin, and in my version of the dist, libgcrypt doesn't have a makefile.  After doing some research, I noticed a tracker ticket for this, and it looks like Robin has added a Makefile to the trunk since.

1 - I didn't see any entries in the current trunk's KConfig system for libgcrypt -- did I just miss them?  I don't have a problem adding them and submitting a patch if that would be useful.

2 - What I was originally looking for is a command-line client for gnupg.  Does this happen to exist somewhere in the distribution as well?

Thanks,

-Matt

QuoteReplyEditDelete

2010-09-30 14:39:40     Re: GnuPG

Mike Frysinger (UNITED STATES)

Message: 94084   

no, the libs arent fully integrated yet.  iirc, some linker script discussions hung things up, but that's been largely sorted now.  feel free to submit a patch.

gnupg is not integrated.  if it were, it'd be at user/gnupg/.

QuoteReplyEditDelete

2010-10-04 19:06:17     Re: GnuPG

Matt Gilg (UNITED STATES)

Message: 94173   

I've attached a diff, but it isn't exactly useful to anybody yet, and it might not be in an acceptable format.  It adds the option and attempts the build, but I get an error when config tries to find libgpg-error:

checking whether a HMAC binary check is requested... no

checking whether padlock support is requested... yes

checking whether a -O flag munging is requested... yes

checking for gpg-error-config... no

checking for GPG Error - version >= 1.4... no

configure: error: libgpg-error is needed.

                See ftp://ftp.gnupg.org/gcrypt/libgpg-error/ .

make[3]: *** [build-libgcrypt-1.4.5/Makefile] Error 1

------------------------------------------------------------------------------------------

libgpg-error is definitely building correctly, and is selected in menuconfig.

The libraries are correctly built in the dist, here is a listing of the .libs directory

within the libgpg-error project.

------------------------------------------------------------------------------------------

gilgm@dev-server:~/Blackfin/uClinux/lib/libgpg-error/build-libgpg-error-1.7/src/.libs$ ls

gpg-error        libgpg_error_la-code-from-errno.o  libgpg_error_la-init.o       libgpg-error.so

libgpg-error.a   libgpg_error_la-code-to-errno.o    libgpg_error_la-strerror.o   libgpg-error.so.0

libgpg-error.la  libgpg-error.lai                   libgpg_error_la-strsource.o  libgpg-error.so.0.5.0

-------------------------------------------------------------------------------------------

Is there something I need to do to tell libgcrypt about the location of libgpg-error?

Thanks,

-Matt

gcrypt.patch

QuoteReplyEditDelete

2010-10-04 19:24:36     Re: GnuPG

Mike Frysinger (UNITED STATES)

Message: 94174   

that output doesnt really tell you the problem.  you need to read config.log.

QuoteReplyEditDelete

2010-10-05 10:56:02     Re: GnuPG

Matt Gilg (UNITED STATES)

Message: 94193   

Thanks Mike.  I'm not too familiar with the autoconf system, and so I guess I'm not sure quite what I'm looking for.  Anyhow, the GPG_ERROR_CONFIG='no' seems wrong, as does the empty GPG_ERROR_LIBS. 

## ----------------- ##

## Output variables. ##

## ----------------- ##

ACLOCAL='${SHELL} /home/gilgm/Blackfin/uClinux-msat-steve/lib/libgcrypt/libgcrypt-1.4.5/missing --run aclocal-1.10'

AMDEPBACKSLASH=''

AMDEP_FALSE=''

AMDEP_TRUE='#'

AMTAR='${SHELL} /home/gilgm/Blackfin/uClinux-msat-steve/lib/libgcrypt/libgcrypt-1.4.5/missing --run tar'

AR='bfin-linux-uclibc-ar'

AS='bfin-linux-uclibc-as'

AUTOCONF='${SHELL} /home/gilgm/Blackfin/uClinux-msat-steve/lib/libgcrypt/libgcrypt-1.4.5/missing --run autoconf'

AUTOHEADER='${SHELL} /home/gilgm/Blackfin/uClinux-msat-steve/lib/libgcrypt/libgcrypt-1.4.5/missing --run autoheader'

AUTOMAKE='${SHELL} /home/gilgm/Blackfin/uClinux-msat-steve/lib/libgcrypt/libgcrypt-1.4.5/missing --run automake-1.10'

AWK='gawk'

BUILD_FILEVERSION=''

BUILD_REVISION='1417'

BUILD_TIMESTAMP=''

CC='bfin-linux-uclibc-gcc'

CCAS='bfin-linux-uclibc-gcc'

CCASDEPMODE='depmode=none'

CCASFLAGS='-pipe -Wall -g -O2      -mcpu=bf537-0.3'

CCDEPMODE='depmode=none'

CFLAGS='-pipe -Wall -g -O2      -mcpu=bf537-0.3'

CPP='bfin-linux-uclibc-gcc -E'

CPPFLAGS='-DEMBED -D__uClinux__ -I/home/gilgm/Blackfin/uClinux-msat-steve  -mcpu=bf537-0.3'

CROSS_COMPILING_FALSE=''

CROSS_COMPILING_TRUE=''

CXX='bfin-linux-uclibc-g++'

CXXCPP='bfin-linux-uclibc-g++ -E'

CXXDEPMODE='depmode=none'

CXXFLAGS='-pipe -Wall -g -O2  -mcpu=bf537-0.3'

CYGPATH_W='echo'

DEFS=''

DEPDIR='.deps'

DLLTOOL='dlltool'

DL_LIBS=''

ECHO='echo'

ECHO_C=''

ECHO_N='-n'

ECHO_T=''

EGREP='/bin/grep -E'

ENABLE_O_FLAG_MUNGING_FALSE='#'

ENABLE_O_FLAG_MUNGING_TRUE=''

EXEEXT=''

F77='bfin-linux-uclibc-gfortran'

FALLBACK_SOCKLEN_T=''

FFLAGS='-g -O2'

GCRYPT_CIPHERS=''

GCRYPT_DIGESTS=''

GCRYPT_PUBKEY_CIPHERS=''

GCRYPT_RANDOM=''

GPG_ERROR_CFLAGS=''

GPG_ERROR_CONFIG='no'

GPG_ERROR_LIBS=''

GREP='/bin/grep'

HAVE_LD_VERSION_SCRIPT_FALSE=''

HAVE_LD_VERSION_SCRIPT_TRUE='#'

HAVE_W32_SYSTEM_FALSE=''

HAVE_W32_SYSTEM_TRUE='#'

INSTALL_DATA='${INSTALL} -m 644'

INSTALL_PROGRAM='${INSTALL}'

INSTALL_SCRIPT='${INSTALL}'

INSTALL_STRIP_PROGRAM='$(install_sh) -c -s'

LDFLAGS='    -mcpu=bf537-0.3'

LIBGCRYPT_CIPHERS=''

LIBGCRYPT_CONFIG_API_VERSION='1'

LIBGCRYPT_CONFIG_CFLAGS=''

LIBGCRYPT_CONFIG_LIBS='-lgcrypt'

LIBGCRYPT_DIGESTS=''

LIBGCRYPT_LT_AGE='5'

LIBGCRYPT_LT_CURRENT='16'

LIBGCRYPT_LT_REVISION='3'

LIBGCRYPT_PUBKEY_CIPHERS=''

LIBGCRYPT_THREAD_MODULES=''

LIBOBJS=''

LIBS=''

LIBTOOL='$(SHELL) $(top_builddir)/libtool'

LN_S='ln -s'

LTLIBOBJS=''

MAINT='#'

MAINTAINER_MODE_FALSE=''

MAINTAINER_MODE_TRUE='#'

MAKEINFO='${SHELL} /home/gilgm/Blackfin/uClinux-msat-steve/lib/libgcrypt/libgcrypt-1.4.5/missing --run makeinfo'

MKDIR_P='/bin/mkdir -p'

MPI_MOD_ASM_MPIH_ADD1_FALSE=''

MPI_MOD_ASM_MPIH_ADD1_TRUE=''

MPI_MOD_ASM_MPIH_LSHIFT_FALSE=''

MPI_MOD_ASM_MPIH_LSHIFT_TRUE=''

MPI_MOD_ASM_MPIH_MUL1_FALSE=''

MPI_MOD_ASM_MPIH_MUL1_TRUE=''

MPI_MOD_ASM_MPIH_MUL2_FALSE=''

MPI_MOD_ASM_MPIH_MUL2_TRUE=''

MPI_MOD_ASM_MPIH_MUL3_FALSE=''

MPI_MOD_ASM_MPIH_MUL3_TRUE=''

MPI_MOD_ASM_MPIH_RSHIFT_FALSE=''

MPI_MOD_ASM_MPIH_RSHIFT_TRUE=''

MPI_MOD_ASM_MPIH_SUB1_FALSE=''

MPI_MOD_ASM_MPIH_SUB1_TRUE=''

MPI_MOD_ASM_UDIV_FALSE=''

MPI_MOD_ASM_UDIV_QRNND_FALSE=''

MPI_MOD_ASM_UDIV_QRNND_TRUE=''

MPI_MOD_ASM_UDIV_TRUE=''

MPI_MOD_C_MPIH_ADD1_FALSE=''

MPI_MOD_C_MPIH_ADD1_TRUE=''

MPI_MOD_C_MPIH_LSHIFT_FALSE=''

MPI_MOD_C_MPIH_LSHIFT_TRUE=''

MPI_MOD_C_MPIH_MUL1_FALSE=''

MPI_MOD_C_MPIH_MUL1_TRUE=''

MPI_MOD_C_MPIH_MUL2_FALSE=''

MPI_MOD_C_MPIH_MUL2_TRUE=''

MPI_MOD_C_MPIH_MUL3_FALSE=''

MPI_MOD_C_MPIH_MUL3_TRUE=''

MPI_MOD_C_MPIH_RSHIFT_FALSE=''

MPI_MOD_C_MPIH_RSHIFT_TRUE=''

MPI_MOD_C_MPIH_SUB1_FALSE=''

MPI_MOD_C_MPIH_SUB1_TRUE=''

MPI_MOD_C_UDIV_FALSE=''

MPI_MOD_C_UDIV_QRNND_FALSE=''

MPI_MOD_C_UDIV_QRNND_TRUE=''

MPI_MOD_C_UDIV_TRUE=''

MPI_SFLAGS=''

NOEXECSTACK_FLAGS=''

OBJDUMP='bfin-linux-uclibc-objdump'

OBJEXT='o'

PACKAGE='libgcrypt'

PACKAGE_BUGREPORT='bug-libgcrypt@gnupg.org'

PACKAGE_NAME='libgcrypt'

PACKAGE_STRING='libgcrypt 1.4.5'

PACKAGE_TARNAME='libgcrypt'

PACKAGE_URL=''

PACKAGE_VERSION='1.4.5'

PATH_SEPARATOR=':'

PTH_CFLAGS=''

PTH_CONFIG=''

PTH_LIBS=''

RANLIB='bfin-linux-uclibc-ranlib'

RC='no'

SET_MAKE=''

SHELL='/bin/bash'

STRIP='bfin-linux-uclibc-strip'

SYS_SOCKET_H=''

USE_RANDOM_DAEMON_FALSE=''

USE_RANDOM_DAEMON_TRUE='#'

VERSION='1.4.5'

ac_ct_CC=''

ac_ct_CXX=''

ac_ct_F77=''

am__fastdepCCAS_FALSE=''

am__fastdepCCAS_TRUE='#'

am__fastdepCC_FALSE=''

am__fastdepCC_TRUE='#'

am__fastdepCXX_FALSE=''

am__fastdepCXX_TRUE='#'

am__include='include'

am__isrc=' -I$(srcdir)'

am__leading_dot='.'

am__quote=''

am__tar='${AMTAR} chof - "$$tardir"'

am__untar='${AMTAR} xf -'

bindir='${exec_prefix}/bin'

build='i686-pc-linux-gnu'

build_alias='i686-pc-linux-gnu'

build_cpu='i686'

build_os='linux-gnu'

build_vendor='pc'

datadir='/usr/share'

datarootdir='${prefix}/share'

docdir='${datarootdir}/doc/${PACKAGE_TARNAME}'

dvidir='${docdir}'

exec_prefix='NONE'

host='bfin-unknown-linux-uclibc'

host_alias='bfin-linux-uclibc'

host_cpu='bfin'

host_os='linux-uclibc'

host_vendor='unknown'

htmldir='${docdir}'

includedir='${prefix}/include'

infodir='/usr/share/info'

install_sh='$(SHELL) /home/gilgm/Blackfin/uClinux-msat-steve/lib/libgcrypt/libgcrypt-1.4.5/install-sh'

libdir='${exec_prefix}/lib'

libexecdir='${exec_prefix}/libexec'

localedir='${datarootdir}/locale'

localstatedir='/var/lib'

mandir='/usr/share/man'

mkdir_p='/bin/mkdir -p'

oldincludedir='/usr/include'

pdfdir='${docdir}'

prefix='/usr'

program_transform_name='s,x,x,'

psdir='${docdir}'

sbindir='${exec_prefix}/sbin'

sharedstatedir='${prefix}/com'

sysconfdir='/etc'

target_alias=''

## ----------- ##

## confdefs.h. ##

## ----------- ##

/* confdefs.h */

#define PACKAGE_NAME "libgcrypt"

#define PACKAGE_TARNAME "libgcrypt"

#define PACKAGE_VERSION "1.4.5"

#define PACKAGE_STRING "libgcrypt 1.4.5"

#define PACKAGE_BUGREPORT "bug-libgcrypt@gnupg.org"

#define PACKAGE_URL ""

#define PACKAGE "libgcrypt"

#define VERSION "1.4.5"

#define PACKAGE "libgcrypt"

#define VERSION "1.4.5"

#define STDC_HEADERS 1

#define HAVE_SYS_TYPES_H 1

#define HAVE_SYS_STAT_H 1

#define HAVE_STDLIB_H 1

#define HAVE_STRING_H 1

#define HAVE_MEMORY_H 1

#define HAVE_STRINGS_H 1

#define HAVE_INTTYPES_H 1

#define HAVE_STDINT_H 1

#define HAVE_UNISTD_H 1

#define HAVE_DLFCN_H 1

#define SIZEOF_UNSIGNED_SHORT 2

#define SIZEOF_UNSIGNED_INT 4

#define SIZEOF_UNSIGNED_LONG 4

#define SIZEOF_UNSIGNED_LONG_LONG 8

#define HAVE_UINTPTR_T 1

#define EGD_SOCKET_NAME ""

#define ENABLE_PADLOCK_SUPPORT 1

#define PRINTABLE_OS_NAME "GNU/Linux"

#define NAME_OF_DEV_RANDOM "/dev/random"

#define NAME_OF_DEV_URANDOM "/dev/urandom"

configure: exit 1

-Matt

QuoteReplyEditDelete

2010-10-05 14:19:41     Re: GnuPG

Mike Frysinger (UNITED STATES)

Message: 94196   

that isnt the important part of the log.  post the whole thing as an attachment.

QuoteReplyEditDelete

2010-10-05 16:22:17     Re: GnuPG

Matt Gilg (UNITED STATES)

Message: 94200   

Oops, sorry about that.  I've attached the whole log.

-Matt

libgcrypt.config.log

QuoteReplyEditDelete

2010-10-06 03:01:25     Re: GnuPG

Mike Frysinger (UNITED STATES)

Message: 94219   

i dont think that is the whole log.  pretty much every config.log ive seen has info at the top like:

This file contains any messages produced by compilers while

running configure, to aid debugging if configure makes a mistake.

It was created by dbus configure 1.3.0, which was

generated by GNU Autoconf 2.63.  Invocation command line was

QuoteReplyEditDelete

2010-10-06 10:57:38     Re: GnuPG

Matt Gilg (UNITED STATES)

Message: 94285   

Sorry Mike,  accidentally attached the same log that my previous post contained.  Oops.  The full log is attached.

Thanks,

-Matt

gcrypt.config.log

QuoteReplyEditDelete

2010-10-06 14:04:54     Re: GnuPG

Mike Frysinger (UNITED STATES)

Message: 94294   

hmm, i guess i fixed this locally but forgot to commit it.  sorry about that.  svn up the trunk lib dir.

  • Created
Was this helpful?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.