2010-07-15 01:30:40     error after update my kernel!

2010-07-15 01:30:40     error after update my kernel!

zhang zhihua (CHINA)

Message: 91263   

My board is BF518F-EZBRD,software is Linux-2.6.28,but after update the kernel to the llatest version(Index of /branches/2009R1),I make it and download it to my board,the kernel is cant work!it found:

## Booting kernel from Legacy Image at 01000000 ...

   Image Name:   Linux-2.6.28.10-ADI-2009R1.1

   Created:      2010-07-15   5:07:00 UTC

   Image Type:   Blackfin Linux Kernel Image (gzip compressed)

   Data Size:    3895780 Bytes =  3.7 MB

   Load Address: 00001000

   Entry Point:  001f0b6c

   Verifying Checksum ... OK

   Uncompressing Kernel Image ... OK

Starting Kernel at = 001f0b6c

Linux version 2.6.28.10-ADI-2009R1.1 (root@ubuntu) (gcc version 4.1.2 (ADI svn))

#476 Wed Jul 14 22:06:45 PDT 2010

bootconsole [early_shadow0] enabled

bootconsole [early_BFuart0] enabled

early printk enabled on early_BFuart0

Board Memory: 64MB

Kernel Managed Memory: 64MB

Memory map:

  fixedcode = 0x00000400-0x00000490

  text      = 0x00001000-0x0014e390

  rodata    = 0x0014e390-0x001b5490

  bss       = 0x001b6000-0x001cf67c

  data      = 0x001cf67c-0x001e4000

    stack   = 0x001e2000-0x001e4000

  init      = 0x001e4000-0x0068e000

  available = 0x0068e000-0x03eff000

  DMA Zone  = 0x03f00000-0x04000000

Hardware Trace Active and Enabled

Boot Mode: 3

Blackfin support (C) 2004-2009 Analog Devices, Inc.

Compiled for ADSP-BF518 Rev 0.0

Warning: Compiled for Rev 0, but running on Rev 1

Blackfin Linux support by   blackfin.uclinux.org/

Processor Speed: 400 MHz core clock and 80 MHz System Clock

NOMPU: setting up cplb tables

Instruction Cache Enabled for CPU0

Data Cache Enabled for CPU0 (write-back)

Built 1 zonelists in Zone order, mobility grouping off.  Total pages: 16001

Kernel command line: root=/dev/mtdblock0 rw clkin_hz=25000000 earlyprintk=serial

,uart0,57600 console=ttyBF0,57600 ip=192.168.0.15:192.168.0.2:192.168.0.1:255.25

5.255.0:bf518f-ezbrd:eth0:off

Configuring Blackfin Priority Driven Interrupts

PID hash table entries: 256 (order: 8, 1024 bytes)

Console: colour dummy device 80x25

console [ttyBF0] enabled, bootconsole disabled

console [ttyBF0] enabled, bootconsole disabled

Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)

Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)

Memory available: 57224k/65536k RAM, (4776k init code, 1332k kernel code, 600k d

ata, 1024k dma, 576k reserved)

Calibrating delay loop... 796.67 BogoMIPS (lpj=1593344)

Security Framework initialized

Mount-cache hash table entries: 512

Blackfin Scratchpad data SRAM: 4 KB

Blackfin L1 Data A SRAM: 16 KB (15 KB free)

Blackfin L1 Data B SRAM: 16 KB (16 KB free)

Blackfin L1 Instruction SRAM: 48 KB (42 KB free)

net_namespace: 288 bytes

NET: Registered protocol family 16

Blackfin DMA Controller

ezbrd_init(): registering device resources

NET: Registered protocol family 2

IP route cache hash table entries: 1024 (order: 0, 4096 bytes)

TCP established hash table entries: 2048 (order: 2, 16384 bytes)

TCP bind hash table entries: 2048 (order: 1, 8192 bytes)

TCP: Hash tables configured (established 2048 bind 2048)

TCP reno registered

NET: Registered protocol family 1

NTFS driver 2.1.29 [Flags: R/O].

JFFS2 version 2.2. (NAND) 漏 2001-2006 Red Hat, Inc.

msgmni has been set to 111

io scheduler noop registered (default)

The major of the gpio device is 110

Registered character driver

The major of the test device is 253

Registered character driver

The major of the bluetooth device is 113

Registered character driver

The major of the test device is 112

Serial: Blackfin serial driver

bfin-uart.1: ttyBF0 at MMIO 0xffc00400 (irq = 29) is a BFIN-UART

bfin-uart.1: ttyBF1 at MMIO 0xffc02000 (irq = 31) is a BFIN-UART

brd: module loaded

bfin_mii_bus: probed

bfin_mac: attached PHY driver [Generic PHY] (mii_bus:phy_addr=0:03, irq=-1, mdc_

clk=2500000Hz(mdc_div=15)@sclk=80MHz)

bfin_mac bfin_mac.0: Blackfin on-chip Ethernet MAC driver, Version 1.1

physmap platform flash device: 00300000 at 20000000

physmap-flash.0: Found 1 x16 devices at 0x0 in 16-bit bank

NOR chip too large to fit in mapping. Attempting to cope...

Amd/Fujitsu Extended Query Table at 0x0040

number of CFI chips: 1

cfi_cmdset_0002: Disabling erase-suspend-program due to code brokenness.

Reducing visibility of 4096KiB chip to 3072KiB

cmdlinepart partition parsing not available

RedBoot partition parsing not available

Using physmap partition information

Creating 3 MTD partitions on "physmap-flash.0":

0x00000000-0x00040000 : "bootloader(nor)"

0x00040000-0x00200000 : "linux kernel(nor)"

0x00200000-0x00300000 : "file system(nor)"

m25p80 spi0.2: m25p16 (2048 Kbytes)

Creating 2 MTD partitions on "m25p80":

0x00000000-0x00040000 : "bootloader(spi)"

0x00040000-0x00200000 : "linux kernel(spi)"

bfin-spi bfin-spi.0: Blackfin on-chip SPI Controller Driver, Version 1.0, regs_b

ase@ffc00500, dma channel@7

bfin-spi bfin-spi.1: Blackfin on-chip SPI Controller Driver, Version 1.0, regs_b

ase@ffc03400, dma channel@5

rtc-bfin rtc-bfin: rtc core: registered rtc-bfin as rtc0

bfin-wdt: initialized: timeout=20 sec (nowayout=0)

dma_alloc_init: dma_page @ 0x03b31000 - 256 pages at 0x03f00000

Hardware Trace:

   0 Target : <0x00004ac0> { _dump_stack + 0x0 }

     Source : <0x0000611c> { _peripheral_request + 0xfc } CALL pcrel

   1 Target : <0x0000610a> { _peripheral_request + 0xea }

     Source : <0x00006008> { _cmp_label + 0x30 } RTS

   2 Target : <0x00006000> { _cmp_label + 0x28 }

     Source : <0x00005ff8> { _cmp_label + 0x20 } IF !CC JUMP

   3 Target : <0x00005fd8> { _cmp_label + 0x0 }

     Source : <0x00006106> { _peripheral_request + 0xe6 } CALL pcrel

   4 Target : <0x000060fe> { _peripheral_request + 0xde }

     Source : <0x00006086> { _peripheral_request + 0x66 } IF !CC JUMP

   5 Target : <0x00006042> { _peripheral_request + 0x22 }

     Source : <0x0000603c> { _peripheral_request + 0x1c } IF !CC JUMP

   6 Target : <0x0000603a> { _peripheral_request + 0x1a }

     Source : <0x0000602e> { _peripheral_request + 0xe } IF !CC JUMP

   7 Target : <0x00006020> { _peripheral_request + 0x0 }

     Source : <0x00006200> { _peripheral_request_list + 0x24 } CALL pcrel

   8 Target : <0x000061fe> { _peripheral_request_list + 0x22 }

     Source : <0x000061ee> { _peripheral_request_list + 0x12 } JUMP.S

   9 Target : <0x000061dc> { _peripheral_request_list + 0x0 }

     Source : <0x0014cda4> { _sdh_probe + 0x1bc } CALL pcrel

  10 Target : <0x0014cd98> { _sdh_probe + 0x1b0 }

     Source : <0x0014cd04> { _sdh_probe + 0x11c } IF CC JUMP

  11 Target : <0x0014cd00> { _sdh_probe + 0x118 }

     Source : <0x00028ed8> { _request_irq + 0x34 } RTS

  12 Target : <0x00028ece> { _request_irq + 0x2a }

     Source : <0x00028f3e> { _request_irq + 0x9a } IF CC JUMP

  13 Target : <0x00028f3c> { _request_irq + 0x98 }

     Source : <0x00028f34> { _request_irq + 0x90 } IF CC JUMP

  14 Target : <0x00028f30> { _request_irq + 0x8c }

     Source : <0x00028cce> { ___setup_irq + 0x1a } RTS

  15 Target : <0x00028cc6> { ___setup_irq + 0x12 }

     Source : <0x00028d84> { ___setup_irq + 0xd0 } JUMP.S

Stack info:

SP: [0x03ee9d00] <0x03ee9d00> /* kernel dynamic memory */

FP: (0x03ee9d14)

Memory from 0x03ee9d00 to 03eea000

03ee9d00:[001d4700]<00006120> 00000002  00008213  00000000 (00000000)<00028f30>

001d46e8

03ee9d20: 000f755c <00006204> 001d1c44  03b2ffbc  001d1c44  00000000  00000000

00187270

03ee9d40: 00000000 <0014cd00> 03b2fe00  03b2ffbc <0014cda8> 03b2fe00  00000000

00001000

03ee9d60: 001dd174  001ff728  001dd174 <0006a122> 0019f2dc  03b2ffbc  001dd174 <

000cce90>

03ee9d80: 001d1750  001dd174  001cd230  001d17fc  000000ac  00000000 <0014b4a4><

0014b4cc>

03ee9da0: 001d1664 <000ccfe8> 001d1750  001dd174  001ff728  001d17fc  001db458

001ff728

03ee9dc0: 00000000 <000cc6a6> 000ccf7c  001db458  00000000  03ee9de4  03a7dbc0 <

000a848c>

03ee9de0: 001b6024  03efb5d8  001d1798 <000ccd3e> 001b6024  00000000  03a7dbc0

00000000

03ee9e00: 03ee9e24  03ee9e24 <000cca58> 000ccf7c <000cca76><000cd138> 03b039a0

001dd124

03ee9e20: 00192c8c  00187270  00000000 <000cd138> 001b6024  001dd174  001ff728

00000000

03ee9e40: 00000000  00000000  00000000  00000000 <00001028> 001b6024  001f8430

00000000

03ee9e60: 00000000  00000000  03ee6bc0  001e183c  00000010  03ee8000  000040d0

00000000

03ee9e80: 00000001  000240d0  00000000  00000000  001e183c  00000001  00000044

03ee8000

03ee9ea0: 03ee8000  03ee8000  000240d0  03ee8000  00000010  0070dac0  00000000

00000000

03ee9ec0: 00000000  00000000  00000000  00000001  00000000  00000000  ffffffff

03ee9f0c

03ee9ee0:<000a7744> 03ed6940  03ed5a40  001c24ec <000a77b8> 03efb6a4  00000000

000000fc

03ee9f00: 001c24ec  000000d0  03ee9f0c  03ee5e10  00000000  00000000 <00189f20><

000a791e>

03ee9f20: 001c24ec  03ed5a40  00000000 <0006527c> 03ed6940  03ed5a40  001ff728

03ee9f60

03ee9f40: 00004000  00000000  00000000  00000000  001c24ec  03ee9f60 <000654a0>

001d54f8

03ee9f60: 000000fc <000654ae> 001d54f8  001c19f8  03ed6940  03ed5a40  03ee9f9c

7fffff00

03ee9f80: 00000001 <0002a2de> 03ee9f9c  00000076  0000000e <00065572> 03ed5a40

00383131

03ee9fa0: 00000000  001f0000 <0002a33a> 001d394c  001ff4b0  00000076  001d54f8 <

001e43a0>

03ee9fc0: 001ff6c0  001ff4b0  00000000  00000000  00000000  00000000  00000000

00000000

03ee9fe0: 00000000 <0000145e> 00000000  00000000  00000000  00000000  ffffffff

00000006

Return addresses in stack:

    address : <0x00006120> { _peripheral_request + 0x100 }

   frame  1 : <0x00028f30> { _request_irq + 0x8c }

    address : <0x00006204> { _peripheral_request_list + 0x28 }

    address : <0x0014cd00> { _sdh_probe + 0x118 }

    address : <0x0014cda8> { _sdh_probe + 0x1c0 }

    address : <0x0006a122> { _create_dir + 0x3a }

    address : <0x000cce90> { _driver_probe_device + 0x80 }

    address : <0x0014b4a4> { _klist_next + 0x20 }

    address : <0x0014b4cc> { _klist_next + 0x48 }

    address : <0x000ccfe8> { ___driver_attach + 0x6c }

    address : <0x000cc6a6> { _bus_for_each_dev + 0x3e }

    address : <0x000a848c> { _kobject_init_and_add + 0x24 }

    address : <0x000ccd3e> { _driver_attach + 0x1a }

    address : <0x000cca58> { _bus_add_driver + 0x64 }

    address : <0x000cca76> { _bus_add_driver + 0x82 }

    address : <0x000cd138> { _driver_register + 0x40 }

    address : <0x000cd138> { _driver_register + 0x40 }

    address : <0x00001028> { _do_one_initcall + 0x28 }

    address : <0x000a7744> { _ida_get_new_above + 0x94 }

    address : <0x000a77b8> { _ida_get_new_above + 0x108 }

    address : <0x00189f20> /* kernel dynamic memory */

    address : <0x000a791e> { _ida_pre_get + 0xe }

    address : <0x0006527c> { _proc_register + 0x30 }

    address : <0x000654a0> { _create_proc_entry + 0x3c }

    address : <0x000654ae> { _create_proc_entry + 0x4a }

    address : <0x0002a2de> { _register_irq_proc + 0x76 }

    address : <0x00065572> { _proc_mkdir_mode + 0x2e }

    address : <0x0002a33a> { _init_irq_proc + 0x42 }

    address : <0x001e43a0> { _kernel_init + 0x84 }

    address : <0x0000145e> { _kernel_thread_helper + 0x6 }

peripheral_request: Peripheral 19 function 1 is already reserved by mmc_spi !

bfin-sdh bfin-sdh.0: unable to request peripheral pins

bfin-sdh: probe of bfin-sdh.0 failed with error -16

mmc_spi spi0.5: ASSUMING 3.2-3.4 V slot power

------------[ cut here ]------------

WARNING: at fs/sysfs/dir.c:462 _sysfs_add_one+0x3a/0x3c()

sysfs: duplicate filename 'mmc0' can not be created

Modules linked in:

Hardware Trace:

   0 Target : <0x00004ac0> { _dump_stack + 0x0 }

     Source : <0x0000e8b0> { _warn_slowpath + 0x58 } CALL pcrel

   1 Target : <0x0000e8b0> { _warn_slowpath + 0x58 }

     Source : <0x0002599e> { _print_modules + 0x7a } RTS

   2 Target : <0x00025998> { _print_modules + 0x74 }

     Source : <0x0000eef2> { _printk + 0x16 } RTS

   3 Target : <0x0000eeee> { _printk + 0x12 }

     Source : <0x0000f754> { _vprintk + 0x12c } RTS

   4 Target : <0x0000f734> { _vprintk + 0x10c }

     Source : <0x0000f878> { _vprintk + 0x250 } JUMP.S

   5 Target : <0x0000f878> { _vprintk + 0x250 }

     Source : <0x0000ed66> { _wake_up_klogd + 0x1a } RTS

   6 Target : <0x0000ed66> { _wake_up_klogd + 0x1a }

     Source : <0x0000ed58> { _wake_up_klogd + 0xc } IF !CC JUMP

   7 Target : <0x0000ed4c> { _wake_up_klogd + 0x0 }

     Source : <0x0000f16e> { _release_console_sem + 0x1a2 } JUMP.L

   8 Target : <0x0000f166> { _release_console_sem + 0x19a }

     Source : <0x0000f15a> { _release_console_sem + 0x18e } IF !CC JUMP

   9 Target : <0x0000f158> { _release_console_sem + 0x18c }

     Source : <0x0000f14a> { _release_console_sem + 0x17e } IF !CC JUMP

  10 Target : <0x0000f144> { _release_console_sem + 0x178 }

     Source : <0x00021188> { _up + 0x38 } RTS

  11 Target : <0x00021182> { _up + 0x32 }

     Source : <0x00021174> { _up + 0x24 } IF !CC JUMP

  12 Target : <0x00021150> { _up + 0x0 }

     Source : <0x0000f140> { _release_console_sem + 0x174 } CALL pcrel

  13 Target : <0x0000f12c> { _release_console_sem + 0x160 }

     Source : <0x0000f016> { _release_console_sem + 0x4a } IF !CC JUMP

  14 Target : <0x0000efee> { _release_console_sem + 0x22 }

     Source : <0x0000f10e> { _release_console_sem + 0x142 } IF !CC JUMP

  15 Target : <0x0000f108> { _release_console_sem + 0x13c }

     Source : <0x0000ecc6> { __call_console_drivers + 0x7a } RTS

Stack info:

SP: [0x03ee9b7c] <0x03ee9b7c> /* kernel dynamic memory */

FP: (0x03ee9ccc)

Memory from 0x03ee9b70 to 03eea000

03ee9b70: 00000000  03ee9b7c  03a78400 [0000e8b0]<0000e8b4> 03ee9b9c  0018d918

00000006

03ee9b90: 0018d918  000001ce  03ee9b9c  7379735f  615f7366  6f5f6464  302b656e

2f613378

03ee9bb0: 63337830  00000000  00000000  03efb820  001c3508  00000000  00000001

ffffffff

03ee9bd0: 03ee9c00 <000a7744> 03efb824  03efb820  001c3508  00000000  00000001

00000001

03ee9bf0: 00000001  00000001  00000000  00000000  03b29800 <0004854a> 00000001

ffffffff

03ee9c10: 03ee9c40 <000a7744> 00efb824  03efb820  001c3508  00000000  00000001

00000001

03ee9c30: 00000001  001c3508  001c3508  03ee9c40  03b29800 <0004854a> 0072ecc4

03ee9cc0

03ee9c50: 03a78400  03ef5000  000698d4  03b29800 <00069d6a> 03b32928  0072ecc4 <

000485c6>

03ee9c70: 03ef5000  03b32928  03b29800  03ee9ca0 <00069c86> 03b32928  ffffffef

03a78490

03ee9c90: 03a78490  03b329ac  001d13b4  03a78400  03b30700 <0006aa26> 03ee9cc0

0072ecc4

03ee9cb0: 00000000  03a7846c <000a843e> 03a7846c  0072ecc4  00000000  00000000 (

00000000)

03ee9cd0:<0006ab3c> 03a78400  001d13b4  00000000  03a78404  0019de40 <000cb310>

03ee9d04

03ee9cf0: 00000001 <000cb500> 03a7846c <000cab7c> 03a78400  03a78490 <000cb012>

03a78404

03ee9d10: 03a78404  03b29800  00000000  03b29800 <000ef02e> 03a78400  001d13b4

03a78400

03ee9d30: 00000000  03b2fc00  001dd1b8  00000000  00000000 <000f8c06> 03a785bc <

000f8d4a>

03ee9d50: 03a785bc  00000000  001dd1b8  0019f75c  03b2988c  001ff728  001dd1b8 <

0006a122>

03ee9d70: 00000001 <000ccd88> 001dd1b8 <000cce90> 03b29800  001dd1b8  001cd230

03b298ac

03ee9d90: 000000ac  00000000 <0014b4a4><0014b4cc> 03b29a48 <000ccfe8> 03b29800

001dd1b8

03ee9db0: 001ff728  03b298ac  001dc748  001ff728  00000000 <000cc6a6> 000ccf7c

001dc748

03ee9dd0: 00000000  03ee9de4  03a7db60 <000a848c> 001b6024  03ed68f8  03b29848 <

000ccd3e>

03ee9df0: 001b6024  00000000  03a7db60  00000000  03ee9e24  03ee9e24 <000cca58>

000ccf7c

03ee9e10:<000cca76><000cd138> 03b039a0  001dd124  00192c8c  0019f75c  00000000 <

000cd138>

03ee9e30: 001b6024  001dd1b8  001ff728  00000000  00000000  00000000  00000000

00000000

03ee9e50:<00001028> 001b6024  001f843c  00000000  00000000  00000000  03ee6bc0

001e183c

03ee9e70: 00000010  03ee8000  000040d0  00000000  00000001  000240d0  00000000

00000000

03ee9e90: 001e183c  00000001  00000044  03ee8000  03ee8000  03ee8000  000240d0

03ee8000

03ee9eb0: 00000010  0070dac0  00000000  00000000  00000000  00000000  00000000

00000001

03ee9ed0: 00000000  00000000  ffffffff  03ee9f0c <000a7744> 03ed6940  03ed5a40

001c24ec

03ee9ef0:<000a77b8> 03efb6a4  00000000  000000fc  001c24ec  000000d0  03ee9f0c

03ee5e10

03ee9f10: 00000000  00000000 <00189f20><000a791e> 001c24ec  03ed5a40  00000000 <

0006527c>

03ee9f30: 03ed6940  03ed5a40  001ff728  03ee9f60  00004000  00000000  00000000

00000000

03ee9f50: 001c24ec  03ee9f60 <000654a0> 001d54f8  000000fc <000654ae> 001d54f8

001c19f8

03ee9f70: 03ed6940  03ed5a40  03ee9f9c  7fffff00  00000001 <0002a2de> 03ee9f9c

00000076

03ee9f90: 0000000e <00065572> 03ed5a40  00383131  00000000  001f0000 <0002a33a>

001d394c

03ee9fb0: 001ff4b0  00000076  001d54f8 <001e43a0> 001ff6c4  001ff4b0  00000000

00000000

03ee9fd0: 00000000  00000000  00000000  00000000  00000000 <0000145e> 00000000

00000000

03ee9ff0: 00000000  00000000  ffffffff  00000006

Return addresses in stack:

    address : <0x0000e8b0> { _warn_slowpath + 0x58 }

    address : <0x0000e8b4> { _warn_slowpath + 0x5c }

    address : <0x000a7744> { _ida_get_new_above + 0x94 }

    address : <0x0004854a> { _ifind + 0xe }

    address : <0x000a7744> { _ida_get_new_above + 0x94 }

    address : <0x0004854a> { _ifind + 0xe }

    address : <0x00069d6a> { _sysfs_new_dirent + 0x42 }

    address : <0x000485c6> { _ilookup5 + 0x2e }

    address : <0x00069c86> { _sysfs_add_one + 0x3a }

    address : <0x0006aa26> { _sysfs_do_create_link + 0x82 }

    address : <0x000a843e> { _kobject_add_varg + 0x12 }

   frame  1 : <0x0006ab3c> { _sysfs_create_link + 0xc }

    address : <0x000cb310> { _device_add + 0x5c }

    address : <0x000cb500> { _device_add + 0x24c }

    address : <0x000cab7c> { _dev_set_name + 0x1c }

    address : <0x000cb012> { _device_initialize + 0x2a }

    address : <0x000ef02e> { _mmc_add_host + 0x22 }

    address : <0x000f8c06> { _mmc_spi_probe + 0xf6 }

    address : <0x000f8d4a> { _mmc_spi_probe + 0x23a }

    address : <0x0006a122> { _create_dir + 0x3a }

    address : <0x000ccd88> { _driver_sysfs_add + 0x44 }

    address : <0x000cce90> { _driver_probe_device + 0x80 }

    address : <0x0014b4a4> { _klist_next + 0x20 }

    address : <0x0014b4cc> { _klist_next + 0x48 }

    address : <0x000ccfe8> { ___driver_attach + 0x6c }

    address : <0x000cc6a6> { _bus_for_each_dev + 0x3e }

    address : <0x000a848c> { _kobject_init_and_add + 0x24 }

    address : <0x000ccd3e> { _driver_attach + 0x1a }

    address : <0x000cca58> { _bus_add_driver + 0x64 }

    address : <0x000cca76> { _bus_add_driver + 0x82 }

    address : <0x000cd138> { _driver_register + 0x40 }

    address : <0x000cd138> { _driver_register + 0x40 }

    address : <0x00001028> { _do_one_initcall + 0x28 }

    address : <0x000a7744> { _ida_get_new_above + 0x94 }

    address : <0x000a77b8> { _ida_get_new_above + 0x108 }

    address : <0x00189f20> /* kernel dynamic memory */

    address : <0x000a791e> { _ida_pre_get + 0xe }

    address : <0x0006527c> { _proc_register + 0x30 }

    address : <0x000654a0> { _create_proc_entry + 0x3c }

    address : <0x000654ae> { _create_proc_entry + 0x4a }

    address : <0x0002a2de> { _register_irq_proc + 0x76 }

    address : <0x00065572> { _proc_mkdir_mode + 0x2e }

    address : <0x0002a33a> { _init_irq_proc + 0x42 }

    address : <0x001e43a0> { _kernel_init + 0x84 }

    address : <0x0000145e> { _kernel_thread_helper + 0x6 }

---[ end trace 101e6d9fc0e40a34 ]---

TranslateQuoteReplyEditDelete

2010-07-15 09:33:16     Re: error after update my kernel!

Mike Frysinger (UNITED STATES)

Message: 91300   

post the kernel config you're actually using

what files exactly have you modified ?

  • Created
Was this helpful?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.