2010-05-06 05:44:29     BF548 ezkit high speed usb bulk read problems

2010-05-06 05:44:29     BF548 ezkit high speed usb bulk read problems

Ian Guest (SOUTH AFRICA)

Message: 89173   

Dear USB experts

I have worked on the BF548 (EZKIT and Bluetchnix) host USB before. I have now got a problem where I am trying to talk to a vendor supplied Cypress FX2 based high speed USB device. As part of the setup, I have to load the device firmware to the peripheral using control messages. To do this I ported FXLOAD to libusb, and this works as the device is recoconfigured, reset and reappears with the correct (changed) PID. I have verified the load by transferring to a desktop and continuing.

The code I have written uses Libusb, and I have cross compiled it for Windows and Suse (where it works. The problem occurs when a bulk read is issued to the device on end point 84. The desktop machines receive zeros for a while and then they receive some bytes triggering the transactions required. On the EZKIT, I only receive zeros.

I suspect there is some problem with the high speed transfers or power (I have mounted 100uF cap and tried throuh a powered hub). I have also checked the USB_PLL multiplier setting as to be 20 - which it is (full setting 0x30a8). I have used usbmon on both the blackfin and the suse box (included) which shows the deviation as described as the bulk reads start.

I have also included the dmesg on both systems. On the blackfin I run through a telnet session so as to keep the system messages uncluttered.

The USB descriptor of the configured device is as follows:

Dev #119: 1512 PIPE PROFILER v1.0 - MARINE ELECTRONICS 1512

  wTotalLength:         60

  bNumInterfaces:       1

  bConfigurationValue:  1

  iConfiguration:       0

  bmAttributes:         a0h

  MaxPower:             50

    bInterfaceNumber:   0

    bAlternateSetting:  0

    bNumEndpoints:      6

    bInterfaceClass:    255

    bInterfaceSubClass: 0

    bInterfaceProtocol: 0

    iInterface:         0

      bEndpointAddress: 81h

      bmAttributes:     02h

      wMaxPacketSize:   64

      bInterval:        0

      bRefresh:         0

      bSynchAddress:    0

      bEndpointAddress: 01h

      bmAttributes:     02h

      wMaxPacketSize:   64

      bInterval:        0

      bRefresh:         0

      bSynchAddress:    0

      bEndpointAddress: 02h

      bmAttributes:     02h

      wMaxPacketSize:   64

      bInterval:        0

      bRefresh:         0

      bSynchAddress:    0

      bEndpointAddress: 84h

      bmAttributes:     02h

      wMaxPacketSize:   64

      bInterval:        0

      bRefresh:         0

      bSynchAddress:    0

      bEndpointAddress: 86h

      bmAttributes:     02h

      wMaxPacketSize:   64

      bInterval:        0

      bRefresh:         0

      bSynchAddress:    0

      bEndpointAddress: 88h

      bmAttributes:     02h

      wMaxPacketSize:   64

      bInterval:        0

      bRefresh:         0

      bSynchAddress:    0

The simplified program is as follows (after configuration - I use a usb_reset and usb_close after configuring):

dh = usb_open(dev);

#if

defined(LIBUSB_HAS_GET_DRIVER_NP)

#if

printf("Seeing if a driver has claimed the interface");

printf("interface %i already claimed by %s - will try detach",0,name);

printf("%s\n", usb_strerror());

}

defined(LIBUSB_HAS_DETACH_KERNEL_DRIVER_NP)if (LIBUSBLOG_usb_get_driver_np(dh, 0, (char *) name, sizeof(name)) == 0) {if (LIBUSBLOG_usb_detach_kernel_driver_np(dh, 0) < 0) {return;}

#endif

#endif

res = usb_set_configuration(dh,1);

res = usb_claim_interface(dh, 0);res = usb_set_altinterface(dh, 0);

retval = usb_bulk_read(dh, 0x84 ,outBuffer,outBufferSize,1000);

ANY help in debugging or getting the high speed bulk reads going will be much appreciated

Ian Guest

QuoteReplyEditDelete

2010-05-06 05:53:34     Re: BF548 ezkit high speed usb bulk read problems

Ian Guest (SOUTH AFRICA)

Message: 89174   

Here are the files.

suse dmesg.txt

blackfin dmesg.txt

usbmonblackfin.txt

usbmon suse.txt

QuoteReplyEditDelete

2010-05-06 14:23:30     Re: BF548 ezkit high speed usb bulk read problems

Mike Frysinger (UNITED STATES)

Message: 89197   

have you checked the async port timings ?

also, have you asked Cypress about working with their part ?

QuoteReplyEditDelete

2010-05-06 14:56:26     Re: BF548 ezkit high speed usb bulk read problems

Ian Guest (SOUTH AFRICA)

Message: 89199   

Could you tell me where the asynch settings are? And what they should be?

QuoteReplyEditDelete

2010-05-07 09:23:23     Re: BF548 ezkit high speed usb bulk read problems

Ian Guest (SOUTH AFRICA)

Message: 89225   

I looked around. These settings seem to apply to the external asynchronous bus. I am using the BF548 internal Inventra USB OTG controller? Are there any other settings to increase the amount of debug information coming out?

QuoteReplyEditDelete

2010-05-07 14:11:17     Re: BF548 ezkit high speed usb bulk read problems

Robin Getz (UNITED STATES)

Message: 89236   

Ian:

The Cypress FX2 based high speed USB device that you were talking about - that's the USB controller on the async bus? or that is the USB device on the other end of the USB cable?

-Robin

QuoteReplyEditDelete

2010-05-07 16:08:30     Re: BF548 ezkit high speed usb bulk read problems

Ian Guest (SOUTH AFRICA)

Message: 89239   

Sorry if it was unclear - it is on the other side of the cable. I am using a type A (host) connector to connect the device to the EZKIT.

QuoteReplyEditDelete

2010-05-08 18:09:52     Re: BF548 ezkit high speed usb bulk read problems

Mike Frysinger (UNITED STATES)

Message: 89254   

you can try toggling the musb dma/pio option in the kernel config to see if that makes a difference

QuoteReplyEditDelete

2010-05-09 11:37:33     Re: BF548 ezkit high speed usb bulk read problems

Ian Guest (SOUTH AFRICA)

Message: 89268   

Thank you Mike - I have already tried that with no success. Do you have any other ideas?

QuoteReplyEditDelete

2010-05-10 17:25:59     Re: BF548 ezkit high speed usb bulk read problems

Mike Frysinger (UNITED STATES)

Message: 89294    can you force the lowest speed possible to see if it makes a difference ?

perhaps double check the cable to make sure you're using the right tips ...

otherwise, a USB analyzer might help to compare the traffic between

the two parts

QuoteReplyEditDelete

2010-05-12 11:11:05     Re: BF548 ezkit high speed usb bulk read problems

Ian Guest (SOUTH AFRICA)

Message: 89337   

Hi Mike

As another option I ported the code to an OMAP with an Inventra USB OTG and it works there. A difference is that the libusb is version 1.0 with a layer using libusb-compat-0.1 so that it looks like the old libusb v0.1.12.

I tried to compile it for the blackfin manually - but it causes an error: Dmesg attached.

Could the old version of libusb be the problem?

Ian

libusb1_dmesg.txt

  • Created
Was this helpful?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.