2010-03-25 12:56:46     why my bf531 can't get right picture?

2010-03-25 12:56:46     why my bf531 can't get right picture?

macgrady tracy (CHINA)

Message: 87695   

hello,every one,

There is a question puzzing me for a long time

i am use bfin531 and ov7670 coms senser to capture picture

i am sure the ov7670 sensor is OK, and when i use the testing mode of ov7670 i can get the correct picture

but when i try to get capture a pict of my own, the pict is black, most of the pict is black!!!!

my question is :

what is the correct of BF531's PPI  I/O volt?  3.3v? 2.8v? 2.5v? or when the input volt is 2.2v, blackfin can recognize the I/O volt?

any one who can help me?

thanks!!!

QuoteReplyEditDelete

2010-03-25 21:54:14     Re: why my bf531 can't get right picture?

macgrady tracy (CHINA)

Message: 87703   

ps:

i means the picture  is dark ....

The blackfin PPI port read the 2.2V  is  "0" or "1"

Blackfin can support OV sensor?

QuoteReplyEditDelete

2010-03-26 05:14:56     Re: why my bf531 can't get right picture?

Michael Hennerich (GERMANY)

Message: 87733    > The blackfin PPI port read the 2.2V is "0" or "1"

This depends on VDDext. For VDDext = 3.3V it may read 1 on the PPI pins, but not sure it will also work on the PPICLK since VIHCLKINmin = 2.2V @ VDDextmax = 3.6Volt.

> Blackfin can support OV sensor?

You have several choices:

1) Increase OV Sensor IO-Voltage.

2) Reduce Blackfin VDDext

3) Use level shifters

QuoteReplyEditDelete

2010-04-01 05:05:16     Re: why my bf531 can't get right picture?

macgrady tracy (CHINA)

Message: 87972   

thanks for you replay!

I have resolved this problem,

the reson of the picture  dark is that  the I2C(on platform of OV we call it SCCB) not been set correct!

thanks!!!

  • Created
Was this helpful?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.