2010-03-24 06:43:47 a problem about creat a node under /dev Automatically
zhang zhihua (CHINA)
Message: 87662
我想在加载驱动程序的时候就自动在/dev目录创建一个设备节点,我首先用class_create(…)函创建一个类my_class,这个类存放于sysfs下面,再调用device_create(…)函数来在/dev目录下创建test_dev设备节点,具体代码如下:
{
my_class = class_create(THIS_MODULE, "my_class");
if(IS_ERR(my_class))
{
printk("Err: failed in creating class.\n");
return -1;
}
device_create( my_class, NULL, MKDEV(major, minor), "test_dev""%d", 0 );
}
{
static void test_cleanup(void)
{
cdev_del(&test_dev);
class_destroy(my_class);
device_destroy(my_class, MKDEV(major, minor)); //delete device node under /dev
unregister_chrdev_region(MKDEV(major, minor), DEVNUM);
printk("Test device uninstalled\n");
}
}
但是我系统启动的时候却出现下面错误:
nari> bootm 1000000
## Booting kernel from Legacy Image at 01000000 ...
Image Name: Linux-2.6.28.10-ADI-2009R1
Created: 2010-03-24 9:39:59 UTC
Image Type: Blackfin Linux Kernel Image (gzip compressed)
Data Size: 3565280 Bytes = 3.4 MB
Load Address: 00001000
Entry Point: 00234bac
Verifying Checksum ... OK
Uncompressing Kernel Image ... OK
Starting Kernel at = 00234bac
Linux version 2.6.28.10-ADI-2009R1 (root@ubuntu) (gcc version 4.1.2 (ADI svn)) #
324 Wed Mar 24 02:39:40 PDT 2010
bootconsole [early_shadow0] enabled
bootconsole [early_BFuart0] enabled
early printk enabled on early_BFuart0
Board Memory: 32MB
Kernel Managed Memory: 32MB
Memory map:
fixedcode = 0x00000400-0x00000490
text = 0x00001000-0x0017b500
rodata = 0x0017b500-0x001ea520
bss = 0x001eb000-0x00211af8
data = 0x00211af8-0x00228000
stack = 0x00226000-0x00228000
init = 0x00228000-0x00644000
available = 0x00644000-0x01eff000
DMA Zone = 0x01f00000-0x02000000
Hardware Trace Active and Enabled
Boot Mode: 3
Blackfin support (C) 2004-2009 Analog Devices, Inc.
Compiled for ADSP-BF518 Rev 0.0
Warning: Compiled for Rev 0, but running on Rev 1
Blackfin Linux support by blackfin.uclinux.org/
Processor Speed: 400 MHz core clock and 80 MHz System Clock
NOMPU: setting up cplb tables
Instruction Cache Enabled for CPU0
Data Cache Enabled for CPU0 (write-back)
Built 1 zonelists in Zone order, mobility grouping off. Total pages: 7873
Kernel command line: root=/dev/mtdblock3 rw rootfstype=jffs2 clkin_hz=25000000 e
arlyprintk=serial,uart0,57600 console=ttyBF0,57600
Configuring Blackfin Priority Driven Interrupts
PID hash table entries: 128 (order: 7, 512 bytes)
I-pipe 1.10-00: pipeline enabled.
Console: colour dummy device 80x25
console [ttyBF0] enabled, bootconsole disabled
console [ttyBF0] enabled, bootconsole disabled
Dentry cache hash table entries: 4096 (order: 2, 16384 bytes)
Inode-cache hash table entries: 2048 (order: 1, 8192 bytes)
Memory available: 25032k/32768k RAM, (4208k init code, 1513k kernel code, 691k d
ata, 1024k dma, 296k reserved)
Calibrating delay loop... 794.62 BogoMIPS (lpj=1589248)
Security Framework initialized
Mount-cache hash table entries: 512
Blackfin Scratchpad data SRAM: 4 KB
Blackfin L1 Data A SRAM: 16 KB (15 KB free)
Blackfin L1 Data B SRAM: 16 KB (16 KB free)
Blackfin L1 Instruction SRAM: 48 KB (42 KB free)
net_namespace: 288 bytes
NET: Registered protocol family 16
Blackfin DMA Controller
ezbrd_init(): registering device resources
NET: Registered protocol family 2
IP route cache hash table entries: 1024 (order: 0, 4096 bytes)
TCP established hash table entries: 1024 (order: 1, 8192 bytes)
TCP bind hash table entries: 1024 (order: 0, 4096 bytes)
TCP: Hash tables configured (established 1024 bind 1024)
TCP reno registered
NET: Registered protocol family 1
I-pipe: Domain Xenomai registered.
Xenomai: hal/blackfin started.
Xenomai: real-time nucleus v2.4.7 (Andalusia) loaded.
Xenomai: starting default API services.
Xenomai: starting POSIX services.
Xenomai: starting RTDM services.
NTFS driver 2.1.29 [Flags: R/O].
JFFS2 version 2.2. (NAND) (SUMMARY) 漏 2001-2006 Red Hat, Inc.
msgmni has been set to 48
io scheduler noop registered (default)
The major of the gpio device is 110
Registered character driver
The major of the test device is 253
NULL pointer access
Kernel OOPS in progress
Deferred Exception context
CURRENT PROCESS:
COMM=swapper PID=1
CPU = 0
invalid mm
return address: [0x000d7cee]; contents of:
0x000d7cc0: 05e3 e800 0044 0c81 e630 004d e631 004e
0x000d7cd0: e632 004f e534 0050 1402 228a e530 004d
0x000d7ce0: e531 004e 5bc8 0a78 14e6 e531 004f [9949]
0x000d7cf0: 4308 0c00 19f3 e533 004d 612a 0810 1820
ADSP-BF518-0.0(Detected 0.1) 400(MHz CCLK) 80(MHz SCLK) (mpu off)
Linux version 2.6.28.10-ADI-2009R1
Built with gcc version 4.1.2 (ADI svn)
SEQUENCER STATUS: Not tainted
SEQSTAT: 00000027 IPEND: 8030 SYSCFG: 0006
EXCAUSE : 0x27
interrupts disabled
physical IVG5 asserted : <0xffa00bfc> { _evt_ivhw + 0x0 }
physical IVG15 asserted : <0xffa00da8> { _evt_system_call + 0x0 }
logical irq 6 mapped : <0xffa00310> { _timer_interrupt + 0x0 }
RETE: <0x00000000> /* Maybe null pointer? */
RETN: <0x01ee9cb4> /* kernel dynamic memory */
RETX: <0x00000480> /* Maybe fixed code section */
RETS: <0x000f6cb8> { _device_create_vargs + 0x68 }
PC : <0x000d7cee> { _vsnprintf + 0x2e }
DCPLB_FAULT_ADDR: <0x00000000> /* Maybe null pointer? */
ICPLB_FAULT_ADDR: <0x000d7cee> { _vsnprintf + 0x2e }
PROCESSOR STATE:
R0 : 01970c8c R1 : 00000014 R2 : 00000000 R3 : 01970e00
R4 : 001caf44 R5 : 00000000 R6 : 0fd00000 R7 : 01e8e220
P0 : 01970c8c P1 : 00000000 P2 : 01970e00 P3 : 0020d484
P4 : 01ee9e44 P5 : 01970c00 FP : 01970ca0 SP : 01ee9bd8
LB0: 000d868c LT0: 000d868c LC0: 00000000
LB1: 00070bc8 LT1: 00070bb6 LC1: 00000000
B0 : 00000000 L0 : 00000000 M0 : 00000000 I0 : 00000003
B1 : 00000000 L1 : 00000000 M1 : 00000000 I1 : 019c9d44
B2 : 00000000 L2 : 00000000 M2 : 00000000 I2 : 00000000
B3 : 00000000 L3 : 00000000 M3 : 00000000 I3 : 00000000
A0.w: 00000000 A0.x: 00000000 A1.w: 00000000 A1.x: 00000000
USP : 00000000 ASTAT: 00003024
Hardware Trace:
0 Target : <0x00004d34> { _trap_c + 0x0 }
Source : <0xffa005f6> { _exception_to_level5 + 0xae } CALL pcrel
1 Target : <0xffa00548> { _exception_to_level5 + 0x0 }
Source : <0xffa00404> { _bfin_return_from_exception + 0x18 } RTX
2 Target : <0xffa003ec> { _bfin_return_from_exception + 0x0 }
Source : <0xffa004a0> { _ex_trap_c + 0x6c } JUMP.S
3 Target : <0xffa00434> { _ex_trap_c + 0x0 }
Source : <0xffa006c0> { _trap + 0x58 } JUMP (P4)
4 Target : <0xffa00668> { _trap + 0x0 }
Source : <0x000d7cea> { _vsnprintf + 0x2a } 0xe531
5 Target : <0x000d7cdc> { _vsnprintf + 0x1c }
Source : <0x000d7cd8> { _vsnprintf + 0x18 } IF CC JUMP
6 Target : <0x000d7cc0> { _vsnprintf + 0x0 }
Source : <0x000f6cb4> { _device_create_vargs + 0x64 } CALL pcrel
7 Target : <0x000f6c7c> { _device_create_vargs + 0x2c }
Source : <0x0006190a> { _kmem_cache_alloc + 0x66 } RTS
8 Target : <0x00061902> { _kmem_cache_alloc + 0x5e }
Source : <0x0006192e> { _kmem_cache_alloc + 0x8a } JUMP.S
9 Target : <0x0006192e> { _kmem_cache_alloc + 0x8a }
Source : <0x000d8692> { _memset + 0x2e } RTS
10 Target : <0x000d8664> { _memset + 0x0 }
Source : <0x0006192a> { _kmem_cache_alloc + 0x86 } CALL pcrel
11 Target : <0x00061924> { _kmem_cache_alloc + 0x80 }
Source : <0x00061900> { _kmem_cache_alloc + 0x5c } IF !CC JUMP
12 Target : <0x000618fa> { _kmem_cache_alloc + 0x56 }
Source : <0x0002e1ca> { ___ipipe_unstall_root + 0x2a } RTS
13 Target : <0x0002e1a0> { ___ipipe_unstall_root + 0x0 }
Source : <0x0002e1fe> { ___ipipe_restore_root + 0x2a } JUMP.L
14 Target : <0x0002e1fe> { ___ipipe_restore_root + 0x2a }
Source : <0x0002e1d6> { ___ipipe_restore_root + 0x2 } IF !CC JUMP
15 Target : <0x0002e1d4> { ___ipipe_restore_root + 0x0 }
Source : <0x000618f6> { _kmem_cache_alloc + 0x52 } CALL pcrel
Kernel Stack
Stack info:
SP: [0x01ee9c7c] <0x01ee9c7c> /* kernel dynamic memory */
FP: (0x01ee9cc0)
Memory from 0x01ee9c70 to 01eea000
01ee9c70: 01970c00 01ee9e44 0020d484 [01970e00] 00000000 01970c8c 01e8e220
0fd00000
01ee9c90: 00000000 001caf44 01970e00 00000000 00000014 01970c8c 01970c8c
01970c8c
01ee9cb0: 00000006 01ee8000 01ee8000 01ee8000 (01ee9d38)<0017a8c4> 00217e78
01ee8000
01ee9cd0: 01ee8000 7fffffff 00000000 01ee9d68 00000002 0020c444 00000001
01ee9d68
01ee9cf0: 001ca238 01efe8e0 01ef72f8 01ee9d34 <0000d9b2> 00000000 <0017a67c>
00217e78
01ee9d10: 7fffffff <0017a6d2> 01eca800 01efe8e0 01ece9e0 00000001 01ee6bc0
0000a80c
01ee9d30: 00100100 00200200 (00000000)<0001c9c4> 01e8e1e0 01ece9e0 0020c444 <
0001c9cc>
01ee9d50: 01e8e1e0 fffffffe <0001c9cc> 01ee9da0 0197d000 000007bb 00000000
01ee9d6c
01ee9d70: 01ee9d6c <000d44be> 0197d010 00000004 <000d44be> 01973ca0 01efac68
00000006
01ee9d90: 000000d0 000000d0 019ce780 0197d000 0021b6ac 01efe8e0 00000000
01e8e220
01ee9db0:<000d3e76> 01973ca0 <000d3cfe> 01973ca0 00000000 00000000 <000f6cb8>
01970c00
01ee9dd0: 00000000 0020d484 01e8e220 0fd00000 00000000 001caf44 01970c8c
00000014
01ee9df0: 00000000 01ee9e44 <000f6cfa> 0020d490 01ee9e44 0021bc48 00000000
00000000
01ee9e10: 01ee2c00 01ee9e34 001caf44 00000000 01ee9e44 01ee9e44 <000e7d6e>
0fd00000
01ee9e30: 0020d448 000000fd ffffffff 001caf44 00000000 0fd00000 <00001028>
001eb024
01ee9e50: 000e7c9c 00244054 00000000 00000000 00000000 00000000 00000000 <
ffa00b98>
01ee9e70: 0008f328 00008050 00000026 00000000 00000000 00000000 0008f328 <
0008f278>
01ee9e90: 00000006 02003004 000d7b4e 000d868c 000d7b42 000d868c 00000000
00000000
01ee9eb0: 00000000 00000000 00000000 00000000 00000000 00000000 00000000
00000000
01ee9ed0: 00000000 ffffffff 01ee9f08 <000d32f2> 01ec6940 <000d2fea> 0020aa8c <
000d3366>
01ee9ef0: 0068e6a4 00000000 00000000 00000000 000080d0 01ee9f08 00000000
ffffffff
01ee9f10: 01ee9f40 <000d32f2> 01ec5920 <000d2fea> 0020aa8c <000d3366> 0068e6a4
00000000
01ee9f30:<000d3366> 0020aa8c 000080d0 01ee9f40 01ee5e10 00000000 00000000
00000000
01ee9f50:<000d352a> 0020aa8c 01ec59e0 00000000 <0008f278> 01ec5920 01ec59e0
00244054
01ee9f70: 01ee9f94 00004000 00000000 00000000 00000000 01ee9f98 01ee9f94 <
0008f49c>
01ee9f90: 001faa78 000000ff <0008f4aa> 001faa78 00243dd0 01ec5920 01ec5980
00243dd0
01ee9fb0: 00000076 00000001 <0002db86><002283a4> 00243f94 00243dd0 00000000
00000000
01ee9fd0: 00000000 00000000 00000000 00000000 00000000 <00001456> 00000000
00000000
01ee9ff0: 00000000 00000000 ffffffff 00000006
Return addresses in stack:
frame 1 : <0x0017a8c4> { _schedule_timeout + 0x6c }
address : <0x0000d9b2> { ___wake_up + 0x56 }
address : <0x0017a67c> { _wait_for_common + 0x9c }
address : <0x0017a6d2> { _wait_for_common + 0xf2 }
frame 2 : <0x0001c9c4> { _call_usermodehelper_exec + 0x44 }
address : <0x0001c9cc> { _call_usermodehelper_exec + 0x4c }
address : <0x0001c9cc> { _call_usermodehelper_exec + 0x4c }
address : <0x000d44be> { _kobject_uevent_env + 0xca }
address : <0x000d44be> { _kobject_uevent_env + 0xca }
address : <0x000d3e76> { _kset_register + 0x32 }
address : <0x000d3cfe> { _kobject_get + 0x12 }
address : <0x000f6cb8> { _device_create_vargs + 0x68 }
address : <0x000f6cfa> { _device_create + 0x1a }
address : <0x000e7d6e> { _test_init + 0xd2 }
address : <0x00001028> { _do_one_initcall + 0x28 }
address : <0xffa00b98> { __common_int_entry + 0x6c }
address : <0x0008f278> { _proc_register + 0x30 }
address : <0x000d32f2> { _ida_get_new_above + 0x92 }
address : <0x000d2fea> { _get_from_free_list + 0x4e }
address : <0x000d3366> { _ida_get_new_above + 0x106 }
address : <0x000d32f2> { _ida_get_new_above + 0x92 }
address : <0x000d2fea> { _get_from_free_list + 0x4e }
address : <0x000d3366> { _ida_get_new_above + 0x106 }
address : <0x000d3366> { _ida_get_new_above + 0x106 }
address : <0x000d352a> { _ida_pre_get + 0xe }
address : <0x0008f278> { _proc_register + 0x30 }
address : <0x0008f49c> { _create_proc_entry + 0x3c }
address : <0x0008f4aa> { _create_proc_entry + 0x4a }
address : <0x0002db86> { ___ipipe_add_domain_proc + 0x1e }
address : <0x002283a4> { _kernel_init + 0x88 }
address : <0x00001456> { _kernel_thread_helper + 0x6 }
Modules linked in:
Kernel panic - not syncing: Kernel exception
TranslateQuoteReplyEditDelete
2010-03-24 12:39:59 Re: a problem about creat a node under /dev Automatically
Mike Frysinger (UNITED STATES)
Message: 87670
you really need to read some basic linux books. the wiki has pointers to plenty of free ones -- go start there.
i'm pretty sure you cant give device_create() a NULL parent.
QuoteReplyEditDelete
2010-03-24 21:23:25 Re: a problem about creat a node under /dev Automatically
zhang zhihua (CHINA)
Message: 87678
sorry,Mike,
In this area, I was a novice!
But if I want to creat a char device driver ,which is the parent?
I am very urgent to solve this problem ,thank you!
This is the code:
static int test_init(void)
{
int result;
dev_t dev = MKDEV(major,minor); /*MKDEV 实现主次设备号的组合来获得dev */
if (major)
{
result = register_chrdev_region(dev,DEVNUM,TEST_DEVICE_NAME);//
}
else
{
result = alloc_chrdev_region(&dev,minor,DEVNUM,TEST_DEVICE_NAME);
major = MAJOR(dev);
}
if (result < 0)
{
printk(KERN_WARNING "test: unable to get major %d\n", major);
return result;
}
/*1st function*/
test_setup_cdev(&test_dev, minor, &test_fops);
printk (KERN_INFO "Registered character driver\n");
printk("The major of the test device is %d\n", major);
/* create your own class under /sysfs */
my_class = class_create(THIS_MODULE, "my_class");
if(IS_ERR(my_class))
{
printk("Err: failed in creating class.\n");
return -1;
}
/* register your own device in sysfs, and this will cause udev to create corresponding device node */
device_create( my_class,NULL, MKDEV(major, minor), "test_dev""%d", 0 );
return 0;
}
/************************************************************************
* NAME: test_cleanup
* FUNCTION:驱动程序卸载函数
* 参数值:
******************************************************************* ******/
static void test_cleanup(void)
{
cdev_del(&test_dev);
class_destroy(my_class);
device_destroy(my_class, MKDEV(major, minor)); //delete device node under /dev
unregister_chrdev_region(MKDEV(major, minor), DEVNUM);
printk("Test device uninstalled\n");
}
/***********************************************************************************/
module_init(test_init);
module_exit(test_cleanup);