2010-03-18 22:44:41     passing argument 2 of ‘request_irq’ from incompatible pointer type

2010-03-18 22:44:41     passing argument 2 of ‘request_irq’ from incompatible pointer type

zhang zhihua (CHINA)

Message: 87433   

我想申请一个中断处理函数,使用下面的函数:

static irqreturn_t  irq_task1(int irq,void *dev_id,struct pt_regs *regs)

{

printk("This is the irq_task!\n");

/**********************************************/

//调用处理函数

/**********************************************/

  return IRQ_HANDLED;

}

{

int ret;

ret = request_irq (UART1_IRQNO,irq_task1,IRQF_SHARED,TEST_DEVICE_NAME,NULL);

}

但是编译却出现如下告警:warning:passing argument 2 of ‘request_irq’ from incompatible pointer type

什么地方有问题呢?

而且将驱动添加到内核之后编写了一个最简单的test程序调用open函数,出现如下:

root:~> ./test

Welcome to the driver open function!

Welcome to the driver ioctl function!

Trying to free already-free IRQ 107

Hardware Trace:

   0 Target : <0x00004bac> { _dump_stack + 0x0 }

     Source : <0x0002b85e> { _free_irq + 0x106 } CALL pcrel

   1 Target : <0x0002b85e> { _free_irq + 0x106 }

     Source : <0x000101da> { _printk + 0x66 } RTS

   2 Target : <0x000101d0> { _printk + 0x5c }

     Source : <0x00010c00> { _vprintk + 0x14c } RTS

   3 Target : <0x00010bf4> { _vprintk + 0x140 }

     Source : <0x0002e1fc> { ___ipipe_restore_root + 0x28 } RTS

   4 Target : <0x0002e1d4> { ___ipipe_restore_root + 0x0 }

     Source : <0x00010bf0> { _vprintk + 0x13c } CALL pcrel

   5 Target : <0x00010be8> { _vprintk + 0x134 }

     Source : <0x00010d32> { _vprintk + 0x27e } JUMP.S

   6 Target : <0x00010d32> { _vprintk + 0x27e }

     Source : <0x0000fc86> { _wake_up_klogd + 0x1a } RTS

   7 Target : <0x0000fc6c> { _wake_up_klogd + 0x0 }

     Source : <0x000105d4> { _release_console_sem + 0x1e0 } JUMP.L

   8 Target : <0x000105cc> { _release_console_sem + 0x1d8 }

     Source : <0x000105c0> { _release_console_sem + 0x1cc } IF !CC JUMP

   9 Target : <0x000105be> { _release_console_sem + 0x1ca }

     Source : <0x0002e1fc> { ___ipipe_restore_root + 0x28 } RTS

  10 Target : <0x0002e1d4> { ___ipipe_restore_root + 0x0 }

     Source : <0x000105ba> { _release_console_sem + 0x1c6 } CALL pcrel

  11 Target : <0x000105b2> { _release_console_sem + 0x1be }

     Source : <0x0002e1fc> { ___ipipe_restore_root + 0x28 } RTS

  12 Target : <0x0002e1d4> { ___ipipe_restore_root + 0x0 }

     Source : <0x00023134> { _up + 0x50 } JUMP.L

  13 Target : <0x000230e4> { _up + 0x0 }

     Source : <0x000105ae> { _release_console_sem + 0x1ba } CALL pcrel

  14 Target : <0x0001059a> { _release_console_sem + 0x1a6 }

     Source : <0x00010464> { _release_console_sem + 0x70 } IF !CC JUMP

  15 Target : <0x00010424> { _release_console_sem + 0x30 }

     Source : <0x0001057c> { _release_console_sem + 0x188 } JUMP.S

Stack info:

SP: [0x01905e60] <0x01905e60> /* kernel dynamic memory */

FP: (0x01905e78)

Memory from 0x01905e60 to 01906000

01905e60:[00217d74]<0002b862> 00000000  0000006b  01905e9c  0000006b (00000000)<000e7ede>

01905e80: 007c4970  0059cd20  007c4970  00000008  0041d668  0192f004 <000655c0> 007c4970

01905ea0: 0059cd20 <000655e4> 01905ec4 <0000b03e><0000a5c2> 00000000  00000000  01938ee0

01905ec0:<000630ca> 0059cd20  00000006  01938f78  00000000  005b6160  00000000  00000003

01905ee0: 01904000 <00063152> 005b6160  0059cd20  ffffe000  01938efc  ffa0085a  01904000

01905f00: ffa00816  000630f0  00000000  01931258  01904000  ffffe000  00000001  00000001

01905f20: 0192f004  01925252  00008000  00000000  00000000  01906000  01925252  01925252

01905f40:<019206fc> ffa00e0c  02003025  01928785  01926969  0192873e  01926966  00000008

01905f60: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

01905f80: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

01905fa0: 0000000c  00000000  67452301  003dcf74  00000000  01938ed4  01938ee0  0192f060

01905fc0: 01931258  01938f78  01930ae0  01938ef8  00000006  00000003  0193360c  0192f004

01905fe0: 00000001  00000001  00000000  01938edb  00000003  00000003  00000006  00000006

Return addresses in stack:

    address : <0x0002b862> { _free_irq + 0x10a }

   frame  1 : <0x000e7ede> { _uart_release + 0xe }

    address : <0x000655c0> { ___fput + 0x6c }

    address : <0x000655e4> { ___fput + 0x90 }

    address : <0x0000b03e> { _pick_next_task_fair + 0x46 }

    address : <0x0000a5c2> { _finish_task_switch + 0x1a }

    address : <0x000630ca> { _filp_close + 0x36 }

    address : <0x00063152> { _sys_close + 0x62 }

    address : <0x019206fc> [ test + 0x6bc ]

Welcome to the driver release function!

TranslateQuoteReplyEditDelete

2010-03-18 23:36:12     Re: passing argument 2 of ‘request_irq’ from incompatible pointer type

Mike Frysinger (UNITED STATES)

Message: 87436   

please review a basic C book.  the warning is telling you the problem -- fix your irq handler's prototype.  i dont know where you got that example because it isnt from our documentation:

  docs.blackfin.uclinux.org/doku.php?id=linux-kernel:interrupts

as for the error, dont call free_irq() on already freed irqs -- like it told you.

  • Created
Was this helpful?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.