2010-03-12 07:48:17     makefile

2010-03-12 07:48:17     makefile

Filip Vanalme (BELGIUM)

Message: 87136   

My knowledge about makefiles is rather limited. I would like to do something like this in the Kernel's main makefile to make a 'special' version of the Kernel (e.g. a stripped variant) :

test:

     @echo "**** building special Kernel ****"

# Saving current config files and replace them by the special one's

     cp linux-2.6.x/.config linux-2.6.x/.savedconfig

     cp linux-2.6.x/.specialconfig linux-2.6.x/.config

     cp config/.config config/.savedconfig

     cp config/.specialconfig config/.config

     export TESTING

     $(MAKE) TESTING=1

# restore the original configs

     cp config/.savedconfig config/.config

     cp linux-2.6.x/.savedconfig linux-2.6.x/.config

I looks like this is working when I do make test (I see the copying of files, then the starting of the 'normal' make ...), but I finally get compilation errors.

When I do the first copy part (i.e. the first 4 cp's) manually from the command prompt and let the makefile start with the 'export' line, It works well (no compilation errors).

test:

     @echo "**** building special Kernel ****"

# .config files manually replace from command prompt before calling make

     export TESTING

     $(MAKE) TESTING=1

# restore the original configs

     cp config/.savedconfig config/.config

     cp linux-2.6.x/.savedconfig linux-2.6.x/.config

Can I replace any .config files within the makefile or is this already too late (i.e. the make has already interpreted the .config files before it reaches the replace part) ?

There are probably better ways to do this kind of things, no ?

Filip

TranslateQuoteReplyEditDelete

2010-03-12 08:17:21     Re: makefile

Mike Frysinger (UNITED STATES)

Message: 87137   

since you use $(MAKE), it should a re-processing of the Makefile, but it's probably using the existing environment as a base instead of a fresh one

you could try creating a GNUmakefile that looks like:

all %:

    $(MAKE) -f Makefile $@

test:

... your current test target ...

QuoteReplyEditDelete

2010-03-12 09:35:43     Re: makefile

Filip Vanalme (BELGIUM)

Message: 87138   

Thanks Mike !

It's working now. I created a 'special' makefile that does the copying and finally calls the 'standard' makefile with a parameter.

  • Created
Was this helpful?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.