2010-02-11 05:34:34     VLC test

2010-02-11 05:34:34     VLC test

yihui zhang (AFGHANISTAN)

Message: 85984   

    I followed the wiki   docs.blackfin.uclinux.org/doku.php?id=uclinux-dist:vlc to test VLC on bf527. It didn't work. Who have really tested it? Please give me some help. Any information will be welcome. Thank you.

ps:I used uClinux-dist-2009R1-RC6.tar.bz2

QuoteReplyEditDelete

2010-02-11 20:17:54     Re: VLC test

Yi Li (CHINA)

Message: 85999   

Yihui,

The wiki may be outdated. But you can tell us what error you see? What is your problem?

-Yi

QuoteReplyEditDelete

2010-02-18 22:25:36     Re: VLC test

Peter Naulls (UNITED STATES)

Message: 86211   

Well, it doesn't build.  For 2009R1.1 it's pulling host system headers/libraries:

bfin-linux-uclibc-gcc -DHAVE_CONFIG_H -I. -I../../../vlc-0.8.6b/modules/audio_output -I../..  -I../../intl -DEMBED -D__uClinux__ -I/home/peter/projects/fish/uClinux-dist  -mcpu=bf548-0.2 -DSYS_LINUX -I../../../vlc-0.8.6b/include `top_builddir="../.." ../../vlc-config --cflags builtin pic aout_file` -Wsign-compare -Wall -pipe -Wall -O2      -mcpu=bf548-0.2 -pipe -c -o libaout_file_a-file.o `test -f 'file.c' || echo '../../../vlc-0.8.6b/modules/audio_output/'`file.c                                                                                                                                                  

In file included from ../../../vlc-0.8.6b/include/vlc_threads.h:51,                                                                                     

                 from ../../../vlc-0.8.6b/include/vlc_common.h:467,                                                                                     

                 from ../../../vlc-0.8.6b/include/vlc/vlc.h:153,                                                                                        

                 from ../../../vlc-0.8.6b/modules/audio_output/sdl.c:34:                                                                                

/usr/include/pthread.h:655: warning: '__regparm__' attribute directive ignored                                                                          

/usr/include/pthread.h:667: warning: '__regparm__' attribute directive ignored                                                                          

/usr/include/pthread.h:690: warning: '__regparm__' attribute directive ignored                                                                          

/usr/include/pthread.h:703: warning: '__regparm__' attribute directive ignored                                                                          

/usr/include/pthread.h:712: warning: '__regparm__' attribute directive ignored                                                                          

../../../vlc-0.8.6b/include/vlc_common.h:554: warning: 'GCD' defined but not used                                                                       

../../../vlc-0.8.6b/include/vlc_common.h:554: warning: 'GCD' defined but not used                                                                       

../../../vlc-0.8.6b/include/vlc_common.h:554: warning: 'GCD' defined but not used                                                                       

rm -f libaout_sdl_plugin.a                                                                                                                              

bfin-linux-uclibc-ar cru libaout_sdl_plugin.a libaout_sdl_plugin_a-sdl.o                                                                                

bfin-linux-uclibc-ranlib libaout_sdl_plugin.a                                                                                                           

rm -f libaout_file.a                                                                                                                                    

bfin-linux-uclibc-ar cru libaout_file.a libaout_file_a-file.o                                                                                           

bfin-linux-uclibc-ranlib libaout_file.a                                                                                                                 

/bin/sh ../../libtool --mode=link bfin-linux-uclibc-gcc -Wsign-compare -Wall -pipe -Wall -O2 -mcpu=bf548-0.2 -pipe -mcpu=bf548-0.2 -o libaout_sdl_plugin.so libaout_sdl_plugin.a -shared -lpthread -fpic -fPIC -L/usr/lib -lSDL -u _vlc_entry__0_8_6                                                              

rm -f liboss_plugin.a                                                                                                                                   

bfin-linux-uclibc-ar cru liboss_plugin.a liboss_plugin_a-oss.o                                                                                          

bfin-linux-uclibc-ranlib liboss_plugin.a                                                                                                                

mkdir .libs                                                                                                                                             

bfin-linux-uclibc-gcc -Wsign-compare -Wall -pipe -Wall -O2 -mcpu=bf548-0.2 -pipe -mcpu=bf548-0.2 -o libaout_sdl_plugin.so -shared -fpic -fPIC -u _vlc_entry__0_8_6  libaout_sdl_plugin.a -lpthread -L/usr/lib /usr/lib/libSDL.so                                                                                  

/bin/sh ../../libtool --mode=link bfin-linux-uclibc-gcc -Wsign-compare -Wall -pipe -Wall -O2 -mcpu=bf548-0.2 -pipe -mcpu=bf548-0.2 -o liboss_plugin.so liboss_plugin.a -shared -lpthread -fpic -fPIC -u _vlc_entry__0_8_6                                                                                         

/opt/uClinux/bfin-linux-uclibc/lib/gcc/bfin-linux-uclibc/4.3.3/../../../../bfin-linux-uclibc/bin/ld: skipping incompatible /usr/lib/libpthread.so when searching for -lpthread                                                                                                                                    

/opt/uClinux/bfin-linux-uclibc/lib/gcc/bfin-linux-uclibc/4.3.3/../../../../bfin-linux-uclibc/bin/ld: skipping incompatible /usr/lib/libpthread.a when searching for -lpthread                                                                                                                                     

/usr/lib/libSDL.so: could not read symbols: File in wrong format                      

For trunk, it can't find the ffmpeg headers (I'm building that, but perhaps its headers are not exported):

checking mad.h usability... yes

checking mad.h presence... yes

checking for mad.h... yes

checking for mad_bit_init in -lmad... yes

checking id3tag.h usability... no

checking id3tag.h presence... no

checking for id3tag.h... no

checking for ffmpeg-config... no

checking for FFMPEG... yes

checking ffmpeg/avcodec.h usability... no

checking ffmpeg/avcodec.h presence... no

checking for ffmpeg/avcodec.h... no

configure: error: Missing header file ffmpeg/avcodec.h.

make[4]: *** [build/Makefile] Error 1

QuoteReplyEditDelete

2010-02-24 08:14:06     Re: VLC test

yihui zhang (AFGHANISTAN)

Message: 86450   

Thank you, Yi Li.

The error information is below:

root:/>vlc v4l:/dev/video0:size=cif:fps=15 --sout '#transcode{vcodec=mp4v}:rtp{

dst=192.168.0.101,port=1234,sdp=  192.168.0.107:8080/test.sdp}' --no-audio

--ttl 1

VLC media player 0.8.6b Janus

starting VLC root wrapper... using UID 0 (root)

***************************************

* Running VLC as root is discouraged. *

***************************************

It is potentially dangerous, and might not even work properly.

Remote control interface initialized. Type `help' for help.

status change: ( new input: v4l:/dev/video0:size=cif:fps=15 )

status change: ( audio volume: 256 )

status change: ( play state: 1 )

[00000235] main private: creating httpd

[00000239] v4l demuxer error: cannot get channel infos (Invalid argument)

[00000239] v4l demuxer error: cannot set audio format (16b little endian) (Invalid argument)

[00000239] v4l demuxer error: cannot open device (No such file or directory)

  • Created
Was this helpful?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.