2010-01-26 02:39:35     Userspace Init problems

2010-01-26 02:39:35     Userspace Init problems

Rob Maris (GERMANY)

Message: 85114   

(also with reference to thread 38357)

Yesterday I updated my distribution to current SVN trunk (in a parallel distribution directory, up to now SVN 8023 was used). I took care of taking customizations from the "current" distribution, especially in vendor/....

Now my init gets stuck. However, I can FTP into the Blackfin module (TCM-BF537), and verify that the directory tree seems OK. Solely the JFFS2 formatted user directory isn't visible - due to not executed rc (note: rc is not set to executable, but the current distristribution isn't set to executable, too - while it operates OK).

The boot output shows no anomalies.

I need some hints where to look for other possible problems.

-Rob

QuoteReplyEditDelete

2010-01-26 02:45:48     Re: Userspace Init problems

Mike Frysinger (UNITED STATES)

Message: 85116   

ive deleted your other posts then to avoid duplication

did you update your busybox config correctly ?  you probably didnt select a shell (old was msh, new is hush and msh is dead).

QuoteReplyEditDelete

2010-01-26 02:57:06     Re: Userspace Init problems

Rob Maris (GERMANY)

Message: 85119   

Wow!  100% hit (wish you were here...)

Thanks!

  • Created
Was this helpful?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.