2010-01-21 04:41:15     thttpd

2010-01-21 04:41:15     thttpd

Parimala Baggiri (INDIA)

Message: 84934   

Hello,

            Why is thttpd is not updated to the latest version(thttpd-2.25b)? With the existing version when I run thttpd apllication I get the following error

root:/> thttpd

chdir: No such file or directory

SEGV

And trace is

Jump to NULL address

Deferred Exception context

CURRENT PROCESS:

COMM=thttpd PID=267 CPU=0

TEXT = 0x00ac0040-0x00acfe60        DATA = 0x00acfe64-0x00ad343c

BSS = 0x00ad343c-0x00ad3b34  USER-STACK = 0x00ad7efc

return address: [0x000003ec]; contents of:

0x000003c0:  ????  ????  ????  ????  ????  ????  ????  ????

0x000003d0:  ????  ????  ????  ????  ????  ????  ????  ????

0x000003e0:  ????  ????  ????  ????  ????  ???? [????] ????

0x000003f0:  ????  ????  ????  ????  ????  ????  ????  ????

ADSP-BF537-0.3 500(MHz CCLK) 125(MHz SCLK) (mpu off)

Linux version 2.6.32.1-ADI-2010R1-pre-svn8037 (parimala@debian) (gcc version 4.3.4 (ADI-trunk/svn-3737) ) #320 Wed Jan 20 13:02:00 IST 2010

SEQUENCER STATUS:        Tainted: P        

SEQSTAT: 0000002d  IPEND: 0008  IMASK: ffff  SYSCFG: 0006

  EXCAUSE   : 0x2d

  physical IVG3 asserted : <0xffa0072c> /* kernel dynamic memory */

RETE: <0x00000000> /* Maybe null pointer? */

RETN: <0x00b76000> /* kernel dynamic memory */

RETX: <0x00000480> /* Maybe fixed code section */

RETS: <0x00aca076> [ thttpd + 0xa036 ]

PC  : <0x000003ec> /* Maybe null pointer? */

DCPLB_FAULT_ADDR: <0x00ad39d0> [ thttpd + 0x139d0 ]

ICPLB_FAULT_ADDR: <0x000003ec> /* Maybe null pointer? */

PROCESSOR STATE:

R0 : 00000001    R1 : 00aca234    R2 : 00ad3210    R3 : 00ad0967

R4 : 00000000    R5 : 00ad346c    R6 : 00000001    R7 : 00ad40ec

P0 : 00000001    P1 : ffffffff    P2 : 000003ec    P3 : 00000001

P4 : 00000001    P5 : 00acfe64    FP : 00ad40fc    SP : 00b75f24

LB0: 00ac8839    LT0: 00ac8836    LC0: 00000000

LB1: 00ac7cd9    LT1: 00ac7cd8    LC1: 00000000

B0 : 00000000    L0 : 00000000    M0 : 00000004    I0 : 00ad2f78

B1 : 00000000    L1 : 00000000    M1 : 00000000    I1 : 00000000

B2 : 00000000    L2 : 00000000    M2 : 00000000    I2 : 00000000

B3 : 00000000    L3 : 00000000    M3 : 00000000    I3 : 00000000

A0.w: 00000000   A0.x: 00000000   A1.w: 00000000   A1.x: 00000000

USP : 00ad40e0  ASTAT: 02003004

Hardware Trace:

   0 Target : <0x000050e0> { _trap_c + 0x0 }

     Source : <0xffa006c0> /* kernel dynamic memory */ CALL pcrel

   1 Target : <0xffa0061c> /* kernel dynamic memory */

     Source : <0xffa004dc> /* kernel dynamic memory */ RTX

   2 Target : <0xffa004c4> /* kernel dynamic memory */

     Source : <0xffa00574> /* kernel dynamic memory */ JUMP.S

   3 Target : <0xffa00500> /* kernel dynamic memory */

     Source : <0xffa00786> /* kernel dynamic memory */ JUMP (P4)

   4 Target : <0xffa0072c> /* kernel dynamic memory */

     Source : <0x00aca074> [ thttpd + 0xa034 ] CALL (P2)

   5 Target : <0x00aca062> [ thttpd + 0xa022 ]

     Source : <0x00aca240> [ thttpd + 0xa200 ] RTS

   6 Target : <0x00aca234> [ thttpd + 0xa1f4 ]

     Source : <0x00aca060> [ thttpd + 0xa020 ] CALL (P2)

   7 Target : <0x00aca050> [ thttpd + 0xa010 ]

     Source : <0x00aca250> [ thttpd + 0xa210 ] RTS

   8 Target : <0x00aca244> [ thttpd + 0xa204 ]

     Source : <0x00aca04e> [ thttpd + 0xa00e ] CALL (P2)

   9 Target : <0x00aca028> [ thttpd + 0x9fe8 ]

     Source : <0x00ac13ce> [ thttpd + 0x138e ] CALL pcrel

  10 Target : <0x00ac13cc> [ thttpd + 0x138c ]

     Source : <0x00ac731e> [ thttpd + 0x72de ] RTS

  11 Target : <0x00ac7318> [ thttpd + 0x72d8 ]

     Source : <0x00ac733e> [ thttpd + 0x72fe ] RTS

  12 Target : <0x00ac733a> [ thttpd + 0x72fa ]

     Source : <0x00ac7762> [ thttpd + 0x7722 ] RTS

  13 Target : <0x00ac775a> [ thttpd + 0x771a ]

     Source : <0x00ac7748> [ thttpd + 0x7708 ] IF CC JUMP

  14 Target : <0x00ac7744> [ thttpd + 0x7704 ]

     Source : <0x00ac7a00> [ thttpd + 0x79c0 ] RTS

  15 Target : <0x00ac79f8> [ thttpd + 0x79b8 ]

     Source : <0x00ac7872> [ thttpd + 0x7832 ] IF !CC JUMP

Userspace Stack

Stack info:

SP: [0x00ad40e0] <0x00ad40e0> [ thttpd + 0x140e0 ]

uclinux-dist: svn9274

Processor: BF537-STAMP

Regards,

Parimala

QuoteReplyEditDelete

2010-01-21 04:44:03     Re: thttpd

Mike Frysinger (UNITED STATES)

Message: 84935   

if no one is using/asking for a package, then we dont really care about it.  people who want simple http server tend to use boa, so that's what we've worked on.

btw, nothing is stopping you from building the latest upstream release yourself.

QuoteReplyEditDelete

2010-01-21 05:15:24     Re: thttpd

Parimala Baggiri (INDIA)

Message: 84936   

Thank you. I will go for latest version

QuoteReplyEditDelete

2010-01-21 13:16:27     Re: thttpd

Mike Frysinger (UNITED STATES)

Message: 84941   

latest svn uclinux-dist trunk has thttpd-2.25b

  • Created
Was this helpful?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.