2010-01-02 02:03:09     to cross compile usb_modeswitch in bfin-uclinux

2010-01-02 02:03:09     to cross compile usb_modeswitch in bfin-uclinux

Suganiya K (INDIA)

Message: 84118   

hi,

    i am trying to cross compile the usb_modeswitch in bfin-uclinux, where im getting error ...

unreferenced variables due to libusb. so i need to install standard user libusb for Bfin-uClinux..

i have the source of libusb-0.1.12.tar.bz2 but im unable to get the [.so/.a] library from that..

please help me out..

thnx

Suganiya

QuoteReplyEditDelete

2010-01-02 23:29:58     Re: to cross compile usb_modeswitch in bfin-uclinux

Mike Frysinger (UNITED STATES)

Message: 84135   

libusb is already integrated into the uclinux-dist

QuoteReplyEditDelete

2010-01-08 08:32:05     Re: to cross compile usb_modeswitch in bfin-uclinux

Suganiya K (INDIA)

Message: 84324   

Hi Mike,

                ok , but i was able to cross compile the usb_modeswitch code using bfin-uclinux, and included this bin with my uImage.

i wanted to connect Huwai Modem EC1260 with Blacfin BF561 board using uclinux platform. i hav used bfin-uclinux 2006R1 toolchain.

my prob is when i try to connect Usb Modem using

" usb_modeswitch -v 0x12d1 -p 0x140b -H -W"

i getting errors..unable to connect the device

if anybody  have any idea plz advise me.

Suganiya

QuoteReplyEditDelete

2010-01-10 22:20:28     Re: to cross compile usb_modeswitch in bfin-uclinux

Sonic Zhang (CHINA)

Message: 84395   

Are you sure  your USB modem is probed properly by kernel driver?

Please run lsusb.

In addition, 2006R1 is too old and never supported any more. Why not upgrade to 2009R1.1 release?

QuoteReplyEditDelete

2010-01-12 04:41:55     Re: to cross compile usb_modeswitch in bfin-uclinux

Suganiya K (INDIA)

Message: 84456   

hi

   i am sure my usb modem works fine... even if i build the kernel image with usb support, i am able to detect the usb device as mass storage device.. then i am unable to proceed with usb_modeswitch cross compilation.

   Right now i can't use uclinux-dist 2009R1 , i hav an already running application using 2006R1 dist. thats why..

  Do u hav any idea plz suggest me..

Regards

suganiya

  • Created
Was this helpful?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.