[2009R1.1-RC4] Failban or alternative?(2011-01-03)

2011-01-03 04:57:32     [2009R1.1-RC4] Failban or alternative?

Gilles Ganault (FRANCE)

Message: 97134   

Hello

I went through the options but didn't find the Failban application so I could stop accepting registration attempts from a given IP after X failed attempts.

Did I miss it, or if it's not part of uClinux-dist, is there an alternative solution?

Thank you.

QuoteReplyEditDelete

2011-01-03 09:14:14     Re: [2009R1.1-RC4] Failban or alternative?

Mike Frysinger (UNITED STATES)

Message: 97136   

do you actually mean fail2ban ?  it is not in the dist.  it is also a bit fat and requires python, so unless you need python for something else, seems like you should write your own simpler log parser.

QuoteReplyEditDelete

2011-01-03 11:52:44     Re: [2009R1.1-RC4] Failban or alternative?

Gilles Ganault (FRANCE)

Message: 97144   

Sorry. Yes, I meant "fail2ban".

I'll see if there a lighter solution that can reconfigure the firewall on the fly.

Thank you.

QuoteReplyEditDelete

2011-01-04 06:14:12     Re: [2009R1.1-RC4] Failban or alternative?

Gilles Ganault (FRANCE)

Message: 97165   

For those looking for the same thing: At least two options are available:

  code.google.com/p/logtrigger/

www.snort.org

  • Created
  • Updated
Was this helpful?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.