2009-12-18 11:52:28     No filesystem could mount root

2009-12-18 11:52:28     No filesystem could mount root

Jianxi Fu (UNITED STATES)

Message: 83702   

Hi

Could someone give me a hand?

My Test Information:

BF537-STAMP;

All were based on 2008R1.5-14

U-boot: u-boot-bf537-stamp-bypass-2008R1.5.bin (without modification)

And I can go through the initialization if I choose uImage-bf537-stamp-2008R1.5-RC3

But I just want to use uImage generated by myselfy

So I use uClinux-dist-2008R1.5-RC3.tar.bz2

Only thing I changed is that I use msh shell program

And others in menuconfig I use default

When the board power up, the information shows following:

-------------------------------------------------------------------------------------

U-Boot 1.1.6 (ADI-2008R1.5) (Dec 17 2009 - 17:18:17)

CPU:   ADSP bf537-0.2 (Detected Rev: 0.3)

Board: ADI BF537 stamp board

       Support:   blackfin.uclinux.org/

Clock: VCO: 500 MHz, Core: 500 MHz, System: 100 MHz

RAM:   64 MB

Flash:  4 MB

In:    serial

Out:   serial

Err:   serial

Net:   Blackfin EMAC

MAC:   00:E0:22:FE:5D:E6

Hit any key to stop autoboot:  0

Using Blackfin EMAC device

TFTP from server 192.168.0.2; our IP address is 192.168.0.15

Filename 'uImage'.

Load address: 0x1000000

Loading: T #################################################################

         #################################################################

         #################################################################

         #################################################################

         #########################################

done

Bytes transferred = 1539082 (177c0a hex)

## Booting image at 01000000 ...

   Image Name:   Linux-2.6.22.19-ADI-2008R1.5-svn

   Created:      2009-12-18  16:21:30 UTC

   Image Type:   Blackfin Linux Kernel Image (gzip compressed)

   Data Size:    1539018 Bytes =  1.5 MB

   Load Address: 00001000

   Entry Point:  00152000

   Verifying Checksum ... OK

   Uncompressing Kernel Image ... OK

Starting Kernel at = 152000

Linux version 2.6.22.19-ADI-2008R1.5-svn (root@localhost.localdomain) (gcc version 4.1.2 (ADI svn)) #3 Fri Dec 18 10:21:25 C9

early printk enabled on early_BFuart0

Hardware Trace Active and Enabled

Warning: limiting memory to 56MB due to hardware anomaly 05000263

Blackfin support (C) 2004-2007 Analog Devices, Inc.

Compiled for ADSP-BF537 Rev 0.2

Warning: Compiled for Rev 2, but running on Rev 3

Blackfin Linux support by   blackfin.uclinux.org/

Processor Speed: 500 MHz core clock and 100 MHz System Clock

Board Memory: 64MB

Kernel Managed Memory: 64MB

Memory map:

  text      = 0x00001000-0x000f9f90

  rodata    = 0x000fa000-0x00141c6c

  data      = 0x00142000-0x00152000

    stack   = 0x00142000-0x00144000

  init      = 0x00152000-0x00313000

  bss       = 0x00313000-0x00323050

  available = 0x00323050-0x037ff000

  DMA Zone  = 0x03f00000-0x04000000

NOMPU: setting up cplb tables for global access

Instruction Cache Enabled

Data Cache Enabled (write-through)

Built 1 zonelists.  Total pages: 14224

Kernel command line: root=/dev/mtdblock0 rw earlyprintk=serial,uart0,57600 console=ttyBF0,57600 ip=192.168.0.15:192.168.0.2:f

Configuring Blackfin Priority Driven Interrupts

PID hash table entries: 256 (order: 8, 1024 bytes)

console handover: boot [early_BFuart0] -> real [ttyBF0]

Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)

Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)

Memory available: 53548k/65536k RAM, (1796k init code, 995k kernel code, 417k data, 1024k dma, 7756k reserved)

Blackfin Scratchpad data SRAM: 4 KB

Blackfin Data A SRAM: 16 KB (15 KB free)

Blackfin Data B SRAM: 16 KB (16 KB free)

Blackfin Instruction SRAM: 48 KB (39 KB free)

Security Framework v1.0.0 initialized

Mount-cache hash table entries: 512

NET: Registered protocol family 16

Blackfin GPIO Controller

Blackfin DMA Controller

stamp_init(): registering device resources

Generic PHY: Registered new driver

NET: Registered protocol family 2

                                  IP route cache hash table entries: 1024 (order: 0, 4096 bytes)

TCP established hash table entries: 2048 (order: 2, 16384 bytes)

TCP bind hash table entries: 2048 (order: 1, 8192 bytes)

TCP: Hash tables configured (established 2048 bind 2048)

TCP reno registered

io scheduler noop registered

io scheduler anticipatory registered (default)

io scheduler cfq registered

ISA-BlackFin-CAN CAN Driver 3.4.6_AD_BLACKFIN (c) Dec 18 2009

BlackFin port by H.J. Oertel (oe@port.de)

bfin-wdt: initialized: timeout=20 sec (nowayout=0)

Serial: Blackfin serial driver

bfin-uart.1: ttyBF0 at MMIO 0xffc00400 (irq = 18) is a BFIN-UART

RAMDISK driver initialized: 16 RAM disks of 4096K size 1024 blocksize

SMSC LAN83C185: Registered new driver

bfin_mac_mdio: probed

bfin_mac: attached PHY driver [SMSC LAN83C185] (mii_bus:phy_addr=0:01, irq=-1, mdc_clk=2500000Hz(mdc_div=19)@sclk=100MHz)

bfin_mac: Version 1.1, Blackfin BF53[67] BF527 on-chip Ethernet MAC driver

bfin-spi bfin-spi.0: Blackfin BF5xx on-chip SPI Contoller Driver, Version 1.0, regs_base@ffc00500, dma channel@7

rtc-bfin rtc-bfin: rtc core: registered rtc-bfin as rtc0

TCP cubic registered

NET: Registered protocol family 1

NET: Registered protocol family 17

rtc-bfin rtc-bfin: setting the system clock to 1970-01-01 01:09:19 (4159)

IP-Config: Complete:

      device=eth0, addr=192.168.0.15, mask=255.255.255.0, gw=192.168.0.1,

     host=bf537-stamp, domain=, nis-domain=(none),

     bootserver=192.168.0.2, rootserver=192.168.0.2, rootpath=

List of all partitions:

No filesystem could mount root, tried:

Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(0,0)

PHY: 0:01 - Link is Up - 100/Full

QuoteReplyEditDelete

2009-12-18 12:00:19     Re: No filesystem could mount root

Mike Frysinger (UNITED STATES)

Message: 83703   

try reviewing:

  docs.blackfin.uclinux.org/doku.php?id=uclinux-dist:images

QuoteReplyEditDelete

2009-12-18 13:03:15     Re: No filesystem could mount root

Robin Getz (UNITED STATES)

Message: 83709   

Also - don't build things as root.

-Robin

QuoteReplyEditDelete

2009-12-18 13:10:07     Re: No filesystem could mount root

Mike Frysinger (UNITED STATES)

Message: 83710   

hmm, should we add to the toplevel Makefile:

ifeq ($(shell id -u),0)

$(error do not build as root)

endif

QuoteReplyEditDelete

2009-12-18 14:37:46     Re: No filesystem could mount root

Jianxi Fu (UNITED STATES)

Message: 83711   

Is it the prime reason that it cannot work?

QuoteReplyEditDelete

2009-12-18 14:47:21     Re: No filesystem could mount root

Jianxi Fu (UNITED STATES)

Message: 83713   

Dear Mike,

I have read the whole page.

I just use the uImage.initramfs, am I right?

And I found that the uImage I generated is just 1.5Mb

but when I download uImage-bf537 is about 4mb

Did I lost anything important?

How can I make a uImage just like the file I download?

Sorry for so much questions.

I'm a rookie and learn from this website step by step.

I hope that someone would give me great help here.

Sincerely

QuoteReplyEditDelete

2009-12-18 15:12:48     Re: No filesystem could mount root

Robin Getz (UNITED STATES)

Message: 83714   

Mike:

Yes, please - I'm sure it would be accepted upstream in the kernel too.

-Robin

QuoteReplyEditDelete

2009-12-18 17:43:37     Re: No filesystem could mount root

Mike Frysinger (UNITED STATES)

Message: 83718   

there is no correct answer for filesize.  if you disable packages/features, the image is going to be smaller.

your kernel output does not include features that are enabled by default, so it looks like you disabled things or the defaults werent selected.

best you upgrade to 2009R1, stop building things as root, and start off with the default config before trying to make any of your own changes.

QuoteReplyEditDelete

2009-12-21 10:05:55     Re: No filesystem could mount root

Robin Getz (UNITED STATES)

Message: 83795   

Jianxi:

There could be numerous issues caused when building as root. We don't test that way - so we don't know.

-Robin

QuoteReplyEditDelete

2009-12-21 14:50:57     Re: No filesystem could mount root

Jianxi Fu (UNITED STATES)

Message: 83799   

Dear Robin&Mike

I reinstall the host machine as your instrustion

Use 2009R1 toolchain,  And My OS is Fedora12

I install the package just as normal user instead of root

when I make the uClinux-dist, it still has problem:

compr_zlib.c: In function ‘jffs2_zlib_compress’:

compr_zlib.c:54: warning: unused parameter ‘model’

compr_zlib.c: In function ‘jffs2_zlib_decompress’:

compr_zlib.c:102: warning: unused parameter ‘model’

compr_zlib.c: At top level:

compr_zlib.c:130: warning: initialization discards qualifiers from pointer target type

mkdir -p /home/Veros/Blackfin/uClinux-dist/user/mtd-utils/build-606f38a2221648ca5c5fa292c9f71d2ddd59fa66-host/

gcc -I./include   -DWITHOUT_XATTR -D_FILE_OFFSET_BITS=64 -O2 -g -Wall -Wextra -Wwrite-strings -Wno-sign-compare -c -o /home/Veros/Blackfin/uClinux-dist/user/mtd-utils/build-606f38a2221648ca5c5fa292c9f71d2ddd59fa66-host/compr_lzo.o compr_lzo.c -g -Wp,-MD,/home/Veros/Blackfin/uClinux-dist/user/mtd-utils/build-606f38a2221648ca5c5fa292c9f71d2ddd59fa66-host/.compr_lzo.c.dep

compr_lzo.c:29:23: error: lzo/lzo1x.h: No such file or directory

compr_lzo.c: In function ‘jffs2_lzo_cmpr’:

compr_lzo.c:51: error: ‘lzo_uint’ undeclared (first use in this function)

compr_lzo.c:51: error: (Each undeclared identifier is reported only once

compr_lzo.c:51: error: for each function it appears in.)

compr_lzo.c:51: error: expected ‘;’ before ‘compress_size’

compr_lzo.c:54: warning: implicit declaration of function ‘lzo1x_999_compress’

compr_lzo.c:54: error: ‘compress_size’ undeclared (first use in this function)

compr_lzo.c:56: error: ‘LZO_E_OK’ undeclared (first use in this function)

compr_lzo.c:49: warning: unused parameter ‘model’

compr_lzo.c: In function ‘jffs2_lzo_decompress’:

compr_lzo.c:72: error: ‘lzo_uint’ undeclared (first use in this function)

compr_lzo.c:72: error: expected ‘;’ before ‘dl’

compr_lzo.c:74: warning: implicit declaration of function ‘lzo1x_decompress_safe’

compr_lzo.c:74: error: ‘dl’ undeclared (first use in this function)

compr_lzo.c:76: error: ‘LZO_E_OK’ undeclared (first use in this function)

compr_lzo.c:69: warning: unused parameter ‘model’

compr_lzo.c: At top level:

compr_lzo.c:84: warning: initialization discards qualifiers from pointer target type

compr_lzo.c: In function ‘jffs2_lzo_init’:

compr_lzo.c:95: error: ‘LZO1X_999_MEM_COMPRESS’ undeclared (first use in this function)

make[4]: *** [/home/Veros/Blackfin/uClinux-dist/user/mtd-utils/build-606f38a2221648ca5c5fa292c9f71d2ddd59fa66-host/compr_lzo.o] Error 1

make[4]: Leaving directory `/home/Veros/Blackfin/uClinux-dist/user/mtd-utils/606f38a2221648ca5c5fa292c9f71d2ddd59fa66'

make[3]: *** [all] Error 2

make[3]: Leaving directory `/home/Veros/Blackfin/uClinux-dist/user/mtd-utils'

make[2]: *** [mtd-utils] Error 2

make[2]: Leaving directory `/home/Veros/Blackfin/uClinux-dist/user'

make[1]: *** [all] Error 2

make[1]: Leaving directory `/home/Veros/Blackfin/uClinux-dist/user'

make: *** [subdirs] Error 1

QuoteReplyEditDelete

2009-12-21 14:57:50     Re: No filesystem could mount root

Mike Frysinger (UNITED STATES)

Message: 83800   

you need to install the lzo devel packages on your host system like the docs said

QuoteReplyEditDelete

2009-12-21 15:34:06     Re: No filesystem could mount root

Jianxi Fu (UNITED STATES)

Message: 83801   

Dear Mike

It works now!!

I appreciate you very much~~

Sincerely

Jianxi

QuoteReplyEditDelete

  • Created
Was this helpful?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.