2009-09-30 04:03:21     boot error

2009-09-30 04:03:21     boot error

Daniele Pagani (ITALY)

Message: 80705   

Dear sirs,

I'm moving my development tool from one pc to another.

Pc source:

uclinux revision 8812

linux 2.6.x revision 7258

toolchain:

blackfin-toolchain-09r1-2

blackfin-toolchain-uclibc-default-09r1-2

I have only one custom board, with BF537.

If I compile the image, it works fine, kernel starts, my application works fine and so on.

Pc destination:

uclinux revision 8915

linux 2.6.x revision 7527

toolchain:

blackfin-toolchain-09r1-2

blackfin-toolchain-uclibc-default-09r1-2

Same board, same u-boot.

OpenSuse 11.1 for Pc source and Pc destination.

If I compile the image, then the system doesn't start.

If I try a:

iminfo 0x20040000 in u-boot, then, I have:

   Image Name:   bf537-2.6.31.1-ADI-2010R1-pre

   Created:      2009-09-30   6:45:17 UTC

   Image Type:   Blackfin Linux Kernel Image (gzip compressed)

   Data Size:    2423584 Bytes =  2.3 MB

   Load Address: 00001000

   Entry Point:  001a0ef4

   Verifying Checksum ... OK

Then, if I do a iminfo with the right kernel, I have:

bfin> iminfo 0x20040000

## Checking Image at 20040000 ...

   Image Name:   bf537-2.6.30.5-ADI-2010R1-pre

   Created:      2009-09-29  15:28:11 UTC

   Image Type:   Blackfin Linux Kernel Image (gzip compressed)

   Data Size:    2552646 Bytes =  2.4 MB

   Load Address: 00001000

   Entry Point:  0019aeb4

   Verifying Checksum ... OK

I see that I have a different Entry Point.

I post also my u-boot settings:

printenv

bootdelay=5

baudrate=115200

loads_echo=1

ipaddr=192.168.0.15

serverip=192.168.0.2

rootpath=/romfs

gatewayip=192.168.0.1

netmask=255.255.255.0

hostname=bf537-stamp

loadaddr=0x1000000

ubootfile=u-boot.bin

update=tftp $(loadaddr) $(ubootfile);protect off 0x20000000 0x2003FFFF;erase 0x20000000 0x2003FFFF;cp.b $(loadaddr) 0x20000000 $(filesize)

addip=set bootargs $(bootargs) ip=$(ipaddr):$(serverip):$(gatewayip):$(netmask):$(hostname):eth0:off

ramargs=set bootargs root=/dev/mtdblock0 rw earlyprintk=serial,uart0,115200 console=ttyBF0,115200

ramboot=tftp $(loadaddr) uImage;run ramargs;run addip;bootm

nfsargs=set bootargs root=/dev/nfs rw nfsroot=$(serverip):$(rootpath),tcp,nfsvers=3

nfsboot=tftp $(loadaddr) vmImage;run nfsargs;run addip;bootm

flashboot=bootm 0x20100000

ethaddr=06:35:03:50:A0:A4

ethact=Blackfin EMAC

boot=bootm 0x20040000

bootcmd=bootm 0x20040000

bootargs=root=/dev/mtdblock0 rw earlyprintk=serial,uart0,115200 console=ttyBF0,115200 max_mem=32M mem=28M

stdin=serial

stdout=serial

stderr=serial

Environment size: 1014/8188 bytes

bfin>

Can somebody suggest me something?

Best regards,

Daniele.

TranslateQuoteReplyEditDelete

2009-09-30 04:16:52     Re: boot error

Mike Frysinger (UNITED STATES)

Message: 80707   

the different entry point really doesnt matter.  it'll change everytime a config option changes as it's in the middle of dynamic code (like it should be).

looks like you're trying to use trunk.  it's known to be a bit unstable so if you want to do real work, use the 2009R1 branch.

QuoteReplyEditDelete

2009-09-30 04:33:03     Re: boot error

Daniele Pagani (ITALY)

Message: 80709   

Ok,

but, see my last message: Message ID: 80198

With 2009R1 branch I've a problem, so I need to use svn version...so, I don't know if is possible to have the same revision on two pc; do I need to copy directory?

Anyway, I think that we can solve the problem. I give you additional information,

"system doesn't work fine" means:

bfin> bootm 0x1000000

## Booting image at 01000000 ...

   Image Name:   bf537-2.6.31.1-ADI-2010R1-pre

   Created:      2009-09-30   6:45:17 UTC

   Image Type:   Blackfin Linux Kernel Image (gzip compressed)

   Data Size:    2423584 Bytes =  2.3 MB

   Load Address: 00001000

   Entry Point:  001a0ef4

   Verifying Checksum ... OK

   Uncompressing Kernel Image ... OK

Starting Kernel at = 1a0ef4

Then the system is halted.

Could this suggest something?

Regards,

Daniele.

TranslateQuoteReplyEditDelete

2009-09-30 04:43:03     Re: boot error

Mike Frysinger (UNITED STATES)

Message: 80710   

you arent comparing the same exact versions of software, so where they're being built really doesnt matter.  you're probably hitting a bug that we've already fixed or are in the process of working on.  svn trunk is unstable and you shouldnt be using it.

there is no limitation whatsoever in any of the software from us in terms of having multiple versions on the same machine or across different machines.  if you know what you're doing, you can easily have multiple toolchains/kernels/uclinux-dists/etc... building simultaneously.

QuoteReplyEditDelete

2009-09-30 11:26:19     Re: boot error

Frank Van Hooft (CANADA)

Message: 80716   

Check your menuconfig settings, and make sure that your console UART port is actually enabled.

  • Created
Was this helpful?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.