2009-09-24 11:12:24     Setting minimal frequency for CPU frequency scaling

2009-09-24 11:12:24     Setting minimal frequency for CPU frequency scaling

Leonid Volpert (UNITED STATES)

Message: 80391   

Hi,

In our new product we are using BF-527 with core frequency 384MHz and sys frequency 96MHz.

By utilizing 'userspace' governor we can efficiently control core frequency from user space between 384 MHz and 192 MHz if DCACHE is enabled and between 384 MHz and 96 MHz if it's not

There is the following restriction in linux-2.6.x/arch/blackfin/mach-common/cpufreq.c that doesn't allow us to have at the same time minimal frequency 96MHz and DCACHE enabled.

#if ANOMALY_05000273 || (!defined(CONFIG_BF54x) && defined(CONFIG_BFIN_DCACHE))

min_cclk = sclk * 2;

#else

min_cclk = sclk;

#endif

What is the reason to have this restriction?

Is there any chance to bypass it?

Thanks,

Leonid

.

QuoteReplyEditDelete

2009-09-24 14:41:22     Re: Setting minimal frequency for CPU frequency scaling

Robin Getz (UNITED STATES)

Message: 80397   

Leonid:

try:

svn annotate linux-2.6.x/arch/blackfin/mach-common/cpufreq.c

  4656  hennerich

  6330     sonicz #if ANOMALY_05000273 || ANOMALY_05000274 || \

  6749       jiez       (!defined(CONFIG_BF54x) && defined(CONFIG_BFIN_EXTMEM_DCACHEABLE))

  4656  hennerich       min_cclk = sclk * 2;

then, when you know what revision you want to look at:

svn log linux-2.6.x/arch/blackfin/mach-common/cpufreq.c

------------------------------------------------------------------------

r6749 | jiez | 2009-06-16 05:48:33 -0400 (Tue, 16 Jun 2009) | 23 lines

[!no_src_qa!]Refine Blackfin cache configure options.

to look at that change -- svn diff -r 6748:6749 linux-2.6.x/arch/blackfin/mach-common/cpufreq.c

Index: linux-2.6.x/arch/blackfin/mach-common/cpufreq.c

===================================================================

--- linux-2.6.x/arch/blackfin/mach-common/cpufreq.c     (revision 6748)

+++ linux-2.6.x/arch/blackfin/mach-common/cpufreq.c     (revision 6749)

@@ -141,7 +141,7 @@

        sclk = get_sclk() / 1000;

#if ANOMALY_05000273 || ANOMALY_05000274 || \

-       (!defined(CONFIG_BF54x) && defined(CONFIG_BFIN_DCACHE))

+       (!defined(CONFIG_BF54x) && defined(CONFIG_BFIN_EXTMEM_DCACHEABLE))

        min_cclk = sclk * 2;

#else

so that isn't anything but a name change. Then it is:

r6330 | sonicz | 2009-05-07 22:43:24 -0400 (Thu, 07 May 2009) | 3 lines

Task[5094] reword workaround for anomaly 05000274.

svn diff -r 6329:6748 linux-2.6.x/arch/blackfin/mach-common/cpufreq.c

Index: linux-2.6.x/arch/blackfin/mach-common/cpufreq.c

===================================================================

--- linux-2.6.x/arch/blackfin/mach-common/cpufreq.c     (revision 6329)

+++ linux-2.6.x/arch/blackfin/mach-common/cpufreq.c     (revision 6748)

@@ -140,7 +140,8 @@

        cclk = get_cclk() / 1000;

        sclk = get_sclk() / 1000;

-#if ANOMALY_05000273 || (!defined(CONFIG_BF54x) && defined(CONFIG_BFIN_DCACHE))

+#if ANOMALY_05000273 || ANOMALY_05000274 || \

+       (!defined(CONFIG_BF54x) && defined(CONFIG_BFIN_DCACHE))

        min_cclk = sclk * 2;

#else

        min_cclk = sclk;

So -- it is something Sonic added. I'm not sure why, and it isn't in the log, or associated with a bug, so he will need to explain.

-Robin

QuoteReplyEditDelete

2009-09-24 14:48:06     Re: Setting minimal frequency for CPU frequency scaling

Mike Frysinger (UNITED STATES)

Message: 80399   

nah, that doesnt go back far enough.  it's faster with `git log -p`.

svn rev 4661 is what you want by Michael:

    [#3862] Cleanup Kconfig, fix comment and make sure we exclude CCLK=SCLK for some configurations

--- a/arch/blackfin/mach-common/cpufreq.c

+++ b/arch/blackfin/mach-common/cpufreq.c

@@ -134,7 +134,7 @@ static int __init __bfin_cpu_init(struct cpufreq_policy *policy)

    cclk = get_cclk();

    sclk = get_sclk();

-#if ANOMALY_05000273

+#if ANOMALY_05000273 || (!defined(CONFIG_BF54x) && defined(CONFIG_BFIN_DCACHE))

    min_cclk = sclk * 2;

#else

    min_cclk = sclk;

QuoteReplyEditDelete

2009-09-29 09:26:28     Re: Setting minimal frequency for CPU frequency scaling

Leonid Volpert (UNITED STATES)

Message: 80634   

Thanks for your help.

Just curious from where this exclusion CCLK=SCLK is coming, is it Linux or Blackfin itself?

Thanks again

Leonid.

QuoteReplyEditDelete

2009-09-29 15:01:49     Re: Setting minimal frequency for CPU frequency scaling

Robin Getz (UNITED STATES)

Message: 80649   

Leonid:

It is the Blackfin. We could not make things work reliably without this change, and reported it to the hardware team, and have been waiting for an answer back. We When you posted - we poked them again, and they said they would look into it.

-Robin

QuoteReplyEditDelete

2009-09-30 09:42:17     Re: Setting minimal frequency for CPU frequency scaling

Leonid Volpert (UNITED STATES)

Message: 80714   

Thank you, Robin.

Looking forward to have more information from hardware team.

Leonid.

  • Created
Was this helpful?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.