2009-09-24 06:10:02     Force NET2272 into full-speed mode

2009-09-24 06:10:02     Force NET2272 into full-speed mode

Mattias K (SWEDEN)

Message: 80370   

Hi,

Is there anybody who has tried to force the usb chip (NET2272) into full-spedd mode?

We have tried setting the testbit as described in the manual without success.

From the manual:

5.9     USB Test Modes

The Force Full Speed and Force High Speed bits of the XCVRDIAG register can be used to force the NET2272

into full and high speed modes, respectively. These forcing bits must not be used in normal operation; they are

for testing purposed only. In normal operation, the NET2272 automatically performs USB 2.0 Chirp Protocol

negotiation with the host to determine the correct operating speed.

USB 2.0 Test Mode support is provided via the Test Mode Select field of the USBTEST register. These bits select

the appropriate USB Test Mode settings (see section 9.4.9 in the USB Specification Revision 2.0 for more details).

Normally, the host sends a SET_FEATURE request with the Test Selector in the upper byte of wIndex. The Test

Selector can be copied directly into the NET2272 USBTEST register to select the correct test mode.

regards,

Mattias

  • Created
Was this helpful?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.