2009-09-23 03:12:57     debugging kernel using kgdb over JTAG

2009-09-23 03:12:57     debugging kernel using kgdb over JTAG

Manu AS (INDIA)

Message: 80273   

Hi

I want to enable kernel debugging using gdb over JTAG.

Following are some of the config details:

Target HW: bf561 based dev board

uClinux distribution: 2008R1

JTAG device: ADDS-HPUSB-ICE

Can some body tell me the steps for the same.

Thanks

QuoteReplyEditDelete

2009-09-23 10:05:55     Re: debugging kernel using kgdb over JTAG

Mike Frysinger (UNITED STATES)

Message: 80309   

as the documentation states, the HPUSB ICE is not supported.  further, kgdb is a software-only debugger which means it makes no sense to use it with jtag.

if you want to debug the kernel via jtag, go buy a gnICE.

QuoteReplyEditDelete

2009-09-24 00:16:08     Re: debugging kernel using kgdb over JTAG

Manu AS (INDIA)

Message: 80327   

Thanks Mike.

  • Created
Was this helpful?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.