2009-09-01 06:14:33     Getting started with an EZKIT-BF533

2009-09-01 06:14:33     Getting started with an EZKIT-BF533

Rainer Zufall (GERMANY)

Message: 79426   

Hi folks.

I would like to try out uCLinux. Unfortunately I don't have a Stamp Board, but only an EZKIT-BF533.

I've found an article which says that it is possible to run uCLinux with an EZKIT:

  docs.blackfin.uclinux.org/doku.php?id=hw:boards:bf533-ezkit

But I have no idea how to start with an EZKIT and I didn't found anything on the internet what could help me.

Would anyone be so kind to give me a hint (or two :-)

Thanks a lot.

TranslateQuoteReplyEditDelete

2009-09-01 06:52:39     Getting started with an EZKIT-BF533

Michael Hennerich (GERMANY)

Message: 79429   

Linux runs also on the BF533-EZKIT.

  docs.blackfin.uclinux.org/doku.php?id=hw:boards:bf533-ezkit

Your main problem for now is to get u-boot flashed.

  docs.blackfin.uclinux.org/doku.php?id=bootloaders:u-boot

  docs.blackfin.uclinux.org/doku.php?id=bootloaders:u-boot:loading

Later you probably want to have a USB-LAN card too.

  docs.blackfin.uclinux.org/doku.php?id=hw:cards:usb-lan_ez-extender

-Michael

QuoteReplyEditDelete

2009-09-02 09:07:13     Re: Getting started with an EZKIT-BF533

Rainer Zufall (GERMANY)

Message: 79495   

Thank you for your answer.

I simply don't know how to start.

I tried to follow these steps:

  docs.blackfin.uclinux.org/doku.php?id=setting_up_your_development_host

1.Step: Installing / Configuring Linux - No Problem. Worked fine.

next Step would be: Terminal Programs

But how could I communicate with my EZKIT via UART? There ist no Firmware which could answer...

What do I have to do next? There is too much (or not good structured) information for a beginner.... :-(

I'am looking for a step by step getting startet guid. Like a tutorial or a HowTo....

Or at least someone who could tell me the first steps to getting started.

TranslateQuoteReplyEditDelete

2009-09-02 09:34:58     Re: Getting started with an EZKIT-BF533

Michael Hennerich (GERMANY)

Message: 79496    As I said - you need to get u-boot flashed first.

If you have the VDSP testdrive installed - You can do that by using the

VDSP flash programmer.

Flash the BF533-EZKIT u-boot.bin image posted here:

  blackfin.uclinux.org/gf/project/u-boot/frs

-Michael

QuoteReplyEditDelete

2009-09-02 09:35:05     Re: Getting started with an EZKIT-BF533

Robin Getz (UNITED STATES)

Message: 79497   

Rainer:

We are in process of getting something like that together over the next day or two.

I need to move some things around in the docs, and I'll point you to the work in progress.

-Robin

QuoteReplyEditDelete

2009-09-02 15:15:29     Re: Getting started with an EZKIT-BF533

Robin Getz (UNITED STATES)

Message: 79498   

Rainer:

https://docs.blackfin.uclinux.org/doku.php?id=intro:getting_started

Can you review - and see if that helps?

Thanks

-Robin

QuoteReplyEditDelete

2009-09-03 09:04:37     Re: Getting started with an EZKIT-BF533

Rainer Zufall (GERMANY)

Message: 79561   

@Robin: This is what I was looking for. Now I have a better understand of the whole process.

Thank you very very much!

TranslateQuoteReplyEditDelete

2009-09-03 09:09:23     Re: Getting started with an EZKIT-BF533

Rainer Zufall (GERMANY)

Message: 79562   

As I said - you need to get u-boot flashed first.

If you have the VDSP testdrive installed - You can do that by using the

VDSP flash programmer.

Flash the BF533-EZKIT u-boot.bin image posted here:

  blackfin.uclinux.org/gf/project/u-boot/frs

I am using VDSP 5.0 and the HPUSB-IC. Do I have to flash the .ldr or the .bin file?

I tried both (selected 'File format: Binary'), but with no success

If it succeeded, U-Boot should send a message after booting via UART which I could receive with the HyperTerminal, is that correct?

TranslateQuoteReplyEditDelete

2009-09-03 11:03:25     Re: Getting started with an EZKIT-BF533

Mike Frysinger (UNITED STATES)

Message: 79567   

which file you select depends on which boot mode you want

please read the documentation:

  docs.blackfin.uclinux.org/doku.php?id=bootloaders:u-boot:loading

  • Created
Was this helpful?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.